Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Is it time to end our love affair with R-PI?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 45 replies
  • Subscribers 701 subscribers
  • Views 10066 views
  • Users 0 members are here
Related

Is it time to end our love affair with R-PI?

KennyMillar
KennyMillar over 3 years ago

It has been almost impossible to buy R-PI for so long now.

The foundation say they are still manufacturing 400,000 a month - but where are they going? 
Certainly not to many retailers.

Is it time to find alternatives, and walk away from R-PI?

  • Sign in to reply
  • Cancel
Parents
  • baldengineer
    baldengineer over 3 years ago

    There are already a number of alternatives out there: Libre Computer, Orange Pi, Banana Pi, BeagleBone Black, and more.

    Some are more powerful. Some offer additional features (and form factors). All run some form of Linux. And most of them are available today.

    If your focus is the GPIO then boards like the BeagleBone are already a better option. And if your focus is a low-cost computing platform, then you can add in the NUC and a ton of other items.

    Will the mass market move to one of these? Probably not. With so many options there will just be fragmentation moving forward.

    The apparent shift of focus for Raspberry Pi Trading, LTD to industrial/commercial customers does imply it is time for the non-commercial market to consider alternatives.

    However, I doubt any will become as ubiquitous as the Pi had been.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • rsjawale24
    rsjawale24 over 3 years ago in reply to baldengineer

    What surprises me is that Beaglebone was available way before Raspberry Pi's launch. Yet R-pi has replaced almost every SBC in the market. Not sure why..

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 3 years ago in reply to rsjawale24

    IMHO, Marketing and availability of open source collaboration. RPi has a pleasant website aimed at kids and beginners, great support organization,  free online fun project books, all kinds of option cards with libraries, all being continuously improved. 

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 3 years ago in reply to rsjawale24

    rsjawale24 I will say dito to robogary's comment. And BTW I really don't care for it, It has almost no I/O but It handles things well, like a complete VOIP phone system but you have to add a IDE drive and a second Network port for the phones via my Cisco VOIP switch. Stuck out tongue winking eye but the dam thing will not support OpenBSD!! Rage

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo over 3 years ago in reply to rsjawale24

    I'm going with price point.  The RPi is hard to beat in that category.  At $35, I could afford to try my hand at it and not worry as much about accidentally destroying it.  The Beaglebone is more affordable now, but I remember it being a bit pricey to start.  Some of the other SBC's now are priced beyond consideration for my limited skill set.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 3 years ago in reply to kmikemoo
    kmikemoo said:
    Some of the other SBC's now are priced beyond consideration

    I agree, those might be good for industry, but for myself as a hobbyist, and for general personal use, other options are much more useable and affordable - like tablets, laptops, those small cube type computers, or even used computers.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to rsjawale24

    BeagleBone Black was superior in many ways technically, but suffered (at least for hobbyists/enthusiasts) a lot from:

    • Unfamiliar Linux distribution (Angstrom) for quite a while
    • Not enough space for a decent full Linux distribution, because the eMMC was small, so the eMMC lay redundant when micro SD was used, as just an extra unwanted cost. I can't recall if Angstrom on the eMMC even had enough space for a compiler, possibly not. This didn't keep up with the trend of just using the target device for native compiles, as the device performance increases. Just because in the past we didn't have enough resources on many SBCs, didn't mean we needed to keep doing things the same way, at least not from the hobbyist perspective. Business is a different matter.
    • Poor user experience with (say) different sysfs paths for features like GPIO from time to time, rendering old helpful blog posts now unhelpful and (to beginners at least) entirely useless
    • No C compiler for the real-time component for ages (years I think)
    • What  kmikemoo says.  There were extremely poor pricing decisions. Production couldn't keep up, so their solution (clearly I guess by a technical person) was to hike the price. They were quite open that this was the reason for the increase in price. Kind of ridiculous because all that does is make people feel they are being short-changed. If you're really going to charge more then give people more.
    • No decent GPIO libraries for C and a few other languages for ages. For example I had to write my own C library and self-support it for quite a while. So the overhead for getting stuff done with the BeagleBone Black was quite a bit higher, unless you were really into JavaScript (which did have some GPIO support).
    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 3 years ago in reply to shabaz

    I was at a conference once with a BeagleBone Black workshop. I was astounded by how much time and effort was required to get to the point of blinking an LED.

    Now, granted, an SBC isn't an ideal platform for LED blinking. But still, the number of steps to get started was so high I ended up walking out of the workshop.

    I never even got to doing anything much on the "Linux side."

    And, as you pointed out, finding good references or tutorials is nearly impossible. There are so many different ways to do seemingly simple tasks that I could never figure out the exact search phrase I needed.

    It's a powerful board and I appreciate its open nature. But it 100% feels like a platform designed by engineers for the engineers who designed it--not everyone else.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • dang74
    dang74 over 3 years ago in reply to kmikemoo

    Yes, I remember hearing about the Beagle board many, many years ago.  But it was its price point that prevented me from pulling the trigger.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to dang74

    Economy changed. Now the Pi is cheaper but virtually not for sale. The BB is available.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • dang74
    dang74 over 3 years ago in reply to Jan Cumps

    True enough.  Could be worth another look.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 3 years ago in reply to shabaz

    This says it all for those who wish to seriously use one or the other as a workstation or a server: https://linuxhint.com/beagle-bone-black-vs-raspberry-pi/

    My RPi4 with LPDDR4 8GB RAM and quad-core Cortex-A72 CPU is an excellent network node when I couple it with a USB3 boot+system drive.  For hobbyist purposes, this comparison may not matter.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 3 years ago in reply to shabaz

    This says it all for those who wish to seriously use one or the other as a workstation or a server: https://linuxhint.com/beagle-bone-black-vs-raspberry-pi/

    My RPi4 with LPDDR4 8GB RAM and quad-core Cortex-A72 CPU is an excellent network node when I couple it with a USB3 boot+system drive.  For hobbyist purposes, this comparison may not matter.