Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum RPi CM4 alternative for a DVR project
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 702 subscribers
  • Views 2032 views
  • Users 0 members are here
  • shortage
  • rpi cm4
  • raspberry pi
Related

RPi CM4 alternative for a DVR project

saadtiwana_int
saadtiwana_int over 3 years ago

Hi,

For a particular project I need to add video and snapshot recording to the device I'm building. I have a Zynq-7000 FPGA performing the video manipulation and all of that is working fine. The customer wants to add video and snapshot recording (a.k.a DVR). One solution I thought of was to feed the video output from my FPGA to a RPi CM4 via the MIPI interface, build a DVR application inside the RPi, and route the HDMI output back to the FPGA. The control signals can be passed via uart or GPIO between the FPGA and RPi. 

However, the RPi compute module has been out of stock for more than a year and things dont' seem to be improving so far.I could probably find one or two on ebay or similar, but I don't want to use somethign I can't source in quantities 6 months down the line. So I think I need to find an alternative. Ideally, I want something that I can plug into the main baseboard I am building (like the RPi CM4 does) for reliability. I have seen many RPi experts on this forum, and I am hoping to get some recommendations for alternatives that are easier to source. 

Looking forward to hearing from you!

- Saad

p.s If you know of a better approach to adding DVR functionality compared to my use of RPi, please do share as well! I have considered switching to KRia SOM but it will not fit the budget, plus that is suffering from availability issues too.

  • Sign in to reply
  • Cancel
  • dougw
    0 dougw over 3 years ago

    A lot of low cost dash cam DVRs record MIPI cameras. Would one of those be adequate?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • saadtiwana_int
    0 saadtiwana_int over 3 years ago in reply to dougw

    Hi dougw 

    Thank you for your reply. You're right there are many dashcam DVRs available. But I cannot put them inside my product because they are closed source and so I cannot integrate them in my system too nicely. Also, replacing the MIPI camera with my own input will be impossible because the control channel (I2C) commands will most certainly be different between the two cameras.