Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum 24v COB rgb 840 strip controled by Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 63 replies
  • Subscribers 698 subscribers
  • Views 11493 views
  • Users 0 members are here
Related

24v COB rgb 840 strip controled by Raspberry Pi

fskrzycki
fskrzycki over 3 years ago

I am having a hard time figuring out the solution to controlling my 24v strip with my Pi 4. I have a 4 pin strip with R. B. G. Bk wires.  I think a N-channel MOSFETs transistor will fix the communication issue and allow control of the colors. most Ara fruit software I have seen is for addressable Leds with only 3 leads. R. Bk. and Green.  Am I on the right track with using the transistors. If so Why? is there an easier way? I am making a bay blade stadium for my son and want to incorporate buttons with lights and sound.. 

  • Sign in to reply
  • Cancel
Parents
  • phoenixcomm
    phoenixcomm over 3 years ago

    image fskrzycki You have a big problem 24+ volts and logic do not never mix.  I have one better than my buddy shabaz has AND you only need 1 part to use an optio-isolator anything in the 4N44 etc (there are tons of them on eBay,) will work just look at the collector voltage and current. ~~ C. Harrison

    Update 9/3 I Fibed!  image It has 2 parts, see the comment below. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to phoenixcomm

    I like opto-isolators too, there are some fancy ones that can directly drive MOSFETs. In the end I only sketched one approach with transistors since unfortunately I didn't have time to provide additional circuit options : (

    The transistors are less exotic I guess!, but really all of these approaches are a bit excessive for the use-case, because the Neopixel-like strips would eliminate all of the circuit (well, almost all - might still need to adapt the 3.3V to 5V logic levels).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 3 years ago in reply to shabaz

     shabaz  Well, there are more ways to skin this cat. Slight smile level shifters cost $ while, your approach used more than a few parts, The optocouplers on eBay are about a half a buck each, buy 10 and save. but you will have to use a resistor in between the coupler and your Arduino's output pin (5v) the iso normally turns on at 1.3 volts so a quick trip to Mr Ohms or E= 1*R  so  R =( 5 -1.2)/20ma = 180Ω. But most likely get away with 220Ω ~~Cris H 

    BTW I use this approach in my sim where the lamps are 28 volts ouch!  REMEMBER DO NOT USE A COMMON GROUND OR POWER SOURCE, or you will lose your galvanic isolation - this could ruin your week!!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • fskrzycki
    fskrzycki over 3 years ago in reply to phoenixcomm

    the logic mosfets i ordered are rated to be maxed out@30v so i was not to concerned. my Pi is controlling the DC24v COB strip with  a GPIO setup for each color. Im using ChangeDutyCycle to control the color. pretty cool. The color wheel runs from 0-255 and CDC controls the current cycle of the mosfets with ratings 0-100%. I can generate any color by dividing 255 (100% power) into any color number than multipling that result by the number again. Currently the program will run any 1 color super bright for me (why i went with 24v) in an endless loop using the "while true" statement. The LEDs turn off fine when i break the loop. the program ends without error. 

    the rub is after ai end the program. if powere is left connected to the strip, The LEDs turn themselves on to a yellow color.  interesting. i think the Red and Green MOSFETs are leaking.

    when the project is complete. the python script will loop endlessly from startup and only break when a button is pushed to execute an "else" statement. which will be a sound wav file and some cycle color changes.

    should i be concerned abiut the yellow? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 3 years ago in reply to shabaz

    I had a negative experience with PC817 opto-isolators and Raspberry Pi so I tend to shy away from using them.

    image

    The Pi 3.3 output didn't drive the opto-isolator into saturation. I spent considerable time trying to resolve the issue and in the end used level-shifters to obtain consistency.

    I would be the first to say it could have been my lack of knowledge but I have a box of  modules that I hope to use someday:)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to colporteur

    I can imagine incompatibility is a common problem with so many modules which are really sub-circuits,

    The modules stores always feel like an attempt to turn electronics into a fast food place, where it doesn't matter what burger goes in which bun, it will all kind of work out. 

    But electronics is not like that, since the devil is in the detail, there's no standard interface on many of these modules. I couldn't find a datasheet, but it appears from some online diagrams that there is an external LED in series with the optocoupler's internal LED, so the total forward voltage drop is quite possibly higher than 3.3V logic levels. A quick fix (would not need level shifters would be to short out the external LED (e.g. desolder it and place a blob of solder). Then, it would be compatible with the outputs from a Pi.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • anniel747
    anniel747 over 3 years ago in reply to shabaz
    This reply was deleted.
    • Cancel
    • Cancel
Reply
  • anniel747
    anniel747 over 3 years ago in reply to shabaz
    This reply was deleted.
    • Cancel
    • Cancel
Children
  • fskrzycki
    fskrzycki over 3 years ago in reply to anniel747

    I like the idea. of using an optocoupler between the MOSFET and the 24v strip. I think it will provide electrical isolation and prevent signal leakage between the Raspberry Pi and the LEDs. This will be an effective way to protect my Raspi from potential voltage spikes... Loke, when I plug in the power cord for the Strip... lol. This should minimize the risk of signal leakage.   Thanks