Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum 24v COB rgb 840 strip controled by Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 63 replies
  • Subscribers 698 subscribers
  • Views 11520 views
  • Users 0 members are here
Related

24v COB rgb 840 strip controled by Raspberry Pi

fskrzycki
fskrzycki over 3 years ago

I am having a hard time figuring out the solution to controlling my 24v strip with my Pi 4. I have a 4 pin strip with R. B. G. Bk wires.  I think a N-channel MOSFETs transistor will fix the communication issue and allow control of the colors. most Ara fruit software I have seen is for addressable Leds with only 3 leads. R. Bk. and Green.  Am I on the right track with using the transistors. If so Why? is there an easier way? I am making a bay blade stadium for my son and want to incorporate buttons with lights and sound.. 

  • Sign in to reply
  • Cancel
Parents
  • fskrzycki
    fskrzycki over 2 years ago

    I only want to have 1 power supply for this Project. Can I use a LM2596 DC-DC Buck Converter to provide power to my 24v LED strip and power to my Raspberry pi.

    I think will have to split off the wires from my current supply to feed into the new controlling Circuit powering the Strip before feeding into the buck converter. I would also need to strip a USB-A extension cable so I a viable connection for the USB-A to USB-C cord that connects to my Ras-pi

    I'm not sure what complications if any could be involved.

    please advise 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to fskrzycki

    The LM2596 modules look a bit risky. It might cause brownout of the Pi 4, or could damage it.

    Disclaimer: I've never used that module, so I'm speculating, but I don't get a good feeling about them visually. The feedback isn't universally good: https://www.eevblog.com/forum/reviews/lm2596-dc-dc-step-down-modules-load-testing/

    Plus, the Pi 4 has more difficult to achieve supply requirement than a Pi 3B.

    It could be better either switching to a Pi 3B, and/or using a board such as these ones:

    https://www.pololu.com/category/261/d36v28fx-step-down-voltage-regulators

    No need to source a USB cable to strip; the power can be applied to the 5V pin on the 40-way connector on the Pi.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 2 years ago in reply to fskrzycki

    The LM2596 modules look a bit risky. It might cause brownout of the Pi 4, or could damage it.

    Disclaimer: I've never used that module, so I'm speculating, but I don't get a good feeling about them visually. The feedback isn't universally good: https://www.eevblog.com/forum/reviews/lm2596-dc-dc-step-down-modules-load-testing/

    Plus, the Pi 4 has more difficult to achieve supply requirement than a Pi 3B.

    It could be better either switching to a Pi 3B, and/or using a board such as these ones:

    https://www.pololu.com/category/261/d36v28fx-step-down-voltage-regulators

    No need to source a USB cable to strip; the power can be applied to the 5V pin on the 40-way connector on the Pi.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • fskrzycki
    fskrzycki over 2 years ago in reply to shabaz

    finished circuit, fingers crossed. imageimageimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fskrzycki
    fskrzycki over 2 years ago in reply to fskrzycki

    Hey Shabaz,

    I  connected  all the zero volt grounds on tbe Zenner Diode side to the Power Supply Ground.

    I am seeing a large decrease in brightness when GPIO PIN IS SET High.

    I am able to control color frequency. so the optocoupler works!  awesome!

    unfortunately, I still have a leak because they gradually get brighter.

    I lowered the resistance after the optocoupler on the diode side to. 10k. no change.

    the leak must be on the diode side. Any suggestions?