Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum 24v COB rgb 840 strip controled by Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 63 replies
  • Subscribers 697 subscribers
  • Views 11621 views
  • Users 0 members are here
Related

24v COB rgb 840 strip controled by Raspberry Pi

fskrzycki
fskrzycki over 3 years ago

I am having a hard time figuring out the solution to controlling my 24v strip with my Pi 4. I have a 4 pin strip with R. B. G. Bk wires.  I think a N-channel MOSFETs transistor will fix the communication issue and allow control of the colors. most Ara fruit software I have seen is for addressable Leds with only 3 leads. R. Bk. and Green.  Am I on the right track with using the transistors. If so Why? is there an easier way? I am making a bay blade stadium for my son and want to incorporate buttons with lights and sound.. 

  • Sign in to reply
  • Cancel
Parents
  • colporteur
    colporteur over 3 years ago

    My apologies  fskrzycki for my response on using modules solutions to solve problems consuming your post. That was never my intention. 

    You being a new member, it does provide an example of the potential the E14 Community provides. You will need to develop the ability to keep from getting upset or offended by the things other people say and do. You have to have a thick skin when it comes to criticism. Most responses are OK but with 700K members there may be some responses that reflect a lack of emotional intelligence.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • javagoza
    javagoza over 3 years ago in reply to colporteur

    I remember one of my early forum adventures when I tried to help out a fellow member with my limited knowledge. I suggested a simple solution, and then this person got all fired up and replied, "Some of us solder components!" Joy My kids still crack up about that post. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • fskrzycki
    fskrzycki over 3 years ago in reply to fskrzycki

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to fskrzycki

    That helps a lot. Based on that, if the circuit so far is successfully operational, then the LED strip is known as common anode (not common ground), which helps understand the circuit.

    The circuit below shows how to insert the PC817. Notice that the Pi's GND is completely isolated from the 0V connection which will be connected to your LED strip's power supply brick.

    With the PC817, the output will be inverted, i.e. you'll have to set the GPIO high to turn off the LED and vice-versa. There's no clean way around that, without changing the design, or inserting more parts (refer to the earlier diagrams to see how that is done). Rather than that, it should be a trivial change to edit the Python code to invert the logic.

    Every component in the diagram below is essential. If you're using a PC817 module (as opposed to just the PC817 component) then, as discussed earlier, the module has some issues. You'd need to remove the LEDs on the PC817 board, and you'd need to replace the 1k resistor on the board with 220 ohms as shown in the sketch here. It would be easier to just buy the PC817 component and not the module, but modifying the module as mentioned would fix it.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • fskrzycki
    fskrzycki over 3 years ago in reply to shabaz

    i understand. Just to be clear the circuit above is for one color only.. if I go with using the 817 component, can I use the same gpio ground pin for each color? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fskrzycki
    fskrzycki over 3 years ago in reply to fskrzycki

    Can the overvoltage protection be the same component in the example above? I think you have the Gate/Source/Drain on the MOSFET mislabeled. can you double check 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fskrzycki
    fskrzycki over 3 years ago in reply to fskrzycki

    i may be over thinking this, but it looks like i dont need the MOSFET at all. what would the circuit look like without it? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to fskrzycki

    Correct, only one channel is shown since they are all identical. All the 0V connections will be common together. All the Pi ground connections (GND) will be common together (GND will not be connected to 0V; they are isolated).

    Every pin labeled ground on the Pi's header is electrically connected to each other (you can verify with a multimeter set to ohms on an unpowered Pi if you like). It makes no difference if you use a single ground pin, or separate ground pins for the project.

    The zener diode protects just the MOSFET. The PC817 protects the Pi by isolating it, since there are zero connections from the Pi that are present on the right side. The GPIO and the Ground from the pi on the left are totally isolated beyond the LED inside the optocoupler.

    The labeling on the MOSFET in the sketch above is correct. Without the MOSFET, this can't work. the PC817 does not have the output capability to operate the strip.

    You could remove the entirety of the circuit with a 'neopixel' style LED strip as mentioned earlier. The strip you currently have will need the parts shown above, if you want the PC817 isolation.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • fskrzycki
    fskrzycki over 3 years ago in reply to shabaz

    thanks, what wattage level resistors would you recommend? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to fskrzycki

    1/4 W is fine for them all, or even 1/8 W.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • fskrzycki
    fskrzycki over 3 years ago in reply to shabaz

    I'm making some progress, P817's have not arrived. currently mapping out PCB. double sided. I have a clever way of connecting them all.  White on left is Raspi ground. long white down middle is zero volt.

    Blue terminal is location of 817's

    imageimage

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • fskrzycki
    fskrzycki over 3 years ago in reply to colporteur

    funny, I cannot find a single free Android circuit design application that includes an optocoupler. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • fskrzycki
    fskrzycki over 3 years ago in reply to colporteur

    funny, I cannot find a single free Android circuit design application that includes an optocoupler.