Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum The Raspberry Pi 5 Case and Active Cooler are available for some, how do they look?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 29 replies
  • Subscribers 697 subscribers
  • Views 14856 views
  • Users 0 members are here
  • raspberry pi case
  • raspberry pi 5 active cooler
  • raspberry pi 5
  • active cooler for raspberry pi
  • Raspberry Pi Case for Raspberry Pi 5
Related

The Raspberry Pi 5 Case and Active Cooler are available for some, how do they look?

cstanton
cstanton over 2 years ago

Raspberry Pi Active Cooler for Raspberry Pi 5

box

The size of this box is about 1/6th of the volume of a Raspberry Pi 5 case, being about half its length and about the same width, and half its height.

The heatsink and fan itself is rather simple in its design. 

I am surprised by the fan not pulling air over the heatsink fins, and those fins being rather uniform. I'm certain they help to pull heat away from the chips, but without active air going over all of it, I suspect its capability is a bit diminished.

The fan though, is over the top of where the processor lies, so that will be doing most of the work anyway. It has a 4 wire connection to the Raspberry Pi, allowing for feedback as to how fast it is spinning, along with control over how fast it spins. Including 5v power and ground.

heatsink fan

The heatsink comes with three pads, probably to help level out the heatsink more than anything, but the areas to which it attaches are the power circuitry, wireless LAN shield and the processor. There are no pads on the RAM or RP1.

pads

Now if we compare this to the Raspberry Pi Case for the Raspberry Pi 5, we only get a small heatsink, which is surprising considering the size and pads on the dedicated heatsink.

case

Now, you can still have the dedicated heatsink attached to the Raspberry Pi 5 and use the case, but you then need to disconnect the fan inside the case and throw away this small, now spare, heatsink.

I find it weird that the 'standalone' heatsink would be such a monster of size compared to what's suggested to use in the case, especially since inside a case you're going to want to pull away and move a lot more heat at once.

And no, you can't connect the case fan and the dedicated heatsink fan at the same time. If you want to, you can remove the fan from the dedicated heatsink and rely on the case fan instead, but that feels a bit weird. I'll have to do some benchmarks and tests to see what the best setup is.

Raspberry Pi Case for Raspberry Pi 5

Case Box

The Raspberry Pi Case is very slick, it has a smooth, nice design and it comes apart really easily. If you have a Raspberry Pi 5 and want it to sit on your desk, this is something that will keep the dust off. Talking of 'off' though, I can see you will mainly keep the lid off if you want to be able to use anything significant, like the GPIO or keep the device cool. 

case internals

The internal design is reasonably solid, giving good access to the GPIO header, and we have the introduction of an active fan cooler. We also have a small heatsink to apply to the processor to help wick that heat away, but as we observed, just why do we have a dedicated heatsink which attaches to more components, but the case doesn't appear to be designed for this?

Well in typical use the Raspberry Pi is probably fine with this setup, having the smaller heatsink and an active fan is likely more than enough if you're sitting with using the device as a desktop computer replacement or you're fiddling with your bits on the GPIO and bit-banging away, but if you want to do a bit more heavy lifting then you're likely going to need that more dedicated heatsink, and you will probably remove this secondary internal fan. 

I think they possibly missed a trick without having a vent on the lid, if you want to keep your Pi cool, you're going to have that lid off most of the time because it impedes airflow and that might affect how fast your Raspberry Pi 5 runs, but ultimately we know that it will be perfectly safe and still function, even with it on, because of the smart way in which the device will scale back its speed to accommodate the temperature requirements.

I may just have to alter that fan header to see if I can run both at once though, it's a common 'hack' used on desktop computers, maybe it will apply here!

How will you use your Raspberry Pi 5?

HATS off, HATS on? Or will you have it sat with the lid on, coding away? What modifications do you want to do to the cooling of the Pi 5? Have you seen any other, custom coolers yet?

I'd be interested in knowing your thoughts.

  • Sign in to reply
  • Cancel
  • anniel747
    anniel747 over 2 years ago in reply to beacon_dave

    Blower.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago

    These cases are not bad (they are Seeed ones, I think CPC sells them).

    image

    I have a few of these (in a blue variant) they can be run with the lid off (it is magnetically attached clear acrylic top) but there's lots of space inside for a HAT and probably even larger fan or blower, two of the sides are removable thin plastic sheets (a bit of an achilles heel, they should be slightly thicker). Also has plugged holes which are perfect for SMA etc. I fitted a Pi camera in an enlarged hole on the side. Kind of handy for rapidly testing out image based stuff! I tuned the little lens on it it for a slightly closer range, since I'm using it as a test camera. The default Pi enclosure isn't ideal for such add-ons, whereas this one is roomy.

    Also for the flashing LED enthusiasts, you can illuminate the insides by sticking LED strip to the inside of the acrylic top : ) (There is a large black border which hides the strips completely from view, so just the light output is seen. I did that to illuminate in white, but to blink red whenever there is LoRaWAN activity. Not completely figured that out yet, but the LEDs look great!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 2 years ago in reply to michaelkellett
    michaelkellett said:

    You're quite right. My look at it was too cursory !

    Hah so was mine, sorry about that,

    beacon_dave said:
    Would expect an exit port on one side facing the heatsink.

    I've rescinded my statement.

    dougw said:
    but you can at least see the left side is not one continuous panel

    You're right Slight smile

     RE: The Raspberry Pi 5 Case and Active Cooler are available for some, how do they look? 

     image

    As an apology, here's a nice, clearer photograph.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 2 years ago in reply to cstanton

    Nice clear photo.

    No question about the exit port now. Slight smile

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 2 years ago in reply to beacon_dave

    It doesn't appear to help significantly.

    The heat simply sits on the fin portion of the heatsink with little to no active air going over it.

    We can see this in the following photos, where the case absorbs the heat, it's nearly the same as internally:

    image

    The camera doesn't quite align the heat pattern that well, but you can get the idea. The plastic of the lid is taking all of the heat, much of it is not flowing out of the gap at all.

    Here's the underside:

    image

    That's the SDCard taking the heat at 52.2degC because it's all collected in the thermal mass of the heatsink

    and if we flip the case off

    image

    Again, not aligned well, but we can see the centre of the fan is hot, but not as hot as the fins which is the same temperature as the SDCard. I would have hoped for more heat coming out/through the fan or at least some inclination that it was cooler near the 'blower' of the fan, and it simply isn't.

    If anything, I would suggest that the 'blower fan' is pulling heat up off the processor, and dumping it into the fins. Or perhaps the heatsink should be partly covered, to encourage the air to actually flow across the fins, even though they're not aligned with the direction of the air flow.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 2 years ago in reply to cstanton

    To see if the vent is working, try taping it closed and measure the difference in temperature and heat signature.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 2 years ago in reply to dougw

    I can take more thorough measurement comparisons, the vent will be relieving some heat, however, I can say with certainty that with the lid closed, versus 'cracked open' or off, the fan is audibly quieter when the lid is not pushed on.

    This is in line with comparisons already made

    image

    Though this chart doesn't appear to show "active cooler with blower with fan case, with lid, and without lid"

    My concern is more that we have a static heat mass which is heating other components.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 2 years ago in reply to dougw

    I recall the video mentioning that the size of the lid vent was matched to the air flow through the blower, however it looks like some air will try to exit through that same vent as it doesn't have a more direct exit route out through the side of the case.

    A paper test would likely tell if the vent is sucking or blowing air at various points.

    Due to the design of the heatsink, some of the first fins will probably be directing the airflow from the blower up to the lid.

    Need a translucent case, a high speed camera and a canned smoke test.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • anniel747
    anniel747 over 2 years ago in reply to cstanton

    The fins are not oriented correctly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<