Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Configuring a WiFi Access Point using Raspberry Pi..... How To with the new kernel
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 11 replies
  • Answers 1 answer
  • Subscribers 698 subscribers
  • Views 19846 views
  • Users 0 members are here
  • access point
  • raspberry pi os bookworm
Related

Configuring a WiFi Access Point using Raspberry Pi..... How To with the new kernel

colporteur
colporteur over 2 years ago

The latest upgrade of Raspberry Pi OS Release date: October 10th 2023 Debian version: 12 (bookworm) breaks the solution I have used for creating an AP on a Raspberry Pi. It relies on configurations in /etc/dhcpcd.conf

The release notes tells the tale.

NetworkManager used instead of dhcpcd as networking interface; various changes made to networking plugin to support this

If anyone has any insight on configuring an AP on the new release I appreciate the insight.

I will continue looking to find a configuration that works.

  • Sign in to reply
  • Cancel
Parents
  • colporteur
    0 colporteur over 2 years ago

    Talking to myself, not a good thing.

    Here is what I have discovered so far.

    A fresh install of Raspberry Pi OS Desktop bookworm followed by the string of commands, will create an AP that I can connect to and surf the internet. 

    sudo apt update
    sudo apt upgrade
    sudo nmcli con add type wifi ifname wlan0 mode ap con-name accesspoint ssid "hotspot" autoconnect true
    sudo nmcli con modify accesspoint 802-11-wireless.band bg ipv4.method shared ipv4.address 192.168.6.1/24
    sudo nmcli con modify accesspoint ipv6.method disabled
    sudo nmcli con modify accesspoint wifi-sec.key-mgmt wpa-psk
    sudo nmcli con modify accesspoint wifi-sec.psk "hotspot1234"
    sudo nmcli con up accesspoint

    I can't take credit for the answer, the bulk of the heavy lifting was provided through these articles.

    www.baeldung.com/.../nmcli-wap-sharing-internet
    forums.raspberrypi.com/viewtopic.php


    That being said I still have an unanswered question. The AP distributes IP Addresses to hosts that connect using addresses from the same IP Pool of it's own address. 

    How is the DHCP pool determined? That I don't have an answer for at the moment.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • obones
    0 obones over 2 years ago in reply to colporteur

    You have to distinguish "dchpcd" and "dhcpd".
    The former has an additional "C" in its name which stands for client. This is the part that is responsible for asking around what IP your raspberry should use when connected to a network.
    This has been replaced by NetworkManager in recent distributions because it can handle a lot of other cases.

    The latter is a DHCP server which keeps track of requests made to it for IP address attribution. It listen on network interfaces for specific messages (DHCPREQUEST) and answers them properly. Its configuration is in /etc/dhcpd.conf and you will find inside it the definition for "subnets" into which there are the IP ranges associated with any given interface.

    Note that "dhcpd" is not the only DHCP server available, nowadays, it is often replaced by DNSMasq which despite its name does not limit itself to DNS handling but also to DHCP management. A frequent situation where DNSMasq is used is in conjunction with PiHole where it is embedded in the solution.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • obones
    0 obones over 2 years ago in reply to colporteur

    You have to distinguish "dchpcd" and "dhcpd".
    The former has an additional "C" in its name which stands for client. This is the part that is responsible for asking around what IP your raspberry should use when connected to a network.
    This has been replaced by NetworkManager in recent distributions because it can handle a lot of other cases.

    The latter is a DHCP server which keeps track of requests made to it for IP address attribution. It listen on network interfaces for specific messages (DHCPREQUEST) and answers them properly. Its configuration is in /etc/dhcpd.conf and you will find inside it the definition for "subnets" into which there are the IP ranges associated with any given interface.

    Note that "dhcpd" is not the only DHCP server available, nowadays, it is often replaced by DNSMasq which despite its name does not limit itself to DNS handling but also to DHCP management. A frequent situation where DNSMasq is used is in conjunction with PiHole where it is embedded in the solution.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • colporteur
    0 colporteur over 2 years ago in reply to obones

    dnsmasq is not installed in the Raspbian OS (bookworm).

    The modifications to /etc/dnsmasq.conf

    interface=wlan0

    dhcp-range=192.168.4.2,192.168.4.20,255.255.255.0,24h

    That enabled a DHCP IP range is not longer available.

    I do have it working using the nmcli commands provided. I just haven't determine (if even possible) how to set the DHCP IP pool range that the AP uses.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • obones
    0 obones over 2 years ago in reply to colporteur

    If dnsmasq is not installed, then it's most likely dhcpd that is available. In that case, the configuration is inside /etc/dhcpd.conf where you find subnet definitions like this:

    subnet 10.10.10.0 netmask 255.255.255.0 {
            authoritative;
            range 10.10.10.100 10.10.10.199;
            option domain-name-servers 10.10.10.254;
            option subnet-mask 255.255.255.0;
            option routers 10.10.10.254;
    }

    Here, I'm telling the DHCP daemon that for the interface plugged to network 10.10.10.0/254 it should act as an authoritative DHCP server and provide an IP between 100 and 199 (inclusive)

    Maybe you have something similar in your case.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colporteur
    0 colporteur over 2 years ago in reply to obones

    I found this note in Debian Network Manager docs for bookworm.

    NetworkManager will override dhcp settings, overwriting resolv.conf even if you've configured DNS in /etc/dhcp/dhclient.conf.....

    I can't find in the Raspberry Pi OS bookworm any dhcp configuration files or services under systemd in the default install. I tried loading dnsmasq, dhcpd, isc-dhcp-server and dhcpcd5 in search of solution. I never got any of them working.

    I found no working docs on setting up a DHCP server for bookworm. Working in the sense I couldn't get it working. I did find some posts as early as three weeks ago making reference to networking services and staying with bulleye until a resolution is forthcoming. 

    Over a forty year career in technology, I played with NetworkManager while bouncing between different flavours of Linux. It now appears to have tentacles into a number of network services. I think being on the cusp of the OS change also makes it more difficult.

    It is a bit of system administration nostalgia. I recall the seismic shift from Solaris 5.6 to 5.10. The hue and cry from the Solaris purist. I cut my administration baby teeth on Linux and learned Solaris after but was never really comfortable with it. The x486 stuff in Solaris seemed familiar. Talking to the SPARC crowd I was a heathen.