Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum A new RPI Pico in the works?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 698 subscribers
  • Views 5469 views
  • Users 0 members are here
Related

A new RPI Pico in the works?

scottiebabe
scottiebabe over 2 years ago

Eben Upton Hints at an RP2040 Successor, Promises a Raspberry Pi Compute Module 5 in 2024

"We know what people don't like [and] what people do like," Upton says, "and we have a chip team."

I will call a spade a spade and say the sleep current of the RP2040 @ 1 mA is atrocious. I sincerely hope they improve the sleep current.

I think the QSPI memory controller could be improved as well.

Maybe more PIO memory...

But I don't have that many criticism about the pico.. 

Does the pico have any sore points for you?

  • Sign in to reply
  • Cancel
Parents
  • baldengineer
    baldengineer over 2 years ago

    To me, it is very clear the RP2040 was an MVP for their first microcontroller.

    There are a lot of great features: dual-core, interpolator, PIO (obviously my favorite), and the robust C SDK. That said, there is no encryption for an external flash, no internal flash, limited internal SRAM, terrible sleep modes, a QFN-only package, maxing out at USB FS, a less-than-stellar ADC, etc.

    I don't think it was ever intended to be incorporated into a volume end-product other than boards like the Pico, where the RP2040's feature set works very well.

    Overall, I'm a fan of the chip. I've got an upcoming project that uses it (well two of them) because of the PIO. And I've probably designed about a dozen boards around it now.

    Regarding the Pico: the lack of a reset button really, really irritates me.

    Also, I hate that the Pico doesn't have a reset button.

    So, along those lines, I think it'd be great if a new Pico came with a reset button.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • baldengineer
    baldengineer over 2 years ago

    To me, it is very clear the RP2040 was an MVP for their first microcontroller.

    There are a lot of great features: dual-core, interpolator, PIO (obviously my favorite), and the robust C SDK. That said, there is no encryption for an external flash, no internal flash, limited internal SRAM, terrible sleep modes, a QFN-only package, maxing out at USB FS, a less-than-stellar ADC, etc.

    I don't think it was ever intended to be incorporated into a volume end-product other than boards like the Pico, where the RP2040's feature set works very well.

    Overall, I'm a fan of the chip. I've got an upcoming project that uses it (well two of them) because of the PIO. And I've probably designed about a dozen boards around it now.

    Regarding the Pico: the lack of a reset button really, really irritates me.

    Also, I hate that the Pico doesn't have a reset button.

    So, along those lines, I think it'd be great if a new Pico came with a reset button.

    • Cancel
    • Vote Up +4 Vote Down