Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum RPi 5 USB C PD
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 13 replies
  • Subscribers 695 subscribers
  • Views 6413 views
  • Users 0 members are here
Related

RPi 5 USB C PD

WA9ONY
WA9ONY over 2 years ago

I there a way to check the RPi 5 to see what USB C PD and USB C Emarker cable configuration is being used?

I believe if the USB C cable does not have a Emarker, the USB C PD current level will be limited to max 3A and to max 20V.

Therefore, using a USB C cable with no Emarker will result in a USB C PD being limited to 3A even if it can supply 5A.

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 2 years ago

    Most Pi models in the past have never been fully standards compliant on their USB power connector, I doubt the Pi 5 will be either. There are flaws in this area in pretty much every one of their models, it wont change, it's embedded in their corporate culture. To save risk of incompatibility, you may as well bite the bullet and purchase the official Pi power supply which offers up the full 5A. 

    Otherwise, its just an expense buying a special cable and a USB-C PD charger that supports that high current, it can be close to $100 for a decent charger and cable. The Pi official charger is cheap in comparison. Granted one may already have a phone charger, but I think if you need the max power, then the only thing that will be supported is that official Pi supply, and all bets are off if any other charger is used. Thats just from experience with the general unreliability of previous Pi models when the official power supply was not used. Also guaranteed each time one has a problem with the Pi, people will ask "are you using the official power supply?".

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 2 years ago

    Most Pi models in the past have never been fully standards compliant on their USB power connector, I doubt the Pi 5 will be either. There are flaws in this area in pretty much every one of their models, it wont change, it's embedded in their corporate culture. To save risk of incompatibility, you may as well bite the bullet and purchase the official Pi power supply which offers up the full 5A. 

    Otherwise, its just an expense buying a special cable and a USB-C PD charger that supports that high current, it can be close to $100 for a decent charger and cable. The Pi official charger is cheap in comparison. Granted one may already have a phone charger, but I think if you need the max power, then the only thing that will be supported is that official Pi supply, and all bets are off if any other charger is used. Thats just from experience with the general unreliability of previous Pi models when the official power supply was not used. Also guaranteed each time one has a problem with the Pi, people will ask "are you using the official power supply?".

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • WA9ONY
    0 WA9ONY over 2 years ago in reply to shabaz

    Great information. 

    Is there RPi 5 status information telling what is the status of the USB C PD and cable being used?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago in reply to WA9ONY

    If there is, it may be documented in blogs, YouTube videos, etc. eventually, as users explore the code and the hardware, under a microscope (some even X-ray it!).

    They rely on the community of users for support and documentation mostly, because it saves them millions of $ per year (their words, not mine). Unless there's better documentation, USB-PD monitor tools can be used to see what voltage and current are being supplied (this will work with all USB-C devices). They cost around $30 USD. I use this one, it's not bad (I didn't spend a lot of time researching it when I bought it, so there may be much better ones for the price too, but it seems to work fine):

    image

    But, as mentioned, I don't think it's worth the effort to use a USB charger for reliability reasons (at least with earlier Pi models, the official power supplies didn't supply 5.0V, they were designed to supply a voltage right at the edge of the tolerance). Who knows what unusual stuff they've had to do with the Pi 5 official supply : (

    Personally, I'm not planning to use the Pi 5 for at least 6 months or so, until others have discovered issues or tricks/tips. Especially if the Pi 5 is required for additional hardware (the drivers will have differences for a lot of add-ons). I think the best advice is to use a known working Pi 3 or Pi 4, and only use a Pi 5 if it's necessary because it is fairly well established by now how to power the Pi 3 and Pi 4 if official power supplies are not used.

    Even between Pi 3 and Pi 4, there is some hardware that won't work on Pi 4 but will work with Pi 3, because drivers are different between those models too.