Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Wiring pi is defunct.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 14 replies
  • Answers 1 answer
  • Subscribers 697 subscribers
  • Views 6367 views
  • Users 0 members are here
  • c
  • gpio
  • wiringpi
  • raspberry_pi
  • raspberry-pi
  • raspberrypi
Related

Wiring pi is defunct.

SensoredHacker0
SensoredHacker0 over 2 years ago

I used to love using the Wiring Pi library in C for programing the IO of the Raspberry pi.
I haven't used a PI for a project in a while, and I guess in that time developer of WiringPi has
stopped supporting the library.
I tried using version 2.52 on a raspberry pi 4, but it says something like the hardware isn't listed in /proc/cpuinfo.

So I guess I cant use wiringPi. what C libraries would you use for programing GPIO in C on a rasperry Pi 4?
Ive looked around the internet, and I see some various options, but Im not sure what code works with which boards, etc.

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 2 years ago

    WiringPi certainly does work with Pi 4, I have used it myself on Pi 4. 

    However, it is not maintained (the author doesn't wish to maintain it anymore), so it won't work with Pi 5 at all (unless someone adapts it, which the original author I think doesn't have an interest in pursuing). There is a list of alternatives (some are for Python, but there are some listed for C) here: https://raspberrypi.stackexchange.com/questions/117591/controlling-raspberry-pi-gpio-with-c-and-python

    However, I've not tried any alternative personally on Pi 4. With C, I've only used WiringPi on Pi 4.

    I suspect some people (those that need it for, say, a job and thus have the time - several days of effort to do it properly) are directly programming registers (i.e. do a mmap, followed by writing/reading the registers that are mapped) for the particular Pi they are using, and effectively creating their own API. I've had to do that myself on some platforms (e.g. BeagleBone Black), but it's a lot of effort to initially do, and to maintain. 

    In summary, if it's only Pi 4 that interests you, and you wish to use C programming, then WiringPi should work. Otherwise, if you may eventually want Pi 5 support too, you'd need to choose a different library (e.g. pigpio, but there are various options at that link), which today may not work for Pi 5 but at least has a chance of being supported eventually, if it is actively being maintained currently, or create your own.

    If you don't need fast GPIO, then there are other options (e.g. using /sys/class/gpio) but those are slower. Not every application will need speed, so that may be a possibility. 

    Yet another possibility is to use SPI or I2C (e.g. SPI or I2C GPIO expander) and avoid the WiringPi and its alternatives altogether since you'd be using the normal Linux i2cdev or spidev API, which will always be supported (unless something better comes along one day).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • BigG
    0 BigG over 2 years ago in reply to shabaz

    Here's yet another, more generic, C programming option for Linux, which looks to be quite active in development but is not found in that list. Have yet to test performance...

    github.com/.../c-periphery

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago in reply to BigG

    Nice find. Regarding your performance comment, I think for general I/O they have a wrapper around /sys/class/gpio, so it won't be super-fast, but most users just want a wrapper anyway, with a simple API, so it should still be fine for a lot of purposes.

    I'm currently writing a direct register access API for a different board that I need to use, it's going to be basic because I don't wish to maintain something complex. but I wish SBC manufacturers had standardized on a way to make it simple for C/C++ developers to use fast access without having to delve into tech ref manuals, e.g. some C/C++ API framework and a config file that was tailored for the processor/SBC.  I wish raspberrypi.com had taken the initiative and come up with something like a framework that any SBC supplier could use to implement GPIO with the same underlying API calls. That way, people could modify apps to suit Pi 5, 6, etc or other manufacturer boards too.

    A few things that would be useful for that would be the ability to write an API on top (such as DigitalIn/DigitalOut for those who want an Arduino-style API), plus the ability to map different identifiers. For instance, if a different SBC used completely different GPIO pins, it would be good if they could be mapped to Pi GPIO numbers (if people were porting code), or even map to physical pin numbers if desired. Lots of SBCs have a 40-way connector, but of course, the registers will be different.

    Also, as well as C++, such a library would also be linkable to C code (since some legacy stuff might not compile as C++ without a load of errors).

    All that, plus maintaining it, is quite some work for an individual, but a nice constrained, not-insurmountable uni project for a sponsored student for raspberrypi org etc.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 2 years ago in reply to shabaz

    I'm checking out the memmap register access on the RPi. To test if I can plug in another implementation in the little oo lib I made. Got sidetracked by LoRaWAN things Grin

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Jan Cumps
    0 Jan Cumps over 2 years ago in reply to shabaz

    I'm checking out the memmap register access on the RPi. To test if I can plug in another implementation in the little oo lib I made. Got sidetracked by LoRaWAN things Grin