Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum What Are My Options for Secure, Non-Permanent Raspberry Pi GPIO Connections?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 698 subscribers
  • Views 1883 views
  • Users 0 members are here
  • gpio
  • raspberry pi 4
  • raspberrypi
Related

What Are My Options for Secure, Non-Permanent Raspberry Pi GPIO Connections?

JunkMuffler
JunkMuffler over 2 years ago

I'm working on a project that utilizes a Raspberry Pi. It's a semi-permanent thing, but I want to be able to easily remove the Pi and use it for other projects if need be. They aren't exactly the easiest or cheapest things to get. This is a RPi 4-b.

My original plan was a 40 pin ribbon cable that went to a piece of proto board. There's a few problems with that:

  • I need to deliver power to the pi via GPIO. I'm not sure if the ribbon cable can handle the Pi's power draw. Especially since I'm connecting an external display via DSI.
  • I'm putting a fan in the case, which means I'd have to run additional cabling to the fan somehow, either back from the other end of the ribbon cable or from the power supply.

In a perfect world I'd like to pop off the ribbon cable and DSI connector, unscrew the Pi from its mount, and then swap out the SD card. However given the circumstances I'm not confident that's feasible. Thoughts?

  • Sign in to reply
  • Cancel
  • Jan Cumps
    0 Jan Cumps over 2 years ago
    JunkMuffler said:
    I need to deliver power to the pi via GPIO. I'm not sure if the ribbon cable can handle the Pi's power draw

    2 pins of the connector are tied to 5V Power. 2 and 4. That means that you have 2 wires available in your ribbon. Double current

    Because 2 and 4 are not next to each other in the ribbon, they are not one single heat source. There's a cooler wire (3) in between them.

    related: 3M Technical Brief: Current Ratings of Common 3MTM Flat Ribbon Cables

    Belden rates their 28 AWG (7x36) Tinned Copper cables 1A per conductor at 20°C: https://www.belden.com/products/Cable/Electronic-Wire-Cable/Flat-Ribbon-Cable/9R28016

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • JunkMuffler
    0 JunkMuffler over 2 years ago in reply to Jan Cumps

    Thank you for the response and the links! Sounds like I can just roll with the ribbon cable. The technical brief was really useful. :)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • JunkMuffler
    0 JunkMuffler over 2 years ago in reply to Jan Cumps

    Actually, taking a second look it appears that the Pi 4b draws 3 amps of power. So I can only send 2 amps of power via a ribbon cable. Looks like I need to find another option, or just use a separate power block.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 2 years ago in reply to JunkMuffler

    It 'll be 3 A peak current.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colporteur
    0 colporteur over 2 years ago

    Will the Pi be networked?

    If yes, I suggest PoE. There are a few reviews in the community exploring that solution.