Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum OpenCM 9.04 or Poppy Pixl Board - to control XL320 Motors
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 700 subscribers
  • Views 650 views
  • Users 0 members are here
  • poppy
  • raspberry_pi
  • opencm
Related

OpenCM 9.04 or Poppy Pixl Board - to control XL320 Motors

pip77
pip77 over 2 years ago

Hello everyone,

I want to control 5x Dynamixel XL-320 motors for a project i started (it have to be these motors, due to the design and properties etc.).
The basis should be an RPi3B, RPi3B+ or RPi4, depending on the possibilities.

Here are the two options that I have found as driver boards:
- Poppy Pixl Board: can control up to 6 pcs. XL-320. These are simply connected "in series". Control via GPIO pins. As far as I could see it, this board can be controlled with max. one RPi3, max. RPI3+.
- OpenCM 9.04: can control up to 4 pcs. XL-320. One port for each motor on the board. Can only be controlled via USB? Would also work with RPi4.

=> does anyone have experience with the boards?

The OpenCM would actually be ruled out, as too few motors can be controlled. Does anyone know whether 2 boards can be controlled with one Pi?
As far as I can see, the Poppy Pixl board is actually only for a specific robot kit. I'm a little worried that the programming would be too limited.
I would like to implement the program and the control generally via Python.

If anyone has experience with both or one of the two boards and could share their knowledge, I would be very grateful.
Many thanks for your help in advance!