Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi Pico 2 MicroPython problem
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 1 answer
  • Subscribers 698 subscribers
  • Views 3631 views
  • Users 0 members are here
  • coding
  • graphics
  • pico 2
  • micropython
  • .uf2
Related

Raspberry Pi Pico 2 MicroPython problem

tonygo
tonygo over 2 years ago

I've got hold of the new Pico 2 and have tried a graphics program to make use of the extra memory. I'm using a Waveshare 2" Pico display with 320 by 240 pixels and the latest available MicroPython uf2 (v1.24.0-preview.201.g269a0e0e1 (2024-08-09) .uf2) and have hit a snag. The Waveshare display driver is included in the code and works perfectly.

To get this loop to terminate I have to include an 'unnecessary' print statement.

for i in range(r, 0, -1):
    print(i) # <==================== WHY IS THIS NEEDED? ==================
    LCD.ellipse(centre_x, centre_y,i+1, i+1,colour(i*5,i*3,i*4), 1)
    LCD.show()
    time.sleep(0.1)
    

If I leave it out the Pico 2 locks up at the end of the loop and if I click on the STOP icon in Thonny I get the message:


Unable to connect to COM3: could not open port 'COM3': PermissionError(13, 'Access is denied.', None, 5)

If you have serial connection to the device from another program, then disconnect it there first.

Process ended with exit code 1.


If I include the print statement it runs through to the following code as expected.

The full code can be found here:
https://pastebin.com/Fmk5iQ18

I wonder what is going on.

I know this is a 'preview' version of the UF2 but I was not expecting a problem with a counted for loop! Any ideas?

  • Sign in to reply
  • Cancel
  • tonygo
    0 tonygo over 2 years ago

    Works OK with:

    for i in range(r, 1, -1):
    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago

    It looks like this is the PR that implements MicroPython for Pico 2:

    https://github.com/micropython/micropython/pull/15619

    It may be worth leaving the detail there, so that the developer can check it out (otherwise it might not get resolved as quickly, until someone raises it as an issue).

    That PR is still really fresh (just three days old) so unfortunately the issues you encounter are probably not experienced by others yet.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tonygo
    0 tonygo over 2 years ago in reply to shabaz

    You can follow the problem discussion here:

    Raspberry Pi Pico 2 · micropython · Discussion #15621 (github.com)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • JWx
    0 JWx over 2 years ago

    maybe it is some timing issue if print can be used as workaround? I wonder if replacing print with sleep would be equally effective...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tonygo
    0 tonygo over 2 years ago in reply to JWx

    # Colour Mixing Routine
    def colour(R,G,B): # Compact method!
    mix1 = ((R&0xF8)*256) + ((G&0xFC)*8) + ((B&0xF8)>>3)
    return (mix1 & 0xFF) *256 + int((mix1 & 0xFF00) /256) # low nibble first
    
    # ==== Main ====
    pwm = PWM(Pin(BL))
    pwm.freq(1000)
    pwm.duty_u16(32768)#max 65535
    
    LCD = LCD_1inch3()
    
    LCD.fill(LCD.WHITE)
    LCD.show()
    
    '''
    # Set up buttons
    key0 = Pin(15,Pin.IN,Pin.PULL_UP)
    key1 = Pin(17,Pin.IN,Pin.PULL_UP)
    key2 = Pin(2 ,Pin.IN,Pin.PULL_UP)
    key3 = Pin(3 ,Pin.IN,Pin.PULL_UP)
    '''
    centre_x =int(LCD.width/2)
    centre_y = int(LCD.height/2)
    R = int((LCD.width + LCD.height)/4)
    r = int((LCD.width + LCD.height)/8)
    LCD.fill(0)
    LCD.show()
    
    LCD.ellipse(centre_x, centre_y,R,r,colour(255,255,0),1)
    LCD.show()
    LCD.ellipse(centre_x, centre_y,r,r,colour(0,0,255))
    LCD.show()
    
    for i in range(r, -1, -1):
    
        LCD.ellipse(centre_x, centre_y,i+1, i+1,colour(i*5,i*3,i*4), 1)
        LCD.show()
        time.sleep(0.1)
    
    time.sleep(1)
    LCD.fill(0)
    LCD.show()
    
    gc.collect
    print()
    print(gc.mem_free())

    There is already a time.sleep(0.1) in the loop. It did not help.

    If I comment out the button/key setup lines it works properly.

    I also tried the same code, with button setup lines on a RP2040 Pico Lipo and it works correctly.

    I think it is the UF2 for the Pico 2 causing the problem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • JWx
    0 JWx over 2 years ago in reply to tonygo

    Hello! 

    if it seems to hang consistently at the end of the loop, have you tried running standalone

    LCD.ellipse(centre_x, centre_y, 2, 2,colour(2*5,2*3,2*4), 1)

    (the last value of problematic range(r, 0, -1))

    (but it will probably succeed if print in the loop remedies it).

    It is strange that it seems to be connected with certain value (when range(r, 1, -1) is ok) and timing/whatever at the same time (when print can be used as a workaround)...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tonygo
    0 tonygo over 2 years ago in reply to JWx

    I do not think it is my loop. If I comment out the Button setup lines it works perfectly even with 

    for i in range(r, -1, -1):

    controlling the loop.

    I've run the full code, including the button setup, with a Pimoroni Pico Lipo (RP2040) and it works perfectly. You are supposed to be able to just substitute a Pico 2 for a Pico 1 and the same code should work.

    I think the new Pico 2 .UF2 is the problem.

    Once again the hardware is available ahead of the essential software as a proper release is not yet available. The current version is a preview (9th Aug 2024).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • JWx
    0 JWx over 2 years ago in reply to tonygo

    Hello! I was not suggesting it is something in the code, only wanted to identify the precise point/conditions when the hang happens Slight smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • paulkevin
    0 paulkevin over 1 year ago
    [deleted]
    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tonygo
    0 tonygo over 1 year ago in reply to paulkevin

    Thank you, I will give it a try.