Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi 4 not responding. Only shows RED light. No green light
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 21 replies
  • Subscribers 702 subscribers
  • Views 10106 views
  • Users 0 members are here
  • raspberry_pi
  • noboot
Related

Raspberry Pi 4 not responding. Only shows RED light. No green light

bugtech
bugtech over 1 year ago

Hi. 

I was working on my newly bought Raspberry pi 4. Suddenly after shutting it down to remove the camera cable, It is not responsive anymore. I have read various posts regarding this issue but no help. 

I have tried 3 different SD cards but still its not responding. What can be the issue? or how can i fix this? 

Thank you 

  • Sign in to reply
  • Cancel
Parents
  • cstanton
    0 cstanton over 1 year ago

    Hi bugtech 

    bugtech said:
    Suddenly after shutting it down to remove the camera cable, It is not responsive anymore. I have read various posts regarding this issue but no help. 

    That's unfortunate.

    bugtech said:
    I have tried 3 different SD cards but still its not responding

    Do you have another computer where you can check the SDCards? Ideally a Linux computer. There's a handy command called 'f3probe' that can check the status of the sdcard which may be useful for you here.

    bugtech said:
    What can be the issue?

    The problem either resides with the sdcard, the raspberry pi power circuitry, or the power supply you're using.

    bugtech said:
    I am using a 5V type C power adapter. 

    Is it a Raspberry Pi power adapter?

    Does it try to negotiate USB-PD? (I believe the Pi 4 doesn't support this)

    Does it provide at least 5v at 2a?

    Have you tested it with another device?

    Do you have another one that you can test with?

    Do you have a bench power supply that can provide 5v at 2a? A good way to test the Raspberry Pi can be to connect to the 5v and ground pin on the Pi ( Raspberry Pi 4 Model B Default GPIO Pinout with PoE Header ) if you have a controlled power source to see if it can boot from the GPIO pins.

    bugtech said:
    There is no sign of Green light.

    Are there any signs of any lights?

    If by chance you have the opportunity to use a thermal camera, you could try using it on the board to see if any components show heat when you apply power.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • cstanton
    0 cstanton over 1 year ago

    Hi bugtech 

    bugtech said:
    Suddenly after shutting it down to remove the camera cable, It is not responsive anymore. I have read various posts regarding this issue but no help. 

    That's unfortunate.

    bugtech said:
    I have tried 3 different SD cards but still its not responding

    Do you have another computer where you can check the SDCards? Ideally a Linux computer. There's a handy command called 'f3probe' that can check the status of the sdcard which may be useful for you here.

    bugtech said:
    What can be the issue?

    The problem either resides with the sdcard, the raspberry pi power circuitry, or the power supply you're using.

    bugtech said:
    I am using a 5V type C power adapter. 

    Is it a Raspberry Pi power adapter?

    Does it try to negotiate USB-PD? (I believe the Pi 4 doesn't support this)

    Does it provide at least 5v at 2a?

    Have you tested it with another device?

    Do you have another one that you can test with?

    Do you have a bench power supply that can provide 5v at 2a? A good way to test the Raspberry Pi can be to connect to the 5v and ground pin on the Pi ( Raspberry Pi 4 Model B Default GPIO Pinout with PoE Header ) if you have a controlled power source to see if it can boot from the GPIO pins.

    bugtech said:
    There is no sign of Green light.

    Are there any signs of any lights?

    If by chance you have the opportunity to use a thermal camera, you could try using it on the board to see if any components show heat when you apply power.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • bugtech
    0 bugtech over 1 year ago in reply to cstanton
    cstanton said:

    Is it a Raspberry Pi power adapter?

    Yes it is a Raspberry Pi adapter. It worked fine for a week. 

    cstanton said:

    Does it provide at least 5v at 2a?

    Yes!

    cstanton said:

    Have you tested it with another device?

    Yes it works fine with Jetson. 

    cstanton said:
    Do you have a bench power supply that can provide 5v at 2a? A good way to test the Raspberry Pi can be to connect to the 5v and ground pin on the Pi ( Raspberry Pi 4 Model B Default GPIO Pinout with PoE Header ) if you have a controlled power source to see if it can boot from the GPIO pins

    Yes it shows very dim red and green light. and the IC gets too hot with it. 

    cstanton said:
    Are there any signs of any lights?

    With Type  C power. It shows only solid RED light. No sign of GREEN light. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cstanton
    +1 cstanton over 1 year ago in reply to bugtech
    bugtech said:
    Yes it shows very dim red and green light. and the IC gets too hot with it. 

    Sounds like a fundamental component has shorted out, unfortunately.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • bugtech
    0 bugtech over 1 year ago in reply to cstanton

    Yes thought so.

    Thanks for your response!