Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Automatic overriding of configuration file in Raspberry Pi 2
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 706 subscribers
  • Views 758 views
  • Users 0 members are here
  • frontpage
  • raspberry_pi
Related

Automatic overriding of configuration file in Raspberry Pi 2

e14 Contributor
e14 Contributor over 10 years ago

Can config.txt file be overridden automatically during boot time? For HDMI and RCA cables we need different types of resolutions and there will be difference in audio configuration too. I want the config.txt file be overridden and loaded automatically at the time of booting and display features as per HDMI or RCA connections. Is it possible?

  • Sign in to reply
  • Cancel
Parents
  • rew
    rew over 10 years ago

    How do you want the override to happen? Keyboard input? Automatic detection of HDMI monitor?

     

    You could write code that does that, and chooses between two variants of the config.txt depending on the presence of an HDMI monitor. This code would run on the graphics core: No compiler available, no specs, nothing.

     

    What you could do is to have two config.txts: config.txt.hdmi, config.txt.rca and early in the boot process, if you detect you've been booted with the RCA config.txt, AND there is an HDMI monitor connected, you copy config.txt.hdmi to config.txt, and reboot. And of course the other way around.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rew
    rew over 10 years ago

    How do you want the override to happen? Keyboard input? Automatic detection of HDMI monitor?

     

    You could write code that does that, and chooses between two variants of the config.txt depending on the presence of an HDMI monitor. This code would run on the graphics core: No compiler available, no specs, nothing.

     

    What you could do is to have two config.txts: config.txt.hdmi, config.txt.rca and early in the boot process, if you detect you've been booted with the RCA config.txt, AND there is an HDMI monitor connected, you copy config.txt.hdmi to config.txt, and reboot. And of course the other way around.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to rew

    How can I detect that it has been booted with RCA config.txt?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 10 years ago in reply to e14 Contributor

    I would grep on fbheight=... in /proc/cmdline It is bound to be different for your RCA configuration. (probably 576 or something, a resolution I don't expect from an HDMI monitor).

     

    With tvservice -d you can try to dump the edid data of the monitor, if that works, you probably have something connected...  OK. I just tested that for you. My raspberry pi seems to remember the last monitor that it has seen. It happily dumps the EDID data of a monitor that is now connected to my other 'pi of which I pulled the power plug.

     

    You'll have to look around for a trick to actually communicate with the monitor to detect the monitor.