Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi 5 randomly reboots when powering an SSD over USB
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • +1 person also asked this people also asked this
  • Replies 17 replies
  • Answers 1 answer
  • Subscribers 701 subscribers
  • Views 929 views
  • Users 0 members are here
  • Locale or Language
Related

Raspberry Pi 5 randomly reboots when powering an SSD over USB

italo_ragazzo
italo_ragazzo 1 month ago

I’m using a Raspberry Pi 5 with an NVMe SSD connected through a USB 3 enclosure. The Pi works normally when the SSD is disconnected, but occasionally reboots when the SSD is under sustained read/write load.I purchased this one in Italy, so it might function differently.

The power supply is rated at 27W, and the issue seems more likely to happen when the CPU is also under load. Has anyone seen this with the Raspberry Pi 5, and would using a higher-rated USB-C supply or a powered USB hub be the recommended solution?

Thank you

best,
Salvatore B.
florist Italy
LTC

  • Sign in to reply
  • Cancel
Parents
  • veluv01
    0 veluv01 1 month ago

    I'm using the M.2 HAT+ to access the NVMe SSD (uses around 5W on R/W, running SLM's) , it works without any problem. If the power supply you're using doesn't have the 5V 5A profile, it's also a cause of the issue you're facing.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • veluv01
    0 veluv01 1 month ago in reply to veluv01

    Here's the USB Power Delivery WhitePaper

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • veluv01
    0 veluv01 1 month ago in reply to veluv01

    Here's the USB Power Delivery WhitePaper