Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum How To Autonomous an UAV via gps ?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 709 subscribers
  • Views 2697 views
  • Users 0 members are here
  • raspberry_pi
Related

How To Autonomous an UAV via gps ?

boombo
boombo over 10 years ago

Hello Guys , I am totally new in the embedded system universe  :D

 

I am looking forward to building an autonomous UAV controlled via fixed gps waypoints and if i want to change the route i will be able to take control through ssh or something :)

 

i have read lots of posts about that but i feel it a bit confusing  :roll:

 

if someone who is a patient could tell me how to start and what is the requirements ?

do i really need an autopilot or i just can control servos through raspberry pi directly ?

Overview mechanism ? :cry:

and Thanks :)

  • Sign in to reply
  • Cancel
Parents
  • DAB
    DAB over 10 years ago

    Hi Darken Hero,

     

    The concept is simple, the devil is in the details.

     

    Ideally, you have a UAV that an establish where it is, using GPS or other navigation aids and then orient itself to move to the next waypoint.

     

    As long as the UAV has an unimpeded path, it is a simple matter of maintaining a movement vector to the next point, recognize that you are at that point and then changing your orientation to begin moving to the next point.

     

    The math is simple, the control logic is simple, but maintaining the vehicle safely against things in the environment that could cause it problems is where the problems occur.

     

    Remotely piloted vehicles rely on onboard instruments and forward looking video to provide the operator with information about the current situation around the vehicle so that the operator has plenty of time to avoid problems.

     

    For fully autonomous vehicles, you need to create that onboard situation awareness with sufficient options to avoid catastrophic events.  Good luck with that one.

     

    In a closed course, it is fairly easy to establish safe movement corridors between the way points to safely move the vehicle.

     

    So depending upon what type of vehicle you want to use and the geography in which you want to use it in.

     

    DAB

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • boombo
    boombo over 10 years ago in reply to DAB

    Thanks DAB for you reply ^_^

     

    so i got my raspberry pi , i should get a GPS .. how to set up a fixed route practically  ? 

     

    another question , can i do all the way process with raspberry pi only with GPS or i need an Ardupilot for control and navigation ?

     

    Sorry am a real noob image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 10 years ago in reply to boombo

    Based on the questions you're asking, I can estimate your "level of expertise" with regard to "raspberry pi" as well as "RC model flying". My analysis says: This project is too ambitious for you.

     

    Your project sounds like a challenging project for a group of 5-10 university level electrical and mechanical engineering students..

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to rew

    Hope you are not offending Roger,

     

    a though arose in my mind reading the request of boombo and thinking to all the difficulties he was "searching" by himself. Without forgetting the very good posts on the UAV issues explained and partially solved by screamingtiger during the SciFi Your PI challenge and beyond. I though to one of my preferred citations, that is also my motto: Ció che é pensato esiste (what is though exists) by J.L.Borges ...

    If I was always doing only what was just at my level of expertise (I am not an engineer, but - maybe - a literate instead a philosopher, poet and story-teller, chemistry) I was always asking myself how to power my first AIM65, bought in 1979

     

    Cheers. Enrico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 10 years ago in reply to boombo

    I highly suggest that you go look at all of the posts related to the use of GPS with a Pi to do geolocation.

     

     

    There are lots of information in those posts that show you how to set up the RPi with the GPS so that you can use it to find geolocations.

     

    Once you get that far, come back and I will suggest some next steps.

     

    As Roger said, you are embarking on a very challenging project, so I hope you are not expecting immediate miracles.

     

    There are commercial quadcopters that can do what you want, but I suspect your budget is limited and you are willing to sacrifice your time to extend your budget.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • DAB
    DAB over 10 years ago in reply to boombo

    I highly suggest that you go look at all of the posts related to the use of GPS with a Pi to do geolocation.

     

     

    There are lots of information in those posts that show you how to set up the RPi with the GPS so that you can use it to find geolocations.

     

    Once you get that far, come back and I will suggest some next steps.

     

    As Roger said, you are embarking on a very challenging project, so I hope you are not expecting immediate miracles.

     

    There are commercial quadcopters that can do what you want, but I suspect your budget is limited and you are willing to sacrifice your time to extend your budget.

     

    DAB