Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum PiZero Powered through CRT Components?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 708 subscribers
  • Views 2020 views
  • Users 0 members are here
  • raspberry_pi
Related

PiZero Powered through CRT Components?

rivera82falcon
rivera82falcon over 10 years ago

Greetings all! Long time lurker and love to read everyone's projects, discussions, and debates.

 

I finally picked up a PiZero (camera edition) because I want to recreate the CRT Raspberry Pi project featured here at Element14 with my son (5 year old). This was his idea as I started going around browsing and he hasn't stopped talking about this since image.  Ideally, I'd like to use the circuitry from the CRT to power the Pi so I only have one power cord. I'm using a Sylvania SSC192 which has a VHS player on it. From what I see on the schematics, it looks like there is a 5V point available. Is it safe to solder onto this point and not damage the Pi? I will have an additional switch in place so the Pi doesn't have power running to it 24/7.

 

I appreciate the help here, thank you! image

  • Sign in to reply
  • Cancel
Parents
  • rew
    rew over 10 years ago

    Officially there is a fuse between the power input of the pi and the rest of the pi. By connecting something to an internal 5V point you are circumventing that fuse.
    IMHO that is not that bad. If the power going into the pi is limited the options for big mishaps are similarly limited.

     

    I would personally not solder directly to the pi except to mount the  40 pin header. I would then put a connector of sorts on the header.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fvan
    fvan over 10 years ago in reply to rew

    There is a poly fuse for Pi3 and co, but I thought there wasn't any for the Pi Zero?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 10 years ago in reply to fvan

    You could be very right!..... In that case, the foundation is accepting my view on the issue: there is not much trouble that this fuse would be preventing. :-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rew
    rew over 10 years ago in reply to fvan

    You could be very right!..... In that case, the foundation is accepting my view on the issue: there is not much trouble that this fuse would be preventing. :-)