Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum PI 3 CUSTOM MULTIMEDIA HIGH PERFORMANCE OS IMAGE
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 704 subscribers
  • Views 675 views
  • Users 0 members are here
  • raspberry_pi_space
Related

PI 3 CUSTOM MULTIMEDIA HIGH PERFORMANCE OS IMAGE

rive
rive over 9 years ago

OS Image download link: http://goo.gl/sMGFGv

 

Default login username: pi
Default login password: raspberry

//////////////////////////////////////////////////////////////////////////

//////////////////////////////////////////////////////////////////////////

 

This video is unavailable.
You don't have permission to edit metadata of this video.

 

-----------------------------------------------

----------------------------------------------

For more "CJNK" raspberry Pi videos and 'Howto' Instructionals, visit my Youtube Channel:
https://www.youtube.com/channel/UCtMmE5rczxaWSgqN6w0ZA2A (or search 'CJNK')


DEBIAN JESSIE MULTIMEDIA PERFORMANCE IMAGE RASPBERRY PI 3

Image updated 11/21/16 (rpi3_debian_jessie_4.4.32_customx11.img.bz2 (3.5G))


Screenshots:

VPN: https://s12.postimg.org/5jprzen8t/2016_10_23_162117_1680x1050_scrot.png
Start Menu: https://s12.postimg.org/u6rsivcot/Untitled.png

 

Desktop1: https://s21.postimg.org/vnm6wvwp3/Untitled4556.png
Desktop2: https://s15.postimg.org/e4ywnuw0b/Untitled1.png
Desktop3: https://s15.postimg.org/e4ywnuw0b/Untitled1.png
Desktop4: https://s15.postimg.org/o4lq71o3f/Untitled1.png
Desktop5: https://s18.postimg.org/jwh2dfva1/version.png
Desktop6: https://s16.postimg.org/i1lu6x051/Untitled3.png


================================================================================
================================================================================

The following are recommended for best Pi3 performance:

 

* UHS-1 (or higher)micro sdcard (supports a clock frequency of 100 MHz). For example, 32GB "Samsung EVO+", or 32GB "Sandisk Pixtor" sdcard.

 

* Adequate airflow/cooling with heatsink on SoC, and fan

================================================================================
===============================================================================


CPU: 1.3 GHz ARMv8 (Cortex A53) Quad Core
SDRAM/Memory: 1 GB LPDDR2 1150 MHz
GPU: 1080p HDMI VideoCore IV 500 MHz (192 MB shared memory)
SDCARD: Optimized for UHS Clock frequency of 100 MHz (for faster, improved read/write speeds)

 

WebRTC IP leak Preventor (prevents WebRTC from leaking real IP when running VPN)
Browser TouchVPN  (Selectable browsing from  US, Canada, UK based IPs, etc) Allows cloaked incognito browsing of country restricted sites, and hides real IP.
Bypass geo-restrictions to unblock any website wherever you are. Get access to sites that are blocked or censored by government, school or workplace.

 

Bluetooth Pulse Audio
Updated Raspbian/Debian Jessie on Linux kernel 4.4.32
Custom FOSS DE (desktop environment)
Custom login screen
CUPS/HP Imaging and printing
Deluge Torrent client
Clam Antivirus with Updated GUI ClamTk v5.24
MP3 shuffle player
Omxplayer media mod*
GIMP Image manipulation and editor
Chrome/Chromium Browser v51
Pepperflash and shockwave v23
Pandora Internet radio
Google Play Music
DOS emulator**
extra games
DOS Starflight game
DOS Master Of Orion game
Benchmarking apps (~/.benchmarks)
Defaulted to US keyboard (but can be set to any keyboard)
Screenlock mod (via start menu/system tools, or via keyboard 'alt'+'ctrl'+'l')
Monitor off/Powersave Mode (not screen blanking- default at 20 min or screenlocking)***
Bluetooth and WiFi on/off (rfkill)

//////////////////////////////////////////////////////////////////////////


* note1-Omxplayer media mod
To watch supported video/movie types in the OMXPlayer, all you need do is click/doubleclick on the video file you want to watch. It
will automatically load, and start to play. Supported file types are: mp3, mp4, mkv, avi, 3gp.

 

** note2-DOSbox fullscreen mode 'alt'+'enter'
fullscreen default for this OS is '1280x960', for smaller supported screens, this can be changed to '1024x768'
while maintaining the same 4:3 game ratio.

nano ~/.dosbox/dosbox-0.74.conf
find: 'fullresolution=1280x960' change to: fullresolution=1024x768
save file

 

*** note3-Monitor Off/Powersave Mode
You can change the time for off, or completely disable it (so screen never turns off)
see: https://youtu.be/aTrp83lgq_s

 


!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!

UPDATE FOR ADOBE/PEPPER FLASH
(You can check installed version here to see if you are on a current build: http://flashbuilder.eu/flash-player-version.html)

For future reference, updates to Flash will be made available here to be installed as it is released:

https://goo.gl/HRZ5ko

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 9 years ago

    sysbench --num-threads=4 --test=cpu --cpu-max-prime=20000 --validate run

     

    RPi2 (no mods to config.txt): 195.2287

    Biostar NM70I-1037U x64 Dual-core Celeron 1.8GHz: 46.5613

    Pine 64+ 2GB (exact same CPU as RPi3 but with x64 Ubuntu Mate and x64 sysbench): 10.0875