Raspberry Pi Forum what works for this card AND pi B+ AND one of the music distros (volumio, rune, musicbox)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 686 subscribers
  • Views 703 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

what works for this card AND pi B+ AND one of the music distros (volumio, rune, musicbox)

vv111y
vv111y over 9 years ago

I just spent time trying this https://volumio.org/forum/cirrus-logic-audio-card-element-t2324.html

which proceeded to crash after installing cirrus-config and rebooting.

 

I am really looking forward to using this as a dlna music player on the stereo, but I am getting lost trying to get this to work.

Please help,

 

Thanks

  • Sign in to reply
  • Cancel
Parents
  • vv111y
    vv111y over 9 years ago

    hmmm

     

    I tried getting help almost 2 years ago and got nothing

    https://www.element14.com/community/message/136386/l/b-with-cirrus-card-using-musicbox-052-wont-work#136386

     

    This is where the product is bought and I've never got to use it (I was busy and forgot about it).

    Come on, somebody at element14, or somebody,

     

    please help

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gvasco
    gvasco over 9 years ago in reply to vv111y

    HiasSoft has been I believe the main hero for us (edit: is > us) all that decided to get this card he's been improving the kernel over the past years and distributes it from the following page: RPi Linux driver for Wolfson / Cirrus Logic Audio Card

     

     

    For solutions that work out of the box I would recommend using LibreElec for all around media solution the developer of the drivers has been keeping up to date versions of the OS with his driver updates which you can find here:

     

    https://forum.libreelec.tv/forum-40.html

     

    All you need to do is flash an original image of the OS to the RPi SD card run a first boot and after place the .tar archive into the update folder and reboot the device. After that you should have LibreELEC running Kodi with the possibility of setting output to the Cirrus Logic DAC.

     

     

    If you're simply looking for dedicated bit perfect music playback you can try Volumio. However there is no out of the box working solution for this but I've been successfully running it on my RPi B+ for the past six months. To make volumio work with the DAC better start with a fresh install of the OS and follow the instructions on this post:

     

    https://www.element14.com/community/message/201098/l/re-driver-fixes-and-updates-to-kernel-31816-and-405#201098

     

    In combination with the instructions on his website (first link).

    So far I have only tried this on a previous version of Volumio with the previous version of the Kernel. Currently trying the above fix with the more recent Kernel version and Volumio version. Will try to remember to report on how well it worked.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • gvasco
    gvasco over 9 years ago in reply to vv111y

    HiasSoft has been I believe the main hero for us (edit: is > us) all that decided to get this card he's been improving the kernel over the past years and distributes it from the following page: RPi Linux driver for Wolfson / Cirrus Logic Audio Card

     

     

    For solutions that work out of the box I would recommend using LibreElec for all around media solution the developer of the drivers has been keeping up to date versions of the OS with his driver updates which you can find here:

     

    https://forum.libreelec.tv/forum-40.html

     

    All you need to do is flash an original image of the OS to the RPi SD card run a first boot and after place the .tar archive into the update folder and reboot the device. After that you should have LibreELEC running Kodi with the possibility of setting output to the Cirrus Logic DAC.

     

     

    If you're simply looking for dedicated bit perfect music playback you can try Volumio. However there is no out of the box working solution for this but I've been successfully running it on my RPi B+ for the past six months. To make volumio work with the DAC better start with a fresh install of the OS and follow the instructions on this post:

     

    https://www.element14.com/community/message/201098/l/re-driver-fixes-and-updates-to-kernel-31816-and-405#201098

     

    In combination with the instructions on his website (first link).

    So far I have only tried this on a previous version of Volumio with the previous version of the Kernel. Currently trying the above fix with the more recent Kernel version and Volumio version. Will try to remember to report on how well it worked.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • gvasco
    gvasco over 9 years ago in reply to gvasco

    If you choose to go with LibreElec and will be running the Pi headless you should probably use "hdmi_force_hotplug=1" or kodi won't load and you'll have to hook up th Pi to a monitor for first set-up.

     

    With any of the os's I've been able to run the Pi overclocked without any issues even at arm_freq=1100 (this clock setting may not work with all boards so try at your own peril max recommended over clock is 1000)

     

    Edit: For Pi config and over clock settings recommendations and testing have a look at this page: RPiconfig - eLinux.org