Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum RaspberryPi3 powering up but no visual HDMI - VGA
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 710 subscribers
  • Views 6760 views
  • Users 0 members are here
Related

RaspberryPi3 powering up but no visual HDMI - VGA

wolfmountaingames
wolfmountaingames over 9 years ago

I recently got a raspberry pi, but all my monitors are VGA so I went to the store got an HDMI to VGA adapter, and plugged in the screen, mouse, keyboard, and finally the pi. The red light came on so the power cord is working, but there was no visual at all it was as if the pi was not on. I read somewhere that in an older version if you changed a line in config.txt that it sometimes help with hdmi to vga, but I can not find config.txt anywhere on the preloaded card I bought. Can someone help me with this or link me to a confirmed working HDMI-VGA adapter that works with the pi?

 

Thanks,

 

Andrew

  • Sign in to reply
  • Cancel
Parents
  • rew
    rew over 9 years ago

    Hi Andrew,

    I am a bit worried about that SD card you have....

     

    There are two hints that this may be the problem. I don't hear anything from you about the green light flashing a bit when you turn on the pi. The green light should go on and off irregularly for a while after you turn on the pi. If NO green light is seen at all the pi is not seeing the SD card.

     

    Secondly, you say something about not finding config.txt. The SD card should have a boot partition which holds the stuff needed for booting. It is a fat partition that should be visible using Windows. And there you should be able to find "config.txt", simply in the root directory.

     

    (Hmm. I don't know how NOOBS handles booting and if you'd be able to see that config.txt file on a NOOBS card. )

     

    To bluntly answer your question: these work:  HDMI Male to VGA RGB Female HDMI to VGA Video Converter adapter 1080P for PC EJ | eBay

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rew
    rew over 9 years ago

    Hi Andrew,

    I am a bit worried about that SD card you have....

     

    There are two hints that this may be the problem. I don't hear anything from you about the green light flashing a bit when you turn on the pi. The green light should go on and off irregularly for a while after you turn on the pi. If NO green light is seen at all the pi is not seeing the SD card.

     

    Secondly, you say something about not finding config.txt. The SD card should have a boot partition which holds the stuff needed for booting. It is a fat partition that should be visible using Windows. And there you should be able to find "config.txt", simply in the root directory.

     

    (Hmm. I don't know how NOOBS handles booting and if you'd be able to see that config.txt file on a NOOBS card. )

     

    To bluntly answer your question: these work:  HDMI Male to VGA RGB Female HDMI to VGA Video Converter adapter 1080P for PC EJ | eBay

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Children
  • beacon_dave
    beacon_dave over 9 years ago in reply to rew

    On the NOOBS card the config.txt file is packed away inside of the \os\Raspbian\boot.tar.xz archive, presumably awaiting the user to select Raspbian from the NOOBS option list, at which point it is then will be extracted to the boot partition as per the Raspbian image.

     

    Within NOOBS however there are some display options available to the user:

    If your display remains blank, you should select the correct output mode for your display by pressing one of the following number keys on your keyboard:
    1. HDMI mode - this is the default display mode.
    2. HDMI safe mode - select this mode if you are using the HDMI connector and cannot see anything on screen when the Pi has booted.
    3. Composite PAL mode - select either this mode or composite NTSC mode if you are using the composite RCA video connector.
    4. Composite NTSC mode

     

     

     

    Roger Wolff wrote:

     

    ...

     

    (Hmm. I don't know how NOOBS handles booting and if you'd be able to see that config.txt file on a NOOBS card. )

     

    ...

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • wolfmountaingames
    wolfmountaingames over 9 years ago in reply to rew

    I should have mentioned it, but yes when I first plug the pi in I do see a green light flash on and off for a few seconds and then it stops.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wolfmountaingames
    wolfmountaingames over 9 years ago in reply to beacon_dave

    These are the files I see on root: https://screenshot.net/ryrcddl   I have found the boot.tar.xz archive where you said it would be, when I opened it  and opened boot.tar and config.txt was inside now to test out the uncommenting image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • pkps1968
    pkps1968 over 9 years ago in reply to rew

    Hi.. Roger...

    I am also facing same problem...

    I can see only red LED  No Green LED not even blinking...

    What should i do...?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 9 years ago in reply to pkps1968

    When a Raspberry pi boots, the GPU will start and load "bootcode.bin" from the SD card. That contains code to do the things that config.txt tells it to and then load "kernel.img" and start the CPU.

     

    All that already causes some flashes of the green led. If you see no flashes, no communication with the SD card is happening. Card not inserted? No "bootcode.bin" on the SD card? stuff like that.

     

    So for both of you, I'd simplify things by just getting a raspbian image and put that on your SD card according to the instructions you can find online. Then you CAN see config.txt and edit if necessary.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • slashthedragon
    slashthedragon over 9 years ago in reply to wolfmountaingames

    Check again. Mine flashes so quickly after it first booted up that I would not have seen it if the lights were low and I had not waited long enough.