Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Your Breakdown of Raspberry Pi Customization
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 68 replies
  • Subscribers 720 subscribers
  • Views 8294 views
  • Users 0 members are here
  • customized pi
  • customized_pi
  • customization_service
  • customization
  • customisation
  • customization service
  • raspberry pi
  • raspberry-pi
  • raspberrypi
  • customised pi
  • customisation service
Related

Your Breakdown of Raspberry Pi Customization

spannerspencer
spannerspencer over 10 years ago

You might have just seen the official joint announcement from the Raspberry Pi Foundation and element14 regarding an exclusive new customization service for the Raspberry Pi, and we'd love to hear your thoughts on the subject.

 

Bulk Customization Services

The facts are these:

 

You can now open a dialogue with element14 about creating a Raspberry Pi that's tailored to specific needs, on orders of 3,000 units or more. You can reconfigure the board, add new functionality, add or remove features, change the memory configuration; pretty much anything besides tinkering with the GPU and related software. A full breakdown of the service can be found here: Raspberry Pi Customization Service

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Cooking Up a Custom Raspberry Pi

Clearly this is aimed squarely at OEM manufacturers, suppliers and bigger companies due to the minimum order quantity, but such places are still populated by engineers and makers who'd be the ones that determine just what a customized Raspberry Pi would require for specific needs.image

 

So we thought it'd be valuable to get the element14 community's opinion on this new service.

 

Will companies find a lot of use for it, and what might they need a custom Pi for?

 

Which kinds of customization are likely to be the most popular? Expansion of the device, or minimization?

 

Give us your predictions on the future of element14's Raspberry Pi Customization Service below, and who knows how it might evolve.

  • Sign in to reply
  • Cancel
Parents
  • fvan
    fvan over 10 years ago

    A customisation I'd like to see is a low(er) profile RPi2:

    • 2x 1 USB port iso 2x 2ports
    • GPIO pins at 90° angle
    • no ethernet port

    (In short, a Raspberry Pi 2 Model A ...)

     

    Unfortunately, as I'm not a business (and do not require 3000 units) I'll just heat up my soldering iron ... image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to fvan

    Thinking seriously to your idea is: why remove pieces to a device that you have paid anyway for the full pieces? As a matter of fact, it has sense - IMHO - that a certain company for its own project needs to pay less than a Raspi but loves it for its technical projects. So ask to build 3000 pcs (at least) with parts removed, that I think will cost less, to embed this custom version in its own project. But if you already have a full PI, why remove what you don't need ? It does not saves money nor time as well. Or I have misunderstood something ?

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to e14 Contributor

    Doug,

     

    my doubt is that for a medium average company 3000 pieces (also for a kickstarter production) is a small number and totally affordable for a production. Or I am wrong and my selling of 10 pieces in two months is alot ?

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to balearicdynamics

    Enrico,

     

    I don't think 3000 units is an achievable amount for a small company to turnover, however it is clear in the video of the press conference that some customers buy tens of thousands of units in a single transaction, therefore there will likely be some demand for this service.

     

    I've only seen a few requests for "barebones Pi" but there may be enough demand for a run of 3000 of them. Possibly a stripped down version of the Pi would be possible in smaller quantities as no redesign works would be required, just a re-program of the pick and place to omit some of the components.

     

    I look forwards to seeing a plethora of kickstarters offering subtle variants on the Pi theme.

     

    Some other likely possibilities (Likely in some combination):

     

    +RTC

     

    +Arduino

     

    +ADC

     

    +DAC

     

    + motor driver

     

    + relays

     

    + Power switching (true powerdown rather than standby)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • gadget.iom
    gadget.iom over 10 years ago in reply to e14 Contributor

    Doug Jefferies wrote:

     

    +RTC

     

    Not thats a good suggestion! image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to e14 Contributor

    Thank you Doug,

     

    I don't think 3000 units is an achievable amount for a small company to turnover


    This is the detail I am not aware. Frankly I was prepending to thing that 100.000$ was the minimal investment for a company gong on the market marketing a custom device... So, considered your assertion, they are orienting this service just to the very big companies.


    Good ideas the customisation options you suggest, obviously image


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to balearicdynamics

    Enrico,

     

    I have no experience as a salesperson or involved in distribution from a company on any scale.

     

    I am primarily a hobbyist user of this type of device (although my profession is semi-related to computing and micro-controllers).

     

    I think it would depend on exactly what the company is trying to do and how much of their service is supply and fit Verses how much is maintain and service.

     

    Several Kickstarter business models manage to achieve in excess of 3000 units, the nature of global access to new products. Other ideas fall far short of this goal.

     

    Unfortunately without an idea of the costs & timescales involved with having your Pi design modified by the Element 14 team it would be hard to design a kickstarter around this plan.

     

    Many of the Pi based Kickstarters I have seen have had between 100 and 1000 backers, far short of the quantities needed to meet the minimum requirements for this program.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to e14 Contributor

    You are right Doug,

     

    making two counts I have just supposed that the customisation costs was part of the final product but probably it is not. So, maybe that the 3000 pieces is just a number but by a marketing point of view it is far from the break even point to grant a decent return per unit sold. I am not a marketing man at all nor salseparson too, but I was just thinking on how much sense can have this premises... There is a lack of information to make a complete and trustable scenario.

     

    Enrico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • poordom
    poordom over 10 years ago in reply to e14 Contributor

    Enrico,


    I love the items you consider for customisation, simply because the items mentioned could be used as part of a Home Automation customisation.


    I would add to your list a built on Z-Wave communication module.


    Dom

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • spannerspencer
    spannerspencer over 10 years ago in reply to e14 Contributor

    Hey, that's an interesting notion though, Enrico. What if someone started a Kickstarter campaign to have a batch of 3,000+ customised RPis put together (using the crowd's bulk buying power), and then effectively making them available to users in much smaller (even single) quantities. It'd be no small task, as you point out, but it's an intriguing thought, eh?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to spannerspencer

    The trick being to find the modification to the Pi that will gather enough buyers for 3000 Pi's of a brand new design. I'm not sure if it will sell when everyone wants something slightly different.

     

    Lets imagine two Modded Pi's:

    Super Pi: As normal Pi + Arduino, RTC, DAC, Relays.

    DAC output at 0-10v, Arduino analog inputs able to accept 0-10v or 4-20mA at 10v, relay outputs safe for use at 240v 10A.

    Cost £100?

     

    Slim Pi: Normal Pi with reduced height by: Swapping double height USB sockets for single height, GPIO pin header not soldered on (user can then solder to individual through hole pins or add a header as they choose). True Powerdown facility added (so when you tell the Pi to turn off, it actually stops using power) with through hole power on/off pin headers so you can add an external switch.

    Cost: a little more than a normal Pi?

     

    Each of those cases would appeal to a market, but would that market be large enough to support 3000 purchases?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • gadget.iom
    gadget.iom over 10 years ago in reply to e14 Contributor

    Doug Jefferies wrote:

     

    I'm not sure if it will sell when everyone wants something slightly different.

     

    Lets imagine two Modded Pi's:

    Super Pi: As normal Pi + Arduino, RTC, DAC, Relays.

    DAC output at 0-10v, Arduino analog inputs able to accept 0-10v or 4-20mA at 10v, relay outputs safe for use at 240v 10A.

    Cost £100?

     

     

    Exactly!

     

    You'd get "What about a DDR3 Socket", "What about SATA sockets", "Can it have a VGA and DVI sockets", "Where's the WiFi", "Bluetooth?", "NFC", etc etc.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • gadget.iom
    gadget.iom over 10 years ago in reply to e14 Contributor

    Doug Jefferies wrote:

     

    I'm not sure if it will sell when everyone wants something slightly different.

     

    Lets imagine two Modded Pi's:

    Super Pi: As normal Pi + Arduino, RTC, DAC, Relays.

    DAC output at 0-10v, Arduino analog inputs able to accept 0-10v or 4-20mA at 10v, relay outputs safe for use at 240v 10A.

    Cost £100?

     

     

    Exactly!

     

    You'd get "What about a DDR3 Socket", "What about SATA sockets", "Can it have a VGA and DVI sockets", "Where's the WiFi", "Bluetooth?", "NFC", etc etc.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to gadget.iom

    Precisely,

     

    Anyone doing a Kickstarter would have to find a market niche that the Pi variant will fill, a niche big enough to support 3000 sales whilst being adaptable enough to absorb the inevitable requests for slight variations and still be cheaper  than other existing products.

     

    I hope we see some of these come to life, but I wouldn't bet on it.

     

    Perhaps the Element 14 team will have lower prices for open designs than proprietary ones?

    This would make sense as a broad library of decent open designs will allow for cheap modifications in the future.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gadget.iom
    gadget.iom over 10 years ago in reply to e14 Contributor

    I imagine most of them will be private customisations for companies to integrate with their products.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 10 years ago in reply to gadget.iom

    also Paul, the organisation that created a given super Pi will be stuck maintaining the H/W and the software drivers for the customers and also keeping it in sync with the main RPi software stack

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gadget.iom
    gadget.iom over 10 years ago in reply to Problemchild

    John Alexander wrote:

     

    also Paul, the organisation that created a given super Pi will be stuck maintaining the H/W and the software drivers for the customers and also keeping it in sync with the main RPi software stack

    True... But we're bound to get end customers on here with issues/questions.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 10 years ago in reply to gadget.iom

    Doesn't sound like fun supporting someone's Supa Pi especially if you don't have one to hand and wondering what he was on about taking about widget XYZ

     

    Any way I think this is really meant to be for commercial suppliers.. question would be what products you could build that would require a custom Pi