Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Your Breakdown of Raspberry Pi Customization
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 68 replies
  • Subscribers 720 subscribers
  • Views 8218 views
  • Users 0 members are here
  • customized pi
  • customized_pi
  • customization_service
  • customization
  • customisation
  • customization service
  • raspberry pi
  • raspberry-pi
  • raspberrypi
  • customised pi
  • customisation service
Related

Your Breakdown of Raspberry Pi Customization

spannerspencer
spannerspencer over 10 years ago

You might have just seen the official joint announcement from the Raspberry Pi Foundation and element14 regarding an exclusive new customization service for the Raspberry Pi, and we'd love to hear your thoughts on the subject.

 

Bulk Customization Services

The facts are these:

 

You can now open a dialogue with element14 about creating a Raspberry Pi that's tailored to specific needs, on orders of 3,000 units or more. You can reconfigure the board, add new functionality, add or remove features, change the memory configuration; pretty much anything besides tinkering with the GPU and related software. A full breakdown of the service can be found here: Raspberry Pi Customization Service

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Cooking Up a Custom Raspberry Pi

Clearly this is aimed squarely at OEM manufacturers, suppliers and bigger companies due to the minimum order quantity, but such places are still populated by engineers and makers who'd be the ones that determine just what a customized Raspberry Pi would require for specific needs.image

 

So we thought it'd be valuable to get the element14 community's opinion on this new service.

 

Will companies find a lot of use for it, and what might they need a custom Pi for?

 

Which kinds of customization are likely to be the most popular? Expansion of the device, or minimization?

 

Give us your predictions on the future of element14's Raspberry Pi Customization Service below, and who knows how it might evolve.

  • Sign in to reply
  • Cancel
  • rew
    rew over 10 years ago in reply to Anonymous-237891

    You already have that: The raspberry pi 2 tolerates 3.3V (*) to 5.5V on its ("officially 5V") input. The only thing is that it won't be able to power USB and HDMI peripherals with a proper 5V if the input 5V isn't up to par.

     

    (*) it stops booting around 2.8V IIRC.... The "5.5V" was not tested. From the datasheet.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 10 years ago in reply to rew

    Out of interest did you put the 2.8 V into the 5V input or in to the 3.3 thus saving the headroom of the regulator?!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 10 years ago in reply to Problemchild

    No, I "feed" the 5V input of the 'pi . Or to be more correct: I feed the pi through the 5V pin on the GPIO connector. This bypasses the input "fuse". In previous experiments with the PI 1,  I found that ethernet would stop working below about 4V on the input. This was due to the 3.3V power line dropping below 3.0V and the ethernet chip failing at 3.3V-10%. However this time I got very similar results until I put a good capacitor on the "5V" near the 'pi. Apparently short surges through the long cables to the power supply were responsible for some sort of crash when closing in on the limit voltage.... The dropout of an efficient DCDC converter is very small.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 10 years ago in reply to Anonymous-237891

    Yeah normally it's much easier to take a much higher voltage. (Say 12v for the motors) then  locally regulate  that down to say 5V to go tot he RPi

    Hopefully even with the motor noise it wouldn't bring the 12 V rail lower than the 5 V regulator could cope with. Overvoltage and  RF noise breaking through this would still be a  problem but could be sorted out .... Over all trying to deliver clean power in a noisy environment is far from trivial and that would be reflected in the price of a formally cheap board.... Probably easier and safer for the RPi to keep al that stuff off the RPi board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Anonymous-237891
    Anonymous-237891 over 10 years ago in reply to Problemchild

    Yeah you are probably right, it could add up to the cost pretty quick.

    Cleaning a really noisy power rail is a real challenge, especially when operating crap DC motors.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wesleyfurr
    wesleyfurr over 10 years ago

    Some interesting discussions.  Personally, I would like to see something very much like the Odroid-W:

     

    http://www.hardkernel.com/main/products/prdt_info.php?g_code=g140610189490

     

    I stumbled into it a while back and got excited, then found out they were no longer selling them because Broadcom wouldn't supply them with chips.  Let's not get into the debate of why, that's been hashed out elsewhere.  Just take a look and what it provided for the price point.  I was interested due to the reduced size and add-on features such as built-in RTC and LiPo battery connector and DC-DC converter.  Something like that I would certainly be interested in...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 10 years ago in reply to wesleyfurr

    Every one was excited when that turned up. Then chip availability brought  the end of it which was very sad

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    I can see myself looking for some fairly specific things, WOL, GbE PoE, PXE, SFP+ with fiber optic speeds(40GbE+), perhaps a modular design for a more consumer grade board, allowing users to put on a second or third SFP+ port, or perhaps multiple HDBaseT over single cable, allowing remote multimonitor, with the added bonus of bidirectional IR. Even a giant hub of USB 3.0 or powered esata RAID. These were the original reasons I had purchased an RPi, and with these features I have mentioned, imagine the true potential of such a device.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Anonymous-237891
    Anonymous-237891 over 10 years ago in reply to rew

    Just as a follow up, I recently tried my homemade step-up converter that bring the lipo voltage to 5 volt and without any surprizes... it didn't worked... you need quite a beefy regulator to step-up the voltage and still have enough power at the output.

     

    The raspi turned on and eventually powered itstelf off as soon as I launched chromium image

    The current needed by the raspi 2 + my keyboard made the voltage on the regulator drop dramatically since it was overloaded with bare raspbian running...

     

    I need to find a new step-up that is drastically better than the TPS 61200 that I used...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to gadget.iom

    Dear friend,

    I wanted tostart with raspberry pi , i new to it could you help?

    Am much familiar to Mictrocontrollers particularly Stellaris and Tiva series, but very much new to Raspberry-pi.

     

    Please help?

     

    Rohit

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>