Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Up Board Pi-Top
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 706 subscribers
  • Views 2659 views
  • Users 0 members are here
Related

Up Board Pi-Top

dheald
dheald over 9 years ago

Has anyone else put an Up Board in a Pi-Top?

  • Sign in to reply
  • Cancel
Parents
  • dheald
    dheald over 9 years ago

    I was referring to the specific Pi-Top product. I put an up board in one for my wife. She loves it. I had to make my own power cord for it, but otherwise it works great.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • uscdadnyc
    uscdadnyc over 9 years ago in reply to dheald

    To DH: so you put an UP Board in the "clam-shell" laptop Pi-Top product? Didn't it come w/ a power Brick.? My Pi-TopCREED uses a 18Vdc @1A Power Brick. I believe the Pi-Top Laptop and Pi-TopCREED share the same inner components. But the Pi-TopCREED does not have Battery, Keyboard, Trackpad. Since I haven't bought an Up board yet. I am going to test my Pi-TopCREED  w/ a RaspberryPi Zero-Wireless.

    USCDADNYC (NY NY USA)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • uscdadnyc
    uscdadnyc over 9 years ago in reply to uscdadnyc

    To DH: Have you used your Pi-Top Laptop(?) as a External HDMI Monitor? I mean cabling the HDMI Cable of the Pi-Top to an External (to Pi-Top) HDMI source? No other Connections aside from DC Power to my HDMI Source (RaspPi Zero). Did Not connect to the GPIO Pins. Pi-Top Support is working this Issue

    BTW the Pi-Top that you configured for Your Wife, the one w/ Up SBC, what O/S did you use?

    USCDADNYC (NY NY USA)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • uscdadnyc
    uscdadnyc over 9 years ago in reply to uscdadnyc

    To DH: I successfully got my Pi-TopCREED to work w/ my RPi-Zero (v1.3). The 40pin Header MUST BE CONNECTED to the 40pin GPIO Pins for the HDMI/LCD Screen to work. Not all 40pins are used. Just pin4 [5V], pin6 [Gnd] (duh. of course), pin19 [SPI_MOSI], pin21 [SPI_MISO], pin23[SPI_CLK], pin26[SPI_CEI_N]. I think these Signals on the GPIO pins are used in conjunction w/ the HDMI Input (into) the Pi-TopCREED internal "Hub" board that produces Output on the LCD Screen. If this is the case, then it looks improbable that I can use the Pi-TopCREED HDMI/LCD Screen as an external HDMI Display Screen. THIS even if I leave my RPI-Zero connected to the GPIO Header and attempt to "drive" the PitopCREED HDMI w/ external (video) Content. Darn. I was hoping this Pi-TopCREED would do Double Duty: (1) as RPi Enclosure, (2) as External HDMI/LCD Monitor. At least my LCD Display is proven to be Good. AAR can you (DH) verify that your (wife's) Pi-Top Laptop is: (1) UP and Running w/ the Up SBC board [Pun Intended], (2) the GPIO Header is connected to the GPIO pins on the Up SBC. BTW what O/S is running? Thanks.

    USCDADNYC (NY NY USA)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • uscdadnyc
    uscdadnyc over 9 years ago in reply to uscdadnyc

    To DH: I successfully got my Pi-TopCREED to work w/ my RPi-Zero (v1.3). The 40pin Header MUST BE CONNECTED to the 40pin GPIO Pins for the HDMI/LCD Screen to work. Not all 40pins are used. Just pin4 [5V], pin6 [Gnd] (duh. of course), pin19 [SPI_MOSI], pin21 [SPI_MISO], pin23[SPI_CLK], pin26[SPI_CEI_N]. I think these Signals on the GPIO pins are used in conjunction w/ the HDMI Input (into) the Pi-TopCREED internal "Hub" board that produces Output on the LCD Screen. If this is the case, then it looks improbable that I can use the Pi-TopCREED HDMI/LCD Screen as an external HDMI Display Screen. THIS even if I leave my RPI-Zero connected to the GPIO Header and attempt to "drive" the PitopCREED HDMI w/ external (video) Content. Darn. I was hoping this Pi-TopCREED would do Double Duty: (1) as RPi Enclosure, (2) as External HDMI/LCD Monitor. At least my LCD Display is proven to be Good. AAR can you (DH) verify that your (wife's) Pi-Top Laptop is: (1) UP and Running w/ the Up SBC board [Pun Intended], (2) the GPIO Header is connected to the GPIO pins on the Up SBC. BTW what O/S is running? Thanks.

    USCDADNYC (NY NY USA)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • uscdadnyc
    uscdadnyc over 9 years ago in reply to uscdadnyc

    W/ help from Pi-Top Support Staff, I found out about the Pi-TopCREED: (1) The HDMI Cable allows the LCD Screen to be used as an External HDMI Display. No connection to the GPIO pins required. (2) the power Supply inside the Pi-topCREED can supply +5V @ 1A. This opens the possibility of Installing an Up SBC instead of RPi 3B (or Zero). But will have to add an additional Power Brick b/c the Up board will draw 3A @ 5V.

    USCDADNYC (NY NY USA)