Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi to PC Need help
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 709 subscribers
  • Views 1468 views
  • Users 0 members are here
  • frontpage
Related

Raspberry Pi to PC Need help

vital
vital over 9 years ago

Greetings,

 

I have a question.  I have a "Raspberry Pi Touchscreen Display" and I am wondering if there is any way to connect it directly into a PC directly?  Maybe by USB or something like that.

I would love the help on this one.  I am really at a loss in connecting them together and thought I would reach out to the pro engineers here.

 

Thank you for your time from,

Michael

  • Sign in to reply
  • Cancel
Parents
  • balearicdynamics
    balearicdynamics over 9 years ago

    Hello Michael,

     

    do you mean to connect a PI to a Pc ?

    In this case there are many ways, depends on the kind of PC. operating system you are using (Windows? Max? Linux?) Anyway I can give you some suggestions below that need an in depth investigation in documentation.

     

    1. You can connect the two machines via the same local lan (Ethernet cable or WiFi). In this case you should define what to share on both sides and connect the two machines together.
    2. You can share the Internet connection from the PC (for example the PC is connected to the Internet via WiFi and yu share che connection through the ethernet cable)
    3. You can connect the PI to the Pc via USB using a proper USB to Serial cable. Then you can access the PI via terminal or using VNC

     

    Maybe you should be more specific for a more detailed definition.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • balearicdynamics
    balearicdynamics over 9 years ago

    Hello Michael,

     

    do you mean to connect a PI to a Pc ?

    In this case there are many ways, depends on the kind of PC. operating system you are using (Windows? Max? Linux?) Anyway I can give you some suggestions below that need an in depth investigation in documentation.

     

    1. You can connect the two machines via the same local lan (Ethernet cable or WiFi). In this case you should define what to share on both sides and connect the two machines together.
    2. You can share the Internet connection from the PC (for example the PC is connected to the Internet via WiFi and yu share che connection through the ethernet cable)
    3. You can connect the PI to the Pc via USB using a proper USB to Serial cable. Then you can access the PI via terminal or using VNC

     

    Maybe you should be more specific for a more detailed definition.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • SGarciaV
    SGarciaV over 9 years ago in reply to balearicdynamics

    From my perspective, since Michael enclosed the device name in quotes, I assume that he is asking about connecting the display, not the R-Pi. As you said, he needs to clarify; however, I have not seen any further participation on his behalf to do this. Hopefully he'll chime in. Salvador