Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum RPI wired network
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 708 subscribers
  • Views 3370 views
  • Users 0 members are here
Related

RPI wired network

setcamerav2
setcamerav2 over 9 years ago

HI,

 

I would like to create a wired network of several (6) RPi with cameraboard v2. I would like to use one (more) RPI to send all the other RPIs the same signal (i.e. to shoot a still picture at the same time).

I am a complete newbie in RPi and networks.

Anyone could give any instructions to do that and or any hints on where to find?

Thank you.

 

Giuseppe

  • Sign in to reply
  • Cancel
Parents
  • balearicdynamics
    balearicdynamics over 9 years ago

    Hi Giuseppe,

     

    first of all, frankly I suggest you to document a while on what the Raspberry PI can do, just to figure ut a scenario and focus better your idea. By a general point of view, also considering that you are not super skilled, probably the easiest way to do this with 6 PI is proceeding by steps. I can suggest a possible draft of the project building:

    BTW, If you can draw us your project more in detail sure we can be more helpful.

     

    1. Completely setup a stand-alone working PI with the camera. This will help you to manage one problems at a time and experiencing a while better with the board focusing the attention on your needs. When you have a PI with a camera that works as you need (shooting, image saving etc.)
    2. Look on how to write simple Python code (or just bash commands) to control the camera features you want, in particular a command for shooting the camera.
    3. Setup a network of Raspberry PI. The first next question is: do you need the Internet on the LAN ? I suppose yes. To reach this you have two choices: at least one of the PI should be a version 3 including the WiFi or add to at least one WiPi (WiFi USB dongle) or similar for one PI.
    4. Setup the PI with the double network as a bridge, so it can share the WiFi Internet connection via the wired connection with the other PIs
    5. Provide a 10/100 Ethernet HUB As PI does not support super high speed ethernet yo can buy a low cost HUB/Switch with 6 (maybe 10) ethernet ports.
    6. Document yourself a while on the ssh protocol, this will be the easiest way you can exchange and send commands between the PI network.

    There is a lot more to say but I think that the first that should tell a complete story it's you.

     

    Enrico

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 9 years ago in reply to balearicdynamics

    Hi Giuseppe,

     

    Enrico has given great advice, break the problem down into manageable chunks as he suggests and build everything up piece by piece and you'll get there.

     

    With regards to this:

    Enrico Miglino wrote:

     

    Document yourself a while on the ssh protocol, this will be the easiest way you can exchange and send commands between the PI network.

    There is a lot more to say but I think that the first that should tell a complete story it's you.

    Once you have read up on SSH and understand it a little then look at the blog I wrote here: Updating security for remotely connecting to my servers via SSH

     

    In here I explain how to set up SSH between linux machines to use shared keys for connections between them rather than having to type passwords.

     

    Then once you've set it up so your controller Pi can SSH directly into each of your slave Pi's, follow what Workshopshed did to run the same command on multiple Pi's on his blog here:  Building a Render Farm with a Bitscope Blade Quatro - Setup of the nodes

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • setcamerav2
    setcamerav2 over 9 years ago in reply to rachaelp

    Thank you Enrico and Rachael for your prompt reply and useful advice!

     

    As you suggested I will buy one RPi and cameraboard v2.

    I will also try to document myself on all the stuff you suggested: Python, SSH.....

     

    My project:

    building a set of RPIcameraboards v2 to shoot stilll pictures to stitch together in a pano (360°) picture.

    There are devices for taht on the market (for example samsung gear) but there resolution is low (30 mpx).

    The lens on the cameraboardv2 is a low quality lens, I suppose.

    I think it is possible to change with a better lens: I find one with a horizontal field of view of about 90°. In this case I would need 12 cameraboards and 12 RPIs to cover the full sphere. Of course i am not sure that will work.

    So first of all let's test on one cameraboard and RPI.and see the oupput in terms of image quality. am not expecting of course professional image quality but I hope not so bad....

     

    Next step is to build a set of 12 RPIs and camera boards with one more RPI to control the others in the set, i.e. tell them to shoot a still picture at the same time. The set should be wired connected (no wifi or internet): it would be like one camera, though not so small.

    Here the problem is to succeed in shooting all the cameras at the same time with a tolerable delay of about 2 ms (that is related to the stitching process) because in the scenes there will be moving objects/subjects.

    That was the aim of my question: if that is not possible I will not proceed.

     

    For example I will shoot a panopicture of a monument with people moving around.

    I would like to put the apparatus on a rig and ....push a button (on a touch screen attached to the master RPI) and shoot a picture from every cameraboards of the set, store each of them on each RPI and alter stitch them all on a pano picture.

     

    Thank you for any remarks and advice.

     

    Giuseppe

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to setcamerav2

    Hello Giusppe,

     

    in my opinion this project seems possible and sounds very interesting. The idea to stitch cameras together is interesting. But as you plan to place 12 PI in a fixed position, why not explore also the option to make a video array for the "matrix effect" ? I mean something like this: https://fstoppers.com/video/using-gopro-camera-arrays-live-bullet-time-effect-3151 The minimum number of cameras to synch for good effect is just 12 image

     

    What I think it is not a great idea is to totally replace the camera lenses as they are glued in the right position over a small sensor and I bet it will be extremely difficult to remove and place a new one. The PI Camera V2 has a good lens and the sensor a good resolution too, not particular visibile lens distortion especially if every image is just a part of a more complex composition. I suggest to explore - may give absolutely better results - additional lenses to the standard V2 camera lens like those available for smartphones. I have done a search in the recent past for another project and beside the really "bottom-glass quality" lenses that are an offense when placed on a iPhone camera lens there are also (more expensive) very good products. Take a look to this link, just as an example: http://thewirecutter.com/reviews/best-lenses-for-iphone/ and https://exolens.com/product/exolens-with-optics-by-zeiss-wide-angle-iphone-66s/

     

    Enrico

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • setcamerav2
    setcamerav2 over 9 years ago in reply to balearicdynamics

    Hi Enrico,

     

    thanks for suggestions.

    I would like to use the set for still pictures of places of historic interest: churches, squares ...

    The problem of space and weight is a real problem which I have not considered in details yet.

    I would build a rig for the cameras and a rig for the RPIs. I will use everything with a tripod and I think (...hope) it will be feasable.

    As regards the original lens in the cameraborad it has a 62° horizontal Field of view and I would need more than twelve for a pano picture.

    tha additional lens you suggest may be interesting to test but I suppose they are designed to be added in Iphone lens and sensor only, which i am not sure are the same as in cameraboard v2.

    I have found this one: https://www.bluerobotics.com/store/electronics/cam-rpi-wide-r1/ which has a mount that allows to change the lens with other M12 lens, although that will be expensive

     

    The first  problem to solve for me now, otherwise I do not go further, is to figure out how to build and manage a wired connection of the 12 (or more) RPIs and their cameras to one RPI (via a router?) which allow me to order the others to shoot at the same time a still picture....

     

    Grazie ancora.

     

    Giuseppe

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 9 years ago in reply to setcamerav2

    Hi Giuseppe,

     

    I think you should be able to get good synchronisation between the pi's but you might need to buy a few and experiment a little to see how much skew you are getting. If you need to get it more accurate you could use ptpd to sync everything over the pi network, and then command the camera pi's to trigger at a given time. I'm not sure how accurate it should get using ptpd on a pi cluster as I haven't tried it.

     

    Best regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 9 years ago in reply to setcamerav2

    giuseppe porciani wrote:

     

    The first problem to solve for me now, otherwise I do not go further, is to figure out how to build and manage a wired connection of the 12 (or more) RPIs and their cameras to one RPI (via a router?) which allow me to order the others to shoot at the same time a still picture....

    This should be fine. You will need a 16 port switch (13 of which you will be using) to connect them all together. Configure all the pi's with static IP addresses or use the master as a DHCP server with reservations set for each of the slave devices to ensure they always get the same IP address. Then follow the details given in previous posts to configure it to do what you need.

     

    Just remember to break it down into small pieces and get each bit working individually before building the system up together.

     

    Bedt Regards,

     

    Rachael

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rachaelp
    rachaelp over 9 years ago in reply to setcamerav2

    giuseppe porciani wrote:

     

    The first problem to solve for me now, otherwise I do not go further, is to figure out how to build and manage a wired connection of the 12 (or more) RPIs and their cameras to one RPI (via a router?) which allow me to order the others to shoot at the same time a still picture....

    This should be fine. You will need a 16 port switch (13 of which you will be using) to connect them all together. Configure all the pi's with static IP addresses or use the master as a DHCP server with reservations set for each of the slave devices to ensure they always get the same IP address. Then follow the details given in previous posts to configure it to do what you need.

     

    Just remember to break it down into small pieces and get each bit working individually before building the system up together.

     

    Bedt Regards,

     

    Rachael