Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Computer Vision, OpenCV + Maths
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 706 subscribers
  • Views 1267 views
  • Users 0 members are here
  • frontpage
  • raspberry_pi_space
Related

Computer Vision, OpenCV + Maths

the48sicks
the48sicks over 8 years ago

I love learning things, and maths - as much as i hated it at school (Why do i need this?) In my older years, I'm starting to see why.

 

The previous version of my robot had camera and laser mounted on the same appendage so the maths was pretty much simple simple.  separating the two has been somewhat of a challenge and a rewarding one, the code is still quite raw and im sure i can make it more responsive but the initial results are amazing.

 

So here we are using the focal length of the camera to determine the distance to the object based on its given size (18cm)  and then using the triangle similarity method to determine how far off center the target is to compute the cartesian coordinates of the object concerned. The offset is then recalculated on the appendage that is 11 cm off center and the polar coords are delivered.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply
  • Cancel
Parents
  • jdlui
    jdlui over 8 years ago

    Cool demo! Can you give more info about your robot? How does the Pi control it?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • the48sicks
    the48sicks over 8 years ago in reply to jdlui

    Thanks guys!

     

    Main robot control is managed through an Arduino Mega, the Pi then sends it commands to operate various features

     

    CMD:value;

     

    so

     

    MTR:150;    #Motors "right" for 150ms

     

    using multithreading in python i can have a thread for each serial connection (2x arduino + gsm modem)  and control it all from the one interface running in the pi.

     

     

    Hope this helps!

     

     

    Cheers,

     

    Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • the48sicks
    the48sicks over 8 years ago in reply to jdlui

    Thanks guys!

     

    Main robot control is managed through an Arduino Mega, the Pi then sends it commands to operate various features

     

    CMD:value;

     

    so

     

    MTR:150;    #Motors "right" for 150ms

     

    using multithreading in python i can have a thread for each serial connection (2x arduino + gsm modem)  and control it all from the one interface running in the pi.

     

     

    Hope this helps!

     

     

    Cheers,

     

    Matt