Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi Zero W instead of B+ for GPIO LCD Panel?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 705 subscribers
  • Views 505 views
  • Users 0 members are here
  • rasberry_pi_3_b_plus
  • raspberry_pi
Related

Pi Zero W instead of B+ for GPIO LCD Panel?

mr_widget
mr_widget over 8 years ago

Per the recent-ish project on the podcast Ben and the gang created a GPIO-based Pi hack with the connectors removed.  Would a similar configuration be feasible using a Pi Zero W?  Most sites in the blogosphere seem to insist only composite video can be connected, but I have a 4.3" panel that I would like to use for a similar project (A dedicated jazz station radio).  It appears that most of the connector is the same between the Pi B+ and the Zero, so if I use the same TFT breakout adaptor would that be successful?

 

J.R.

  • Sign in to reply
  • Cancel
  • ifish
    ifish over 8 years ago

    Yah, a bunch of us who participated in the Hack Like Heck contest used Pi zero w's with the 40pin break out board.  I had to add a pi zero w section to the dtblob file before compiling it, this tid bit of data was found on this page https://www.raspberrypi.org/documentation/configuration/pin-configuration.md

     

    I also had to use mode 3 instead of mode 2 (used by Ben and the gang) so that I'd have access to two pwm pins for producing stereo audio, as per the documentation outlined on these two pages

    https://www.raspberrypi.org/documentation/hardware/raspberrypi/dpi/

     

    https://www.raspberrypi.org/documentation/hardware/raspberrypi/dpi/

     

     

    Cheers,

    Chris