Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum RPi 2 Model B v1.2 with BCM2837
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 704 subscribers
  • Views 407 views
  • Users 0 members are here
  • broadcom bcm2837
  • raspberry-pi-2
Related

RPi 2 Model B v1.2 with BCM2837

mp2100
mp2100 over 8 years ago

I just ordered a couple RPi 2, now at version 1.2, which ships with the newer BCM2837 SoC. 

https://www.newark.com/raspberry-pi/rpi2-modb-v1-2/silicon-manufacturer-broadcom/dp/95Y1948

I see this change to BCM2837 has been around since 2016.

(Why buy a "2" you ask?  I have my reasons, I have an RS232 board that works perfectly with a RPi 1 on the UART, and the RPi 3 moved UART things around, and I want a faster RPi but one that just works, using my configuration)

 

So my question is, can I USB boot?   I've been using my RPi 3 by booting it from the USB port instead of the SD card.  My understanding from:

https://www.raspberrypi.org/documentation/hardware/raspberrypi/bootmodes/msd.md

that this is a feature of the BCM2837.  Is that correct?  Does that mean I can modify /boot/config.txt. with the one-time-program change, in my RPi 2 for USB boot?  The article only mentions the RPi 3.  Is it a feature of the BCM2837, or something else?  I don't want to write to a register in the BCM2837 if that's a bad idea.