Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum how to maka a telescope turn with high precision?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 709 subscribers
  • Views 12372 views
  • Users 0 members are here
  • telescope
  • dc motors
  • raspber
  • raspberry_pi
  • raspberry_pi_3_model_b_plus
  • arduino
Related

how to maka a telescope turn with high precision?

simon.ganne
simon.ganne over 8 years ago

Hey everyone, I'm preparing myself because I need to build a project next year and write a thesis about it. My project is an automated telescope. Now I was wondering how I could turn the telescope around with some kind of motors at a precision of at least 1 degree. Has anyone experience with this kind of stuff or someone who has an idea?

  • Sign in to reply
  • Cancel
Parents
  • schismata53
    schismata53 over 7 years ago

    I'm experimenting with telescope tracking at the moment. I've used a NEMA17 stepper motor with a 5:1 gearbox and used a DRV8825 driver controlled by Arduino. In theory you can make stepper motors more smooth using microstepping but in practice I've found it difficult to get the speed consistent. It surges for some reason. Perhaps I can improve it with a better driver or a higher gear ratio. You can get stepper motors with 100:1 gearboxes online.

     

    Regarding precision the moon is about 1/2 degree or 30 arcminutes. Venus at it's largest is about 1 arcminute. I would suggest for accurate tracking for astrophotography you need to aim for around 1 arcsecond. I.e. one step of the stepper motor is usually 1.8 degree which is 1.8 x 3600 = 6480 arcseconds. If you gear it down by a 1:100 gearbox you get 64.8 arcseconds. That should reduce further by the ratio of the output of your gearbox to the gear it is driving which depends on your design but let's say it 10:1 which gives you 6.48 arcseconds. That's not bad but would probably still be noticeable. It's roughly the separation of the double stars in Alpha Centauri. With 4x or 8x microstepping you would just make it if you could get your microstepping to be smooth.

     

    The precision of the equatorial axis is most important as it is the one that does the tracking. The declination is less so once you're on the object this axis doesn't move. If you don't have an equatorial mount you can track by moving both motors at the right speed (which is a little complicated) but even with perfect tracking the image slowly rotates which is a problem for astrophotography.

     

    I personally think that a motor to drive focus is more important than the declination axis. Whenever you try to change the focus manually you bump the telescope and have to wait for it to settle before you can see the results of your focusing unless it's a very stable telescope. If people with different eyesight are looking through it, each person needs to focus it for their own eye. Having said that I know motorised focusers exist but they're not common.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 7 years ago in reply to schismata53

    I am not sure why you would need to mess with the focus, I thought with the stars so far away it is focused to infinity or there abouts.

     

    regarding the motors, it sounds a bit like you have a lack of torque. Don't try to micro step too much, over 8 only makes movement sound smoother but adds no accuracy. (A common stepper is only 5% accurate on its primary step and you cant change that, add a heavy load like a telescope and it can easily ignore many of the micro-steps as they have no were near enough torque to move the stepper until they get to near a full step (4:1 or even 2:1)

     

    What power supply are you using ?, and what motors

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • schismata53
    schismata53 over 7 years ago in reply to Robert Peter Oakes

    I'm using Nema17 stepper motors and a 12 Volt battery and a poorly soldered circuit just containing the arduino and the stepper motor drivers. The voltage gets pulled down to 10 or 11 volts when I connect the arduino nano which I think is supposed to accept a 12 Volt input. So all in all a pretty lousy setup. I have ordered a variety of driver chips to try out and will be improving my power supply circuit. The TMC2130 'ultra silent' chip will be interesting as the DRV8825 can be quite noisy when attached to the telescope. Is a square wave from the arduino the best signal to drive the driver chip with?

     

    Another issue I'm curious about is how to stop back-current from the motors from destroying the driver chip. If someone pushes the telescope manually the stepper motor creates quite a bit of back current and I'm pretty sure I've blown up chips by doing that in the past.

     

    As you say the focal plane doesn't change when you are looking at distant objects but being able to control the focus without touching the telescope is desirable when you set focus in the first place, when you change eyepieces or when short-sighted people like myself take their glasses off and refocus to their eye. Also the thermal expansion of the telescope can affect the focus.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • schismata53
    schismata53 over 7 years ago in reply to Robert Peter Oakes

    I'm using Nema17 stepper motors and a 12 Volt battery and a poorly soldered circuit just containing the arduino and the stepper motor drivers. The voltage gets pulled down to 10 or 11 volts when I connect the arduino nano which I think is supposed to accept a 12 Volt input. So all in all a pretty lousy setup. I have ordered a variety of driver chips to try out and will be improving my power supply circuit. The TMC2130 'ultra silent' chip will be interesting as the DRV8825 can be quite noisy when attached to the telescope. Is a square wave from the arduino the best signal to drive the driver chip with?

     

    Another issue I'm curious about is how to stop back-current from the motors from destroying the driver chip. If someone pushes the telescope manually the stepper motor creates quite a bit of back current and I'm pretty sure I've blown up chips by doing that in the past.

     

    As you say the focal plane doesn't change when you are looking at distant objects but being able to control the focus without touching the telescope is desirable when you set focus in the first place, when you change eyepieces or when short-sighted people like myself take their glasses off and refocus to their eye. Also the thermal expansion of the telescope can affect the focus.