Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Wiring up a PIR to a PiFace Digital2
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 706 subscribers
  • Views 4160 views
  • Users 0 members are here
  • piface_digital pir
  • rasberry_pi_3_b_plus
Related

Wiring up a PIR to a PiFace Digital2

balanga
balanga over 7 years ago

Apologies for this newbie type question, but I can't figure out how to use inputs on a PiFace Digital2.... I would like to connect up a PIR to a to this device and have come across instructions here Review of PiFace Digital , which even has sample code, but it's not clear to me which wires go where.

 

Any guidance would be appreciated.

  • Sign in to reply
  • Cancel
  • Gough Lui
    Gough Lui over 7 years ago

    It would help if you could specify the type of PIR you are trying to use? Is it an alarm system type PIR that needs a 12V supply and has a set of NO/NC relay contacts? Or is it a 5V module of sorts that has a logic signal output?

     

    In general, you need to power the PIR (+ve and GND) and get a signal from the PIR. If the PIR outputs a logic level signal, you could use the digital inputs and connect the PIR output to one of them. If the PIR is a relay output, then you will need to configure a pull-up using resistors to provide an appropriate logic signal.

     

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • balanga
    balanga over 7 years ago in reply to Gough Lui

    It's one of these:-

    https://projects.raspberrypi.org/en/projects/physical-computing/13

     

    On mine the pins aren't labelled, but I assume they are standard as in https://howtomechatronics.com/wp-content/uploads/2015/09/PIR-Sensor-Pinout.jpg?x57244

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 7 years ago in reply to balanga

    I think you are correct about the pinout:

    image

    https://www.mpja.com/download/31227sc.pdf

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 7 years ago

    A lot of these PIR sensors will work on 3V3 and if the one you have is similar to the one Doug shows above then you should be able to feed the OUT signal directly to the PI

     

    I cant remember if the PIFace Dig 2 has level shifter, if it does them a more reliable 5V supply will also be OK

     

    But in a basic setup you would not need the PIFace Digital at all.

     

    I do have an older video showing how to wire and use the PIFace Digital 2 here https://www.hackster.io/peteroakes/piface-digital-2-on-a-rasberry-pi-2-and-windows-10-iot-3aa858  but it uses Windows 10 for IOT. the wiring will be the same

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 7 years ago in reply to Robert Peter Oakes

    The one above runs on a 5V supply but the output is only 3.3V.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • balanga
    balanga over 7 years ago in reply to dougw

    From my searches, I should connect:-

     

    VCC to GPIO pin 2

    OUT to GPIO pin 7

    GND to GPIO pin 6

     

    according to https://www.researchgate.net/profile/Zakaria_Rada2/publication/312218161/figure/fig3/AS:449572641218564@1484197878779/GP…

     

    but am unsure how to map these pins to the PiFace Digital2...

     

    Having said that this diagram https://projects-static.raspberrypi.org/projects/physical-computing/0cb2cbd34292a05a668aeea3f291ceb3c7d9cd83/en/images/p…  appears to have the pins inverted....

     

    This diagram http://www.piface.org.uk/static/img/piface_digital_2/pifacedigital2_diagram.png  show two possible locations for VCC and three possible locations for GND. Does it make any difference which I choose? And am I correct in thinking OUT must be one of the eight green terminals?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 7 years ago in reply to balanga

    Operating with and without the PiFace Digital is slightly different. The diagrams you have before are designed for direct GPIO interfacing rather than going through an I/O expander such as the PiFace Digital. The principles are, however, much the same.

     

    The VCC line should be connected to any of the 5V outputs from the PiFace Digital, the GND line should be connected to any of the GND lines on the PiFace Digital and the OUT line can be connected to any one of the input lines on the PiFace Digital. Your code should read the corresponding input line to find out the status of the PIR.

     

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • balanga
    balanga over 7 years ago in reply to Gough Lui

    I finally managed to get this working connecting the OUT pin to the terminal 0 of the input row.  I'm using the following code:-

     

    # Alarm program by Francesco Balsamo

    #

    # Using a PIR sensor with inverted logic

    #

     

     

    from time import sleep

     

     

    import pifacedigitalio as pfio

    # import piface.pfio as pfio

     

     

    pfio.init()

     

     

    while(True):

        for pin_number in range(0,4):

            if pfio.digital_read(pin_number) == 0:

                pfio.digital_write(pin_number+4,1) # Using only the leds

            else:

                pfio.digital_write(pin_number+4,0) # Disabling only the leds

    This switches on LEDs 7,6,5,4  of which 4 is toggled by the PIR, although I can't figure how the code is supposed to work at all...

     

    I guess this calls for some experimentation. At least I have managed to get the PIR to control one of the LEDs.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 7 years ago in reply to balanga

    The code is pretty simple:

    - while (True) runs the code block that follows infinitely.

    - for pin_number in range(0,4) basically repeats the code for every pin_number in this set (0, 1, 2, 3)

    - if pifo.digital_read(pin_number) == 0 basically says "is this input at pin_number low (as the PIR output goes low when it senses something)?"

    - pfio.digital_write(pin_number+4,1) basically says "lets make LED at pin_number+4 (e.g. for pin 0, then LED4 will) turn on"

    the other case is for if that isn't the case, it turns off the LED.

     

    This is a rather simple case of polling the input continuously ...

     

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • jomoenginer
    jomoenginer over 7 years ago in reply to Gough Lui

    The example that was referenced looks like a PiFace Digital rather than a Digital 2 but should be similar.  From my understanding, the first 4 (0-3) inputs/outputs are tied to the switches (S0-S3) so the example skips these to set LEDs 4-7 by offsetting the value from the 'for/range' loop with "pin_number+4" .  However, the "if" statement is only checking for inputs 0-3 which would be one of the switches or an input from 0-3 but then sets an LED, 4 plus pin_number (4-7), which seems odd.  The example also is using 4 PIR sensors, so if you have only 1 PIR sensor then you could remove the for range loop from the code example.

     

    If you want an output on say output 4, then you should put the Out from the PIR sensor to Input 4 on the Digital 2.   However, I found the inputs on the Digital 2 are tied to 5v which causes an issue with the Parallax PIR sensor so I place a 10K Ohn resistor between the input port I am using on the Digital 2 to ground (GND) to ensure the PIR reading is clean.  You can disable the pull-up on the input of the Digital 2 but that causes them to float so you would still have to to either tie it high or low depending on the device connected to the Digital 2.

     

    Reference to PiFace Digital inputs:

    https://pifacedigitalio.readthedocs.io/pifacedigital.html#inputs

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
>