Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum PiFace connection
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 706 subscribers
  • Views 3052 views
  • Users 0 members are here
  • piface control display
  • connection
  • raspberrypi3
Related

PiFace connection

cclegends
cclegends over 7 years ago

Hi E14 community, I just received my PiFace Control and Display. After I connect them to the GPIO pins and nothing appears / pops up. I've done install the library as well as module. Upon running sys info.py, the errors are :

 

Traceback (most recent call last):

  File "sysinfo.py", line 61, in <module>

    cad = pifacecad.PiFaceCAD()

  File "/usr/lib/python3/dist-packages/pifacecad/core.py", line 50, in __init__

    self.init_board()

  File "/usr/lib/python3/dist-packages/pifacecad/core.py", line 80, in init_board

    h=self.hardware_addr, b=self.bus, c=self.chip_select))

pifacecad.core.NoPiFaceCADDetectedError: No PiFace Control and Display board detected (hardware_addr=0, bus=0, chip_select=1).

 

 

Tried to search more information about this, other forums shows that the kernel update makes this display are not able to work. Is there any workaround to make this display working? Thanks.

  • Sign in to reply
  • Cancel
Parents
  • jomoenginer
    jomoenginer over 7 years ago

    This is what I have in the spi.py file

    /usr/lib/python3/dist-packages/pifacecommon/spi.py

     

        
    # create the spi transfer struct
        
    transfer = spi_ioc_transfer(
            
    tx_buf=ctypes.addressof(wbuffer),
            
    rx_buf=ctypes.addressof(rbuffer),
            
    len=ctypes.sizeof(wbuffer),
            
    speed_hz=ctypes.c_uint32(100000)
        
    )

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • cclegends
    cclegends over 7 years ago in reply to jomoenginer

    Updates, Thanks Jon for the code modification. Now the display power ups and working but there is a little hiccup. Where it can't display free memory on the display. The tracebacks are :

     

    Traceback (most recent call last):

      File "sysinfo.py", line 75, in <module>

        show_sysinfo()

      File "sysinfo.py", line 56, in show_sysinfo

        cad.lcd.write(":{}".format(get_my_free_mem()))

      File "sysinfo.py", line 35, in get_my_free_mem

        used_mem = float(run_cmd(USED_MEM_CMD))

    ValueError: could not convert string to float:

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • cclegends
    cclegends over 7 years ago in reply to jomoenginer

    Updates, Thanks Jon for the code modification. Now the display power ups and working but there is a little hiccup. Where it can't display free memory on the display. The tracebacks are :

     

    Traceback (most recent call last):

      File "sysinfo.py", line 75, in <module>

        show_sysinfo()

      File "sysinfo.py", line 56, in show_sysinfo

        cad.lcd.write(":{}".format(get_my_free_mem()))

      File "sysinfo.py", line 35, in get_my_free_mem

        used_mem = float(run_cmd(USED_MEM_CMD))

    ValueError: could not convert string to float:

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • jomoenginer
    jomoenginer over 7 years ago in reply to cclegends

    cclegends  wrote:

     

    Updates, Thanks Jon for the code modification. Now the display power ups and working but there is a little hiccup. Where it can't display free memory on the display. The tracebacks are :

     

    Traceback (most recent call last):

      File "sysinfo.py", line 75, in <module>

        show_sysinfo()

      File "sysinfo.py", line 56, in show_sysinfo

        cad.lcd.write(":{}".format(get_my_free_mem()))

      File "sysinfo.py", line 35, in get_my_free_mem

        used_mem = float(run_cmd(USED_MEM_CMD))

    ValueError: could not convert string to float:

    Is this working now?

     

    I inadvertently updated my config and ran into this issue as well.  I found the solution at the following:

    https://github.com/piface/pifacecad/issues/27

     

    This is what I have in my sysinfo.py file

    #USED_MEM_CMD = "free | grep '\-\/+' | awk '{print $3}'"
    USED_MEM_CMD = "free | grep 'Mem' | awk '{print $3}'"

     

    This is actually running on an older Pi B+ but I am still having an issue on a Pi 3 B+ with the sp.py entry.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jomoenginer
    jomoenginer over 7 years ago in reply to jomoenginer

    On my Pi 3 B+ I ended up having to download the pifaceacad code from their github repo and run the setup install from that to get it to work.  Just running from apt-get loaded some older code that did not like the spi.py entry.

     

    This is what I had seen prior to loaded the code from the github repo.

    python3 /usr/share/doc/python3-pifacecad/examples/sysinfo.py
    Traceback (most recent call last):
      File "/usr/share/doc/python3-pifacecad/examples/sysinfo.py", line 61, in <module>
        cad = pifacecad.PiFaceCAD()
      File "/usr/lib/python3/dist-packages/pifacecad/core.py", line 50, in __init__
        self.init_board()
      File "/usr/lib/python3/dist-packages/pifacecad/core.py", line 75, in init_board
        self.iocon.value = ioconfig
      File "/usr/lib/python3/dist-packages/pifacecommon/mcp23s17.py", line 238, in value
        self.chip.write(v, self.address)
      File "/usr/lib/python3/dist-packages/pifacecommon/mcp23s17.py", line 163, in write
        self._pyver_write(data, address)
      File "/usr/lib/python3/dist-packages/pifacecommon/mcp23s17.py", line 167, in _py3write
        self.spisend(bytes((ctrl_byte, address, data)))
      File "/usr/lib/python3/dist-packages/pifacecommon/spi.py", line 69, in spisend
        speed_hz=ctypes.c_uint32(self.speed_hz)
    AttributeError: 'PiFaceCAD' object has no attribute 'speed_hz'

     

     

    It is working now on both a RasPi B+ and a RasPi 3 B+.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • cclegends
    cclegends over 7 years ago in reply to jomoenginer

    Hi Jon, sorry for late updates. Thanks for the code, the screen is able to display and show the available memory. image

    jomoenginer  wrote:

     

    cclegends   wrote:

     

    Updates, Thanks Jon for the code modification. Now the display power ups and working but there is a little hiccup. Where it can't display free memory on the display. The tracebacks are :

     

    Traceback (most recent call last):

      File "sysinfo.py", line 75, in <module>

        show_sysinfo()

      File "sysinfo.py", line 56, in show_sysinfo

        cad.lcd.write(":{}".format(get_my_free_mem()))

      File "sysinfo.py", line 35, in get_my_free_mem

        used_mem = float(run_cmd(USED_MEM_CMD))

    ValueError: could not convert string to float:

    Is this working now?

     

    I inadvertently updated my config and ran into this issue as well.  I found the solution at the following:

    https://github.com/piface/pifacecad/issues/27 
    

     

    This is what I have in my sysinfo.py file

    #USED_MEM_CMD = "free | grep '\-\/+' | awk '{print $3}'"
    USED_MEM_CMD = "free | grep 'Mem' | awk '{print $3}'"
    

     

    This is actually running on an older Pi B+ but I am still having an issue on a Pi 3 B+ with the sp.py entry.