Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Establishing time in Raspbian Stretch Release 2019-04-08
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 707 subscribers
  • Views 3524 views
  • Users 0 members are here
  • raspberry_pi
Related

Establishing time in Raspbian Stretch Release 2019-04-08

colporteur
colporteur over 7 years ago

G'Day,

Does someone have the inside track on how time is established with the current version of Raspbian?

 

I'm looking for the details starting from power-up to power down. If you have some insight into fake-hwclock that would be useful also.

 

The references I have found refer to ntp as the seed source for time. I can find no ntp services or configuration files in the current release. I'm stumped on finding time. Unfortunately, I am away from my network currently and can't do more extensive testing. I was hoping someone had insight or a link I could do some reading.

 

Sean

  • Sign in to reply
  • Cancel
Parents
  • dougw
    dougw over 7 years ago

    Is your concern that your Pi is not set to the correct time, or do you want to improve on the time accuracy it keeps?

    If your Pi is connected to the Internet, on power up it will use Network Time Protocol to get the correct time.

    The Pi needs to be configured for your time zone in raspi-config under Localization Options.

    If you are not connected to the Internet, you may need to add an external RTC.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 7 years ago in reply to dougw

    G'Day,

    Time is functioning as expected. I am trying to understand how. If ntp is used as you suggest, when and how?

     

    I am currently experimenting with a technology call zymbit. In their write-up they suggest ntp time source is used on Pi's. They override it with the RTC. At one point ntp was used but on the current Raspbian version I can find no indication. i.e. no ntp.conf no ntp.services.

     

    All references on the internet associated with time predate the current release. I don't have my network tools to watch the output of a Pi booting. So i can't get answers.

     

    Sean

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 7 years ago in reply to colporteur

    I believe the latest Raspbian releases use systemd and it has its own lightweight ntp client, systemd-timesync. There should be a /etc/systemd/timesyncd.conf file and the timedatectl status command

    should produce useful information about the ntp server and time. You can google for more information about this service and command. I'm sure the time for fake-hwclock is initialized at boot and it may also be updated

    at regular intervals while Raspbian is running.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 7 years ago in reply to gdstew

    Thank you for the response. I will follow up on these bread crumbs to further my discovery.

     

    I suspected time sync relied on some form of ntp. At one point ntp daemon could be found and configured. Not finding the service listed lead me to believe some changes had been made. Suggesting Pi uses ntp for time sync is correct but details I found seem to refer to the old method and not what is currently used.

     

    Sean

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 7 years ago in reply to colporteur

    Even if the raspberry would use NTP to get the time that would not automatically imply that the NTP package needs to be installed. Especially when you don't need a super precise time estimate, a primitive NTP client could be something like 20 lines-of-code. So after deciding: "we're going to do NTP for the time", it can be either: "lets use ntpdate, then we don't have to write any code", or "lets just write our own client, it's less than 20 lines..." Both decisions have their merit.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 7 years ago in reply to rew

    My frustration is how the meaning of terms like ntp are watered down.

     

    I acknowledge the application of ntp is diverse. Why use CPU cycles to run a daemon when a kick in the pants to adjust time every few minutes is acceptable. As an individual that was once responsible for supporting time in a telecommunication environment the term ntp has a comprehensive meaning.

     

    How ntp is applied in Raspberry Pi appears to have changed. When google searches return ntp results from a year ago that suggest ntp.conf, it has the potential to confuse the Raspberry Pi'er using todays O/S. 

     

    Sean

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 7 years ago in reply to colporteur

    I share your frustration. The reason my response was so sparse on information was that I don't care for systemd at all. On of the biggest reasons is that it has

    a really bad case of feature creep so much so that what was originally touted as a new and improved init system now has 1.2 million lines of code. A little over

    a year ago I swapped distributions for my home computers from Debian which uses systemd to Devuan which doesn't but I still can't just ignore it. So anytime

    somebody says they can't find some program or configuration file that should (must?) exist the first thing I google for is a systemd version and this is how I

    found systemd-timesync.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 7 years ago in reply to gdstew

    Thanks for your insight. I grew up with writing machine language code to maximize memory. Efficient coding no longer appears to be a concern.

    Sean

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • jomoenginer
    jomoenginer over 7 years ago in reply to gdstew

    This is not a Raspbian thing but a Debian Stretch thing considering Raspbian is pulled from the Debian source.  Stretch does not use ntp but rather systemd-timesyncd.

     

    https://manpages.debian.org/stretch/systemd/systemd-timesyncd.service.8.en.html

    https://manpages.debian.org/stretch/systemd/timesyncd.conf.5.en.html

     

    However, to understand what is new in Raspbian you can look through the Readme for the release:

    http://downloads.raspberrypi.org/raspbian/release_notes.txt

     

    Or Debian Release notes:

    https://www.debian.org/releases/stable/armhf/release-notes/

     

    Welcome to Linux.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 7 years ago in reply to jomoenginer

    Yes it is a Raspbian thing, Devuan is Debian stretch without systemd and there are seven other main Linux distributions that do not use systemd (source

    wikipedia). However, given the long time use of the Debian code base, the effort required to get stretch to work without systemd (it took the Devuan people

    almost a year to get to a fully working 1.0), and the user space environment that has grown up around it, I can understand why it would not be the preferred

    path for Raspbian. Devuan also has a Raspberry Pi version that I installed and did some preliminary testing with almost a year ago and although it worked

    OK it was not up to par with Raspbian in a few areas. What I would really like to see is a full fork of Raspbian to Devuan but due to the effort required and

    the resources available to the Devuan people I don't think this will happen any time soon.

     

    Sean,

     

    I am a long time assembly language guy mainly writing code for microcontrollers (mostly 8051 derivatives) for PBX phones and other telecom equipment

    so I know exactly where you are coming from. I've also used C extensively for writing drivers for boards I've designed and other support/test programs.

    You may want to look into the Raspberry Pi version of Devuan if you would prefer a more "traditional" version of Linux.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jomoenginer
    jomoenginer over 7 years ago in reply to gdstew

    Debian is the main distro; all derivatives of it are just fork distros.

     

    Devuan sounds like it was created by folks that don't want to move forward with the rest of the Linux world.  Fedora runs into this as well where Red Hat 7 / CentOS 7 implement enough changes from 6.x that it causes havoc for some folks.   I had seen the same issue when Solaris went from 9 to 10.  OS evolution is fun.

     

    I suppose you could always fork Debian and create you own distro configured the way you want it.

     

    Or just stop systemd-timesyncd from running.

    https://stackoverflow.com/questions/43093636/stop-timesyncd-from-polling-hard-coded-debian-timeservers

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 7 years ago in reply to jomoenginer

    Thanks for the links, I look forward to the read. I'm interest in the documentation on development of the application. My search criteria didn't return much in the way of results.

     

    Sean

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • colporteur
    colporteur over 7 years ago in reply to jomoenginer

    Thanks for the links, I look forward to the read. I'm interest in the documentation on development of the application. My search criteria didn't return much in the way of results.

     

    Sean