Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum What would you like to see tested on the Raspberry Pi 4?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 50 replies
  • Subscribers 713 subscribers
  • Views 7607 views
  • Users 0 members are here
  • raspberry pi 4 testing
Related

What would you like to see tested on the Raspberry Pi 4?

cstanton
cstanton over 7 years ago

We have a couple of these in the office that we can run software / test some things on - so what would you like to see tested on the hardware that would help to swing the decision for you as to whether or not it's worth it?

 

I've seen a few questions about Sega Rally running on MAME, questions about h264 encoding, realtime transcoding - for some of these I'd have to find the software/setup but it's certainly do-able.

 

So let me know, what do you want to see tested on the Pi 4?

  • Sign in to reply
  • Cancel
  • shabaz
    shabaz over 7 years ago

    Hi Christopher,

     

    This is not maybe a test, but maybe something that could be queried from RPF.. it concerns the BLE interfacing from the SoC.

    In the past, the UART that it used required the other UART (that could be used as a console) to vary in baudrate, unless the core speed was fixed.

    It is the issue discussed here: https://www.raspberrypi.org/documentation/configuration/uart.md

     

    I was wondering, is that now resolved in Pi 4, i.e. can we have a UART for console that does not vary in baud rate, and have the BLE working.

    The reason is, I would always want the UART pins exposed on the 40-way header to permanently provide console access, but with a fixed baudrate, and without fixing core speed, and have bluetooth functioning.

    It may be fixed on Pi 4's new chip, I just don't know. Either way, it would be handy to know if the behaviour in this area is similar to earlier Pi's or not.

     

    Also, I drew this diagram, now old: Raspberry Pi 3 Block Diagram (mainly through guesswork). It would be nice to update it for Pi 4, I don't mind having a shot at it, but would be good if someone with Pi hardware knowledge could double-check it. I find such block diagrams useful, for giving a quick overview of what the Pi 4 is about.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 7 years ago in reply to shabaz

    Just FYI: This sounds plausible: The GPIO module is probably clocked at that 250Mhz. On simpler ARM processors like the STM32 family the same happens: the CPU core runs at some frequency and then you get a bunch of choices for the IO module clocks and bus clocks. Sometimes completely separate from the CPU clock sometimes your choice is restricted to "div2" or "div 1 or div2 as long as the result is below xxx". For the BCM2711 hardware running the IO modules at 250MHz base clock sounds reasonable.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 7 years ago in reply to shabaz

    I remember / am familiar with this issue, I think there was/is a way to check this by interrogating the hardware from what I recall. I suspect this hasn't changed.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • luislabmo
    luislabmo over 7 years ago

    I know this is probably a bad suggestion but how about running DOOM!. Haven't seen it running on an RPi 4B ........ yet image

    image

    Luis

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 7 years ago in reply to luislabmo

    The question here is, is DOSBox acceptable, or recompiled for linux/other OS ?

     

    Though I doubt I can get Doom 3 running image

     

    Haha.. I was wrong, this looks do-able

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • jack.chaney56
    jack.chaney56 over 7 years ago

    Picking a random Pi forum for this. Saw a few of my favorite respondents, so this was the winner. I wanted to note the two changes to Pi-4 that cause me some grief (and re purchasing). First is using mini-HDMI for the display cables. I understand this is probably for real estate reasons. Would have preferred a stacked plug design, akin to the USBs, and kept the HDMI the same size (at least for one monitor).  Second is changing up the power input to USB-C, with the new power requirements as well, make it so the sourcing is very limited.

    I am able to make all the necessary adjustments to my workbench, but it would have been nice to have a heads up prior to release. Also, selling out on the day of announced release is a little disheartening. By the time I got the approval to purchase, they were all gone. (wait list)

     

    Jack

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • luislabmo
    luislabmo over 7 years ago in reply to cstanton

    Well there you have some options image, and could get extra points if you run Jedi Knight II image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 7 years ago

    Does throttling due to temperature adversely affect 4K video quality/performance?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • donjr
    donjr over 7 years ago

    Using it with a PI 7" Display. I will try it again but there is an documentation issue in that the board supplied with the 7" display is used to power the PI but I doubt that it supplies 3.5 Amps. Also, it is back to the old mini USB power. Do I power the display separately? Should I power the it from the pi? Still researching it but my first attempt was unsuccessful. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 7 years ago in reply to jack.chaney56

    Sure, and what would you want tested on the hardware?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>