Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi 5 FAQs How can I connect a battery for the Real Time Clock (RTC) on the Raspberry Pi 5?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 1 reply
  • Subscribers 408 subscribers
  • Views 5597 views
  • Users 0 members are here
  • raspberry pi 5 battery
  • real time clock
  • raspberry pi 5
  • rtc
Related

How can I connect a battery for the Real Time Clock (RTC) on the Raspberry Pi 5?

cstanton
cstanton over 3 years ago

Now that I no longer have to rely on Network Time Protocol (NTP) to retain the correct time on my Raspberry Pi, how do I connect a battery?

  • Sign in to reply
  • Cancel
  • cstanton
    +1 cstanton over 3 years ago

    The Raspberry Pi 5 has a location where a battery can be connected.

    J5 allows for a battery to be connected using a pre-configured cable assembly with the battery.

    image

    This will be available soon.

    This means to set and change or check the time you can use the command hwclock.

    J2 has an unpopulated 2-pin header allowing for any type of connection to be soldered to the board, a jumper header or otherwise, also functioning as a power switch when connected together.

    There are important notes about connecting a battery:

    "We do not recommend using a primary lithium cell for the RTC, as it has a trickle charge circuit which is disabled by default. If enabled, this will kill the cell quickly. The official battery part is a rechargeable lithium manganese coin cell, with a pre-fitted two-pin JST plug and an adhesive mounting pad. This is suitable for powering the Raspberry Pi 5 RTC when the main power supply for the board is disconnected, with a power-off current draw measuring in single-digit µA, giving a retention time that can be measured in months."

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer