Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Files Assembled Gertboard Software (Jan 2013)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Next
  • Previous
  • Share
  • More
  • Cancel
  • Author Author: joeman
  • Views 4992 views
  • Downloads 172 downloads
  • Likes 0 likes
  • Comments 17 comments
Toptech-Voices
Related
Recommended

Assembled Gertboard Software (Jan 2013)

Download Software for the Assembled Gertboard.

  • the
  • download
  • raspberry_pi
  • gertboard.
  • for
  • assembled
  • software
joeman
joeman
  • 30 Jan 2013
  • 172 Downloads
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 13 years ago in reply to alanwood +1
    Hi Alan, thanks again for the help. Got the software, and ran buttons and leds, this is way cool! Next stop, A/D and D/A Bill
  • jamespi
    jamespi over 10 years ago in reply to wmbell65

    @William_BellThe gertboard MUST face so that it covers the yellow video port otherwise it won't work

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to wmbell65

    The gertboard actually faces away from the USB ports. Notice the square box on the J1 with the little dot. That has to line up with P1 and the little square that is on the Pi Board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • wmbell65
    wmbell65 over 12 years ago

    Hi all,

    I am running into issues with the basic tests for the buttons and leds... For the button test, nothing seems to happen.. The wiring diagram for the button test appears to be correct, and I added the jumpers for outputs B1 - B3 on the pins above U3... With this configuration I would expect leds D1 - D3 to light up when I press one of the buttons, but nothing happens. I also have a jumper on pins 1&2 of J7 so things should be Ok....

    When I run the led test I am only using 7 wires for (J3) B1- B7 going to GP25, GP24, GP23.. I connected jumpers for B1 - B7 on U3 & U4... when I have the J7 jumper in place on pins 1&2 nothing happens. When I remove the J7 Jumper all of the LEDs flash through the patterns... The fact that the board flashes without the J7 jumper implies that the board itself is OK.... I've had the Gertboard attached directly to my Pi and I've also tried it via the PiFace rack, thinking that the board is not connected properly when directly on the Pi GPIO connector - I have a RaspberryPi model B and the board seems to not go into place fully due to the USB riser.. I've tried both the C code and the Python code with the same results.

     

    As an aside, when running these tests, CPU on the Pi goes to 100% - no doubt due to the tight loop that the code runs in

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to alanwood

    Hi Allen, yest the Gertboard was connected.  Apparently the Rpi could not find avrsetup.  Maybe I should go back and try the install again from the very beginning?

     

    Bill

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • alanwood
    alanwood over 13 years ago in reply to e14 Contributor

    Hello Bill,

     

    Have you tried connecting the Gertboard and the programming wires before running setup? Perhaps the software needs to see it there to complete.

     

    Cheers,

    Alan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>