Raspberry Pi Projects
  • Products
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog Adding Wireless Capability to Custom RP2040/RP2350 Projects: Pi Radio Module 2 - Anyone tried it?
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 30 Jun 2026 4:29 PM Date Created
  • Views 341 views
  • Likes 10 likes
  • Comments 11 comments
  • RP2350
  • Pi Pico W
  • RM2
  • wlan
  • 2.4ghz
  • wireless lan
  • rpiexpert
  • rp2040
  • 2.4 ghz
  • wireless
  • Pi Radio Module 2
  • RMC20452T
  • pi pico
Related
Recommended

Adding Wireless Capability to Custom RP2040/RP2350 Projects: Pi Radio Module 2 - Anyone tried it?

shabaz
shabaz
30 Jun 2026

I just noticed the other day that this thing existed; it supports 2.4 GHz wireless (not 5 GHz), and Bluetooth LE (BLE); the manufacturer part code is RMC20452T , also known as RM2 and it costs about $4. 

image

Underside; the board is 16.5 x 14.5 mm in size (but you'll need some space for a ground plane):

image

The RM2 is useful for custom RP2040 or RP2350 projects where WLAN (again, annoyingly just 2.4 GHz)/BLE is needed; not useful for anything else as far as I'm aware. From a software perspective, coding should be no different to using a Pi Pico W.

The RM2 should be very easy to drop into KiCad projects, since the footprint/symbol/3D model is available.

The RM2 datasheet (PDF) seems easy enough to follow, but is extremely basic; and I found it a bit confusing regarding a 'reset' line it mentions, but the text is silent on that later. It is not clear what line that refers to.

There are no suggested layouts (there might be if you sign an NDA, I wasn't willing to do that), the PDF just states a good ground plane is needed, and shows the copper fill keepout area.

Note that there isn't a version with antenna connector, however, one workaround would be to place the module on a PCB (large enough to have a ground plane, or perhaps use parts of an enclosure for that) and run the interface wires a short distance to the microcontroller, if you needed the antenna positioned somewhere not feasible on the main circuit board. Personally, if it were me, I would try to use the module in that way, i.e. on a separate PCB with short wires, before integrating onto a larger PCB; I'd much rather have it separately and position it for the best signal.

Anyone see a use for this module? Or if anyone has seen it in use, any photos showing how it was deployed in the design would be great to see. 

At some point I'd like to experiment with creating a PCB for it (EDIT: I've now created one), but I was wondering if anyone else had given it a shot, or were planning to, or would like to!

Thanks for reading.

 

Example Circuit and PCB

Here's the circuit I used:

image

50 x 23mm PCB render, all passives are 0603-sized, and the LED can be 0805:

image

The Gerber files, and KiCad source files are downloadable here:

export_gerber_wlan_ble_rev1.zip

rm2_wlan_board.zip

  • Sign in to reply

Top Comments

  • shabaz
    shabaz 18 days ago +1
    Here's a board attempt with two wireless modules (both don't need to be populated). Circuit diagram: The unusual board shape is needed to fit over the main PCB: The Sub-1GHz module (eByte E07…
  • embeddedguy
    embeddedguy 1 month ago in reply to shabaz

    haha, nice tiny little device, but the TX power is bit low it is 12dbm max. I have seen some modules with +20dbm and that will increase the comm. range for sure. Another thing that I would look is how to make P2P link secure and hackproof. That way I am good to go.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • wolfgangfriedrich
    wolfgangfriedrich 1 month ago

    When I saw this, my first thought was: put it on some sort of m.2 carrier for a more universal wireless card. But the interface does not seem to be fully compatible with whatever m.2 has to offer. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz 1 month ago in reply to embeddedguy

    Or connect both! For example LoRaWAN with Pi Pico:   community.element14.com/.../test-lorawan-thing-code-ported-for-raspberry-pico   .

    Since Winter I've been running the home heating (not right now since it's extremely hot!) using a low-cost TI CC1101 module connected to a Pi Pico W. (I used that TI part because it is quite flexible radio-protocol-wise, and chances are high to interwork that to existing systems if they are not using LoRa). The WiFi was used to obtain a weather report, and then the CC1101 issued on/off instructions to the boiler.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz 1 month ago in reply to veluv01

    Ah, great, that will be very helpful to confirm the connections! Funnily enough I ordered a Pimoroni Pico Plus 2 but missed that there was a W variant of that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • veluv01
    veluv01 1 month ago

    image

    The pimoroni pico plus 2W has it.The schematic is available for it.

    image

    Apparently, it can only be used with the rp2040 and rp2350's.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>