Raspberry Pi Projects
  • Products
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog Adding Wireless Capability to Custom RP2040/RP2350 Projects: Pi Radio Module 2 - Anyone tried it?
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 30 Jun 2026 4:29 PM Date Created
  • Views 342 views
  • Likes 10 likes
  • Comments 11 comments
  • RP2350
  • Pi Pico W
  • RM2
  • wlan
  • 2.4ghz
  • wireless lan
  • rpiexpert
  • rp2040
  • 2.4 ghz
  • wireless
  • Pi Radio Module 2
  • RMC20452T
  • pi pico
Related
Recommended

Adding Wireless Capability to Custom RP2040/RP2350 Projects: Pi Radio Module 2 - Anyone tried it?

shabaz
shabaz
30 Jun 2026

I just noticed the other day that this thing existed; it supports 2.4 GHz wireless (not 5 GHz), and Bluetooth LE (BLE); the manufacturer part code is RMC20452T , also known as RM2 and it costs about $4. 

image

Underside; the board is 16.5 x 14.5 mm in size (but you'll need some space for a ground plane):

image

The RM2 is useful for custom RP2040 or RP2350 projects where WLAN (again, annoyingly just 2.4 GHz)/BLE is needed; not useful for anything else as far as I'm aware. From a software perspective, coding should be no different to using a Pi Pico W.

The RM2 should be very easy to drop into KiCad projects, since the footprint/symbol/3D model is available.

The RM2 datasheet (PDF) seems easy enough to follow, but is extremely basic; and I found it a bit confusing regarding a 'reset' line it mentions, but the text is silent on that later. It is not clear what line that refers to.

There are no suggested layouts (there might be if you sign an NDA, I wasn't willing to do that), the PDF just states a good ground plane is needed, and shows the copper fill keepout area.

Note that there isn't a version with antenna connector, however, one workaround would be to place the module on a PCB (large enough to have a ground plane, or perhaps use parts of an enclosure for that) and run the interface wires a short distance to the microcontroller, if you needed the antenna positioned somewhere not feasible on the main circuit board. Personally, if it were me, I would try to use the module in that way, i.e. on a separate PCB with short wires, before integrating onto a larger PCB; I'd much rather have it separately and position it for the best signal.

Anyone see a use for this module? Or if anyone has seen it in use, any photos showing how it was deployed in the design would be great to see. 

At some point I'd like to experiment with creating a PCB for it (EDIT: I've now created one), but I was wondering if anyone else had given it a shot, or were planning to, or would like to!

Thanks for reading.

 

Example Circuit and PCB

Here's the circuit I used:

image

50 x 23mm PCB render, all passives are 0603-sized, and the LED can be 0805:

image

The Gerber files, and KiCad source files are downloadable here:

export_gerber_wlan_ble_rev1.zip

rm2_wlan_board.zip

  • Sign in to reply

Top Comments

  • shabaz
    shabaz 18 days ago +1
    Here's a board attempt with two wireless modules (both don't need to be populated). Circuit diagram: The unusual board shape is needed to fit over the main PCB: The Sub-1GHz module (eByte E07…
  • embeddedguy
    embeddedguy 1 month ago

    Would be nice to add some sub-ghz module. You can have better range with that.!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<