Raspberry Pi Projects
  • Products & Partners
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog Converting bulk samples from Data Acquisition Board for Pi Pico with C++ STL
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 15 Dec 2023 11:33 AM Date Created
  • Views 1186 views
  • Likes 8 likes
  • Comments 1 comment
  • ADC (Analog-to-Digital Converter)
  • pico
  • data acquisition
  • stl
  • ads1115
  • rp2040
  • daq
  • pico-eurocard
  • raspberry_pi_projects
  • adc
  • test&measurement
Related
Recommended

Converting bulk samples from Data Acquisition Board for Pi Pico with C++ STL

Jan Cumps
Jan Cumps
15 Dec 2023

 shabaz designed a Data Acquisition Board for Pi Pico . In the first post, I used it in continuous sample mode. I took 1 second worth of samples, in 860 samples per second mode. In the second blog, I averaged those samples, using C++ STL constructs. Now I'm going to use STL to convert all raw samples to voltage.

Actions to do on the raw ADC buffer:

  • swap the bytes. The ADS1115 delivers them in the wrong order for Pico math. (done in previous post)
  • create a new array with the converted voltage values.

image

Create an array of doubles from the 2-compliment uint32_t buffer with a Transform and a Callable

A callable is a function that can be invoked while iterating a container, that (in this case) will apply on all values of a dataset. I'm using shabaz ' to_volts() as a callable:

double to_volts(uint8_t boardnum, uint8_t chan, int16_t raw) {
double v;
v = (double)raw * (adc_range[boardnum][chan] / 32768.0); // convert the raw value to volts present at the ADC input
v = v / opamp_gain[boardnum][chan]; // adjust for opamp gain
return(v);
}

Here is how STL can call this on all elements of my 860 samples buffer, and store the values in an array of doubles::

 // convert every value to voltage
double volts[SAMPLES];
std::transform(std::begin(buf), std::end(buf), std::begin(volts),
[](uint16_t u){ return to_volts(BOARD0, 0, u); });

The std::begin() and std::end() iterators work on a common buffer. std::for_transform() will iterate from begin to end, call the to_volts() on each element in that range. Result of each call is stored in volts (array of doubles) using the std::begin(volts) iterator.

The use of the iterators, transform and callable function, and other STL functions did not add noticeable resource use.
Enjoy.

  • Sign in to reply
  • DAB
    DAB over 2 years ago

    Nice update Jan.