Raspberry Pi Projects
  • Products & Partners
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog Low-cost 8V 6A Power Supply for motor projects : )
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 14 Dec 2021 3:38 PM Date Created
  • Views 6598 views
  • Likes 8 likes
  • Comments 3 comments
Related
Recommended

Low-cost 8V 6A Power Supply for motor projects : )

shabaz
shabaz
14 Dec 2021

This Power Supply has been available for a while perhaps, but I just noticed it now, it is just £11+tax, which is very good for a (hopefully) safe power brick. The information here is just informational : ) use caution with supplies capable of high current output.

image

Region-specific variants:

Power supply with UK plug    Power supply with EU plug     Power supply with Aussie plug    Power supply with US plug

It has a normal 5.5/2.1mm barrel connector, center positive, and 1.5m long lead. A fairly significant annoyance (forgivable at the price) is that it doesn't use C8 (figure-8) or larger IEC connector on the mains supply side. It doesn't have a power LED either, which would be convenient.

Anyway, at 8V output it looks ideal for small motorized projects (I think Lego and Fischertechnik both use this ballpark voltage for their motors), or even 7805 voltage regulator based projects where 7.5 or 8V is a nice input voltage for them. I've briefly looked at the output and it may need a capacitor on the output to smooth things a bit (since this power supply is manufactured for use with motors, you'd expect a capacitor across the power rails anyway, close to the H-bridge) or a linear voltage regulator.

Anyway, here is the output when supplying 1 amp (I used a speaker simulator for the load, it is 8 ohm). 

The scale is 100 mV/division, so the switching noise amplitude is about 300 mV p-p:

image

Here is the output with a low-cost 1000 uF 16V electrolytic capacitor across the supply:

image

Adjusting the vertical resolution to 20 mV/division:

image

 

From the specifications in the datasheet, it appears protected from output shorts:

image

Anyway, I think it could be a handy power supply to have, especially with the high current capability.

On the safety topic (with no liability, these suggestions are just being given for free as things to think about) I believe it would be a good idea to use some protection (perhaps a polyswitch) for at least the low power portion of circuits. Something like RXEF010S  would be handy, costs about £0.50 and could operate a microcontroller and small display for instance. Also, if you are powering actual motors/hobby servos etc., then bear in mind that motors do not like being stalled, so keep an eye on them, and implement some protection if possible to handle the stall condition, because even though the power supply may be protected, the rest of your circuit and nearby possessions/property may not be.

Flame retardant wiring would also be a good idea (definitely not e-bay wire!).

Thanks for reading.

  • Sign in to reply
  • scottiebabe
    scottiebabe over 4 years ago

    That is a great find! I am excited to see what the USB-C revolution will bring once some of the higher output voltage/power supplies make it into extremely high volume manufacture. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 4 years ago in reply to Fred27

    Hi Fred,

    Thanks for the info and link! Interesting board, great that it can support 4 motors. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Fred27
    Fred27 over 4 years ago

    This power supply is intended for use with the Build HAT so definitely intended for use with Lego motors. Unfortunately it wasn't yet available when I bought mine.