Products
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
Raspberry Pi Projects
  • Products
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog Min and Max bulk samples from Data Acquisition Board for Pi Pico with C++ STL
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 16 Dec 2023 5:31 PM Date Created
  • Views 1449 views
  • Likes 7 likes
  • Comments 2 comments
  • ADC (Analog-to-Digital Converter)
  • pico
  • data acquisition
  • stl
  • ads1115
  • daq
  • pico-eurocard
  • raspberry_pi_projects
  • adc
  • test&measurement
Related
Recommended

Min and Max bulk samples from Data Acquisition Board for Pi Pico with C++ STL

Jan Cumps
Jan Cumps
16 Dec 2023

 shabaz designed a Data Acquisition Board for Pi Pico . In the first post, I used it in continuous sample mode. I took 1 second worth of samples, in 860 samples per second mode.

In this post, I use C++ STL constructs to find the minimum and maximum value. I'm using all the code from the 1st post, to collect 860 samples in a buffer.

image

Actions to do on that buffer:

  • swap the bytes. The ADS1115 delivers them in the wrong order for Pico math (done in  Average bulk samples from Data Acquisition Board for Pi Pico with C++ STL )
  • use std::minmax_element() to fetch both in a std::pair.

In the original program, the buffer is a plain C array, not an STL container. I don't change that. I use STL iterators that can work on such a continuous buffer.

Find the min and max value with an STL algorithm

STL has an algorithm that finds both values in a single call: std::minmax_element(). It returns a pair of values, where first represents the min value, and second the max.

auto minmax = std::minmax_element(std::begin(buf), std::end(buf));
printf("MIN = %.7f V\n", to_volts(BOARD0, 0, *minmax.first));
printf("MAX = %.7f V\n", to_volts(BOARD0, 0, *minmax.second));

Full source of the main function. There are more functions that can be STL'd (the to_volts() conversion, printing the results, ...). For this post, I wanted to focus on the two calls related to averaging.

// ************ main function *******************
int main(void) {

    stdio_init_all();

    board_init();

    build_data_rate(BOARD0, DR_860);
    build_gain(BOARD0, AIN1, GAIN_2_048); // +- 2.048V

    #define SAMPLES 860
//    #define SAMPLES 10

    uint16_t buf[SAMPLES];
    
    build_cont_conversion(0);
    adc_set_mux(BOARD0,0,false);
    adc_enable_rdy(0);

    uint8_t* buf8_ptr = (uint8_t*)buf;
    *buf8_ptr = ADS1115_REG_CONVERSION;
    i2c_write_blocking(i2c_port, adc_addr[BOARD0], buf8_ptr, 1, false);

    uint8_t* buf8_end_ptr = ((uint8_t*)buf) + (sizeof buf);
    rdy = false;

    while (buf8_ptr < buf8_end_ptr) {
        if (rdy) {
            rdy = false;
            i2c_read_blocking(i2c_port, adc_addr[BOARD0], buf8_ptr, 2, false);
            buf8_ptr += 2;
        }
    }

    // buffer bytes will now get swapped, 
    // and that's needed for the next actions
    // use stl iterator and lambda function
    std::for_each(std::begin(buf), std::end(buf), [](uint16_t& u){ u = u >> 8 | u << 8; }); // swap bytes

    // prereq: bytes are already swapped

    uint16_t statistic;
    // average
    statistic = std::accumulate(std::begin(buf), std::end(buf), 0.0) / std::size(buf);
    // std::cout << "AVG = " << to_volts(BOARD0, 0, statistic) <<" V" << std::endl;
    printf("AING = %.7f V\n", to_volts(BOARD0, 0, statistic));
    // min and max
    auto minmax = std::minmax_element(std::begin(buf), std::end(buf));
    printf("MIN = %.7f V\n", to_volts(BOARD0, 0, *minmax.first));
    printf("MAX = %.7f V\n", to_volts(BOARD0, 0, *minmax.second));

    // convert every value to voltage
    double volts[SAMPLES];
    std::transform(std::begin(buf), std::end(buf), std::begin(volts),
               [](uint16_t u){ return to_volts(BOARD0, 0, u); });


    std::for_each(std::begin(volts), std::end(volts), [](double& d){ 
        printf("AIN1 = %.7f V\n", d);
    }); 

    while (FOREVER) {}
}

Check the first  post for the source of the functions called in this example.

The use of the iterators, minmax_elements() and other STL functions did not add noticeable resource use.
Enjoy.

  • Sign in to reply
  • shabaz
    shabaz over 2 years ago

    Impressive that STL features work with decent performance on the Pico! And the code is readable (a lot of STL'd code can look extremely confusing at first). I read somewhere Arduino does not support it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 2 years ago

    Nice update Jan.