Raspberry Pi Projects
  • Products & Partners
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog Pi Hiker - Raspberry Pi Geocaching System
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: bobalexander
  • Date Created: 13 Aug 2015 3:16 PM Date Created
  • Views 1376 views
  • Likes 6 likes
  • Comments 0 comments
  • microstack_gps
  • geocaching
  • raspberry_pi_gps_kit
  • the_magpi
  • raspberry_pi_2
  • raspberry_pi_geocaching
  • geolocation
  • raspberry_pi_projects
  • geo_location
Related
Recommended

Pi Hiker - Raspberry Pi Geocaching System

bobalexander
bobalexander
13 Aug 2015

Raspberry Pi Geocaching System (Pi Hiker)

Author: Bob Alexander


A kid friendly, high accuracy geocaching platform.

  • Accuracy of the GPS location could be improved by putting the L80 into 10Hz mode and then performing an averaging and filtering function such as outlined in this paper:

          An Effective Approach to Improving Low-Cost GPS Positioning Accuracy in Real-Time Navigation

  • With the addition of a magnetometer, a direction indicator could be added that would not be dependent upon movement to show the target azimuth.
  • We would utilize our Makerspace's 3D printer to print an enclosure for this platform to sit in such that it could be used by children.
  • I think the Pi 2 is a good candidate for this project as it should have the horsepower to perform the averaging function and be able to utilize a database of geocaches downloaded before the trip.


Journal:

Received notification that I won a Raspberry Pi 2 GPS kit from Christopher Stanton on July 17th 2015.

Received kit in mail August 4th 2015.

20150804_213133.jpgimage

20150804_213146.jpg20150804_213205.jpg

20150804_213347.jpg

Look at all the goodies!!

20150804_213940.jpg

Starting to assemble...

20150804_232208.jpg

I soldered the right angle header pins to the PiFace GPIO Duplication Board Shim and tacked the shim in place on the Raspberry Pi 40 pin header board by soldering the four outermost pads as I applied pressure against the shim. It was a little loose and didn’t maintain good contact without this. Yes, I soldered the pins on the wrong side and the silk screen is backwards. Oh well. A quick assembly sheet would be nice to prevent this as it wasn’t obvious to me - NOOB!

20150804_232902.jpg

The footprint is a lot bigger than I expected! How am I going to house all this?!

The Microstack is definitely a nice system for prototyping but I don’t think it will work for a ‘finished’ project.

Ben Heck style chopping/hacking in store?

20150804_232913.jpg

Maybe a game pad style case will accommodate the assembly as is? It will need to accommodate a 1S 3.7V battery - perhaps a 5,000mAh.

G910-gamepad-bluetooth-controller-side-android-racing.jpg

20150804_233259.jpg

Connected to GPS antenna sitting on the window sill. Retractable reel for the GPS antenna?

20150804_233902.jpg

Ready to power up! Note the DVI-HDMI adaptor for my DVI only monitor.

20150804_233913.jpg

It works!

20150805_001330.jpg

After downloading the PiFace Control and Display software and enabling the SPI bus I ran the sysinfo demo.

20150805_002419.jpg

Just a quick tweak and it displays my local weather!

August 5th 2015: GPS testing

Following along with Christopher Stanton’s blog:

Putting Together the Pieces - Raspberry Pi 2 GPS Geocaching Project


After not having luck with

cat /dev/ttyAMA0

and ‘cgps -s’ just returning “cgps: GPS timeout”

I unplugged the PiFace CAD and moved the GPS Microstack to the direct connection instead of going through the shim (after powering off the pi).

20150805_222748.jpg


After booting back up and waiting for the GPS to initialize, I reran ‘cgps -s’ and BINGO!

┌───────────────────────────────────────────┐┌─────────────────────────────────┐

│    Time:       2015-08-06T02:07:10.000Z   ││PRN:   Elev:  Azim:  SNR:  Used: │

│    Latitude:    3X.650558 N               ││  15    78    169    41      Y   │

│    Longitude:   7Y.667636 W               ││  20    71    001    32      Y   │

│    Altitude:   214.9 m                    ││  21    45    311    29      Y   │

│    Speed:      0.4 kph                    ││  29    44    220    36      Y   │

│    Heading:    252.9 deg (true)           ││  18    26    274    36      Y   │

│    Climb:      0.0 m/min                  ││  24    08    163    00      N   │

│    Status:     3D FIX (1 secs)            ││  43    00    000    00      N   │

│    Longitude Err:   +/- 173 m             ││                                 │

│    Latitude Err:    +/- 20 m              ││                                 │

│    Altitude Err:    +/- 478 m             ││                                 │

│    Course Err:      n/a                   ││                                 │

│    Speed Err:       +/- 1251 kph          ││                                 │

│    Time offset:     -0.511                ││                                 │

│    Grid Square:     FM08pp                ││                                 │

└───────────────────────────────────────────┘└─────────────────────────────────┘


Now, I just need to troubleshoot the shim…

Even though I soldered the connector on backwards shouldn’t the one for one pinout be the same? Or, maybe the serial port connections are not making contact?

Time to ohm it out and check!

20150805_232650.jpg


Nope, pinout is fine - but the gap around the solder pads on the shim and the pins themselves seems to be too big and is not making a connection with the board.

20150805_233338.jpg

This is probably a symptom of me soldering the right angle pins on the wrong side of the shim. Perhaps the holes drilled and plated on the other side of the shim (where the right angle pins are now) are smaller? Rather than desolder the shim/header pins and do it all over again (never have had much luck desoldering right angle pins without destroying the board and the pins) I just soldered the shim VERY carefully to the Pi’s headers with a tiny amount of solder so as to not interfere with the rest of the GPIO pin on the board itself. I want it to be reliable and at least somewhat durable anyways! A quick run through with the continuity tester verified this fixed the problem.

20150805_235154.jpg20150805_235034.jpg

Reassemble and power back up the system and continue with the testing!


The cgps command checks out - I get a fix!  image

Running the weather python script displays the data to the screen but it isn’t acting the same. The buttons/city toggle aren’t working now!  image

Unplugging the microstack/GPS module doesn’t seem to help matters any.

Looks like more troubleshooting is needed. Perhaps the shim/my soldering is preventing the CAD from seating all the way? It looks fully seated.


Running through the print(cad.switches[x].value) in Python while toggling the switches seems to be working fine. I’m not sure what has changed at this point as all of the buttons seem to be working but the weather.py demo program is not.  Moving on!



August 6th 2015: GPS output to LCD screen

Referencing:

Microstack GPS and Piface Control and Display Geocaching by callum smith

This code will simply get the coordinates and time from the GPS and display them on the LCD:

#!/usr/bin/env python3
"""
Grab data from GPS and spit it out to LCD
"""


import sys
PY3 = sys.version_info[0] >= 3
if not PY3:
    print("Please use `python3`.")
    sys.exit(1)


###import libraries and set up gps
from time import sleep
import pifacecommon
import pifacecad
import sys,math,time,microstacknode.gps.l80gps
gps=microstacknode.gps.l80gps.L80GPS()
cad=pifacecad.PiFaceCAD()
cad.lcd.backlight_on()
cad.lcd.cursor_off()
cad.lcd.blink_off()
cad.lcd
cad.lcd.home()
cad.lcd.write("Obtaining pos...")


while True:
    cad.lcd.home()
    current_pos=False
    while current_pos==False:
      try:          # try command used to prevent crash when no response from GPS
          current_pos=gps.gpgll          # gets current GPS position
      except (microstacknode.gps.l80gps.DataInvalidError, microstacknode.gps.l80gps.NMEAPacketNotFoundError):          # if no GPS response or if response is invalid
          time.sleep(1)                    #pauses before retry to connect to GPS
          cad.lcd.write("No GPS Lock\nTry moving or check ant")
    cad.lcd.write(str(current_pos["latitude"])[:7]+","+str(current_pos["longitude"])[:8]+"\n"+str(current_pos["utc"]))
    time.sleep(1)                    #pauses before looping to allow user to read output
    #cad.lcd.clear()  #will cause flickering but will ensure no mess is left on screen





August 12th 2015:

This code will grab the coordinates from the GPS and stick them into an array. Once 10 values have been accumulated it will spit out the average and standard deviation.

This is a VERY basic averaging and not the permanent or intended method of obtaining a 'high accuracy' reading. In this mode it takes 10 seconds for the averaging, I intend to speed up the GPS output to 10Hz which will give a simple average once per second.

The goal of this method is to provide a baseline (which will be logged to a CSV file by the Pi) to compare methods of obtaining a highly accurate location.

This method will be called 'Simple Averaging' and will be compared with 'Recursive Averaging', the Kalman filter, the Wiener filter, autoregressive-moving average (ARMA), and the method outlined in the paper referenced above which improves position while moving. Once the data from these methods is graphed I will decide which method to implement for the geocaching tool.

#!/usr/bin/env python3
"""
Grab data from GPS and average it
ToDo: Log to csv for processing
"""


import sys
PY3 = sys.version_info[0] >= 3
if not PY3:
    print("Please use `python3`.")
    sys.exit(1)


###import libraries and set up gps
from time import sleep
#from threading import Barrier
import numpy
import sys,math,time,microstacknode.gps.l80gps
gps=microstacknode.gps.l80gps.L80GPS()
lat_pos = numpy.zeros(10)
lon_pos = numpy.zeros(10)


current_pos=False
while current_pos==False:
    try:          # try command used to prevent crash when no response from GPS
        current_pos=gps.gpgll          # gets current GPS position
    except (microstacknode.gps.l80gps.DataInvalidError, microstacknode.gps.l80gps.NMEAPacketNotFoundError):          # if no GPS response or if response is invalid
            time.sleep(1)                    #pauses before retry to connect to GPS
#print(current_pos)                                # for debugging
count=0
lat_pos.itemset((count),current_pos["latitude"])
lon_pos.itemset((count),current_pos["longitude"])
while True:
    if count == 9:
        print(lat_pos)#+" STD: "+numpy.std(lat_pos)                                # for debugging
        print(lon_pos)#+" STD: "+numpy.std(lon_pos)                                # for debugging
        print(numpy.mean(lat_pos, dtype=numpy.float64),numpy.std(lat_pos))                                # for debugging
        print(numpy.mean(lon_pos, dtype=numpy.float64),numpy.std(lon_pos))                                # for debugging
        count=0
    else:
         count += 1
    try:          # try command used to prevent crash when no response from GPS
        current_pos=gps.gpgll          # gets current GPS position
    except (microstacknode.gps.l80gps.DataInvalidError, microstacknode.gps.l80gps.NMEAPacketNotFoundError):          # if no GPS response or if response is invalid
            time.sleep(1)                    #pauses before retry to connect to GPS
#    print(count)
    lat_pos[count]=current_pos["latitude"]
    lon_pos[count]=current_pos["longitude"]

 

 

Next step is to implement data logging and then the other methods of improving position.