Raspberry Pi Projects
  • Products
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog Raspberry Pi temperature and cooling testing Part 1 initial tests.
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: bwelsby
  • Date Created: 9 Mar 2016 1:29 PM Date Created
  • Views 5242 views
  • Likes 6 likes
  • Comments 24 comments
  • rpi cooling
  • heatsink
  • pi hat
  • heat_sink
  • rpi3
  • rpi
  • raspberry_pi_projects
Related
Recommended

Raspberry Pi temperature and cooling testing Part 1 initial tests.

bwelsby
bwelsby
9 Mar 2016

Raspberry Pi 3 temperature and cooling testing :

 

Part 1 Inital tests

Part 2 with a HAT tests.

Part 3 with Fan Speed Control. (Still to come)

 

 

 

This experiment started out after discussions following a post by shabaz   here Raspberry Pi 3 Cooling / Heat Sink Ideas

The tests were carried out with the new RPi 3 as it was found to get hot under heavy load, I may repeat the tests at a later date with the RPi 2 for comparisons.

For the tests I created a simple 3D printed enclosure and also 3D printed dummy HATs the OpenScad files are attached, feel free do do with these as you wish.

 

imageimage

The OpenScad image of the test enclosure and the final printed case with RPi 3 installed

image

 

 

 

A total of eight tests were carried out to the following plan where 0 = option not installed,  x = option installed

The test plan:-

 

Test#  Fan   Cover    Heatsink   Graph Colour

1         0        0           0               Brown

2         x        0           0               Red

3         0        x           0               Orange

4         x        x           0               Yellow

5         0        0           x               Green

6         x        0           x               Blue

7         0        x           x               Violet

8         x        x           x               Grey

 

The heatsink used is a ceramic part  MPC222225T - AMEC THERMASOL - Heat Sink, Square, Micro Porous, 10.21 °C/W, 2.5 mm, 22 mm, 22 mm | Farnell element14

chosen because it is only 2.5mm thick and would fit easily between RPi and an installed HAT. If no HATs are being used and height above the RPi is not an issue then there may be larger more efficient heatsinks available that would provide better cooling but these tests were specifically an experiment to see if there was a solution for HAT use.

The fan used was MC25100V2-0000-A99 - SUNON - Axial Fan, MAGLevimage Motor, Medium Speed, Vapo, MC Series, 5 VDC, 25 mm, 10 mm, 3.002 cu.ft/m…

 

To run the tests I first installed the latest NOOBS and configured Raspbian as the operating system, and to make sure everything was up to date this was then followed by

 

sudo apt-get update
sudo apt-get upgrade
sudo rpi-update

 

The Test Script

I used the following shell script I called temptest for the tests which outputs the data in a csv format it includes both temperature and also CPU frequency which showed that the CPU was being throttled when the temperature reached 80'C

 

#!/bin/bash

I=0;
stress --cpu 4 --timeout 600 &
while [ $I -lt 600 ]; do
    echo -n "$I,"
    vcgencmd measure_temp | sed -e 's/temp=//g' | tr -d "'C\n"
    echo -n ","
    vcgencmd measure_clock arm | sed -e "s/frequency(45)=//g"
    let I=I+1
    sleep 1
done

 

I ran the RPi without monitor, keyboard or mouse just an ethernet connection to my local network then I SSH'd from my linux desktop computer for windows you could use PuTTY: a free SSH and Telnet client  or something similar the IP address on my system was 192.168.0.26

 

ssh pi@192.168.0.26

 

Then I ran the tests as root privilage

 

sudo -s

 

Each test was run piping the output to a testx.csv where x is the test number. time between tests allowed the RPi co cool back to idle operating temperature and the ambient temperature in the room was 22'C

 

./temptest > test1.csv

 

On completion I had eight csv files, I then used Gnumeric  (a spreadsheet program) on my linux desktop to import just the temperature data and produce the following graph. The numbers along the bottom are approximate seconds and the numbers on the left are CPU temperature. The colours are as listed above for each test. If you click on the image you should get a larger view.

image

As I said in the other blog I will leave it for you to draw your own conclusions and I will give mine when I have done further tests image

 

One thing observed was that the fan on full speed is quite powerful and a little noisy so reducing it's speed with a suitable PWM control would reduce the noise and could still provide sufficient airflow. This is for further testing.

 

Edit: 10-March-2016

A word of caution for the inexperienced

The heatsinks we have been discussing are held in place by a thermally conductive adhesive pad. In essence they are glued to the processor chip.

I would recommend that you DO NOT attempt to remove them as any twisting,pulling or prising is likely to damage the chip or its many extremely tiny soldered connection to the PCB

 

The Raspberry Pi may be an inexpensive single board computer but it could easily become a very expensive piece of scrap.

Attachments:
openscad_files.zip
  • Sign in to reply

Top Comments

  • cstanton
    cstanton over 10 years ago in reply to shabaz +4
    Well, the diamond heatsink and diamond thermal compound arrived, now I just need a way to 3D print the case (I already had the fan).
  • cstanton
    cstanton over 10 years ago +3
    I've picked up some diamond heatsinks and thermal compound, as soon as I find a 3D Printer I want to try it out in this setup with the fan
  • cstanton
    cstanton over 10 years ago +3
    Finally got the 3D printer working at the hackspace, however it had some build quality issues, gaps are temporarily plugged with blu-tac
  • cstanton
    cstanton over 10 years ago in reply to bwelsby

    Regarding fan speed control, I was talking to a few people at the hackspace and discovered that it should be possible to do PWM to control the fan from the Raspberry Pi ( https://pythonhosted.org/RPIO/pwm_py.html  ), I guess the only problem then is that it's 3v rather than 5v and that would require some interim kit.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bwelsby
    bwelsby over 10 years ago in reply to cstanton

    Christopher Stanton wrote:

     

    Finally got the 3D printer working at the hackspace, however it had some build quality issues, gaps are temporarily plugged with blu-tac

    Great stuff, doesn't look so bad image  Interested to see what results you get.   I am recently back from a nice long holiday and still catching up with things ( like over 2000 emails!).  When I get to it I will update with an improved enclosure and fan speed control.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cstanton
    cstanton over 10 years ago

    image

     

    Finally got the 3D printer working at the hackspace, however it had some build quality issues, gaps are temporarily plugged with blu-tac image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bwelsby
    bwelsby over 10 years ago in reply to clem57

    Clem Martins wrote:

     

    Or quote the difference between the ambient temp and the core temp in the graph/figures.

    Clem

    Yes I can add that too, also when I have all the data I will upload the files so anyone who wants can analyze however they like.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bwelsby
    bwelsby over 10 years ago in reply to cstanton

    Christopher Stanton wrote:

     

    I think it would also be important to measure the ambient temperature and humidity when doing these tests as that could affect results. Perhaps inside and outside of the case?

    I agree, I did measure the ambient in the room here at home where I carried out the tests with a digital thermometer near the enclosure but I don't have anything to measure humidity image.  My tests with fan speed control will measure the heatsink temperature as I have drilled a tiny hole in it now to take a 104GT-2 thermistor and I am using that to automatically control fan speed as well as logging the temp.   More on that to come image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>