Raspberry Pi Projects
  • Products
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog Raspberry Pi temperature and cooling testing Part 1 initial tests.
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: bwelsby
  • Date Created: 9 Mar 2016 1:29 PM Date Created
  • Views 5243 views
  • Likes 6 likes
  • Comments 24 comments
  • rpi cooling
  • heatsink
  • pi hat
  • heat_sink
  • rpi3
  • rpi
  • raspberry_pi_projects
Related
Recommended

Raspberry Pi temperature and cooling testing Part 1 initial tests.

bwelsby
bwelsby
9 Mar 2016

Raspberry Pi 3 temperature and cooling testing :

 

Part 1 Inital tests

Part 2 with a HAT tests.

Part 3 with Fan Speed Control. (Still to come)

 

 

 

This experiment started out after discussions following a post by shabaz   here Raspberry Pi 3 Cooling / Heat Sink Ideas

The tests were carried out with the new RPi 3 as it was found to get hot under heavy load, I may repeat the tests at a later date with the RPi 2 for comparisons.

For the tests I created a simple 3D printed enclosure and also 3D printed dummy HATs the OpenScad files are attached, feel free do do with these as you wish.

 

imageimage

The OpenScad image of the test enclosure and the final printed case with RPi 3 installed

image

 

 

 

A total of eight tests were carried out to the following plan where 0 = option not installed,  x = option installed

The test plan:-

 

Test#  Fan   Cover    Heatsink   Graph Colour

1         0        0           0               Brown

2         x        0           0               Red

3         0        x           0               Orange

4         x        x           0               Yellow

5         0        0           x               Green

6         x        0           x               Blue

7         0        x           x               Violet

8         x        x           x               Grey

 

The heatsink used is a ceramic part  MPC222225T - AMEC THERMASOL - Heat Sink, Square, Micro Porous, 10.21 °C/W, 2.5 mm, 22 mm, 22 mm | Farnell element14

chosen because it is only 2.5mm thick and would fit easily between RPi and an installed HAT. If no HATs are being used and height above the RPi is not an issue then there may be larger more efficient heatsinks available that would provide better cooling but these tests were specifically an experiment to see if there was a solution for HAT use.

The fan used was MC25100V2-0000-A99 - SUNON - Axial Fan, MAGLevimage Motor, Medium Speed, Vapo, MC Series, 5 VDC, 25 mm, 10 mm, 3.002 cu.ft/m…

 

To run the tests I first installed the latest NOOBS and configured Raspbian as the operating system, and to make sure everything was up to date this was then followed by

 

sudo apt-get update
sudo apt-get upgrade
sudo rpi-update

 

The Test Script

I used the following shell script I called temptest for the tests which outputs the data in a csv format it includes both temperature and also CPU frequency which showed that the CPU was being throttled when the temperature reached 80'C

 

#!/bin/bash

I=0;
stress --cpu 4 --timeout 600 &
while [ $I -lt 600 ]; do
    echo -n "$I,"
    vcgencmd measure_temp | sed -e 's/temp=//g' | tr -d "'C\n"
    echo -n ","
    vcgencmd measure_clock arm | sed -e "s/frequency(45)=//g"
    let I=I+1
    sleep 1
done

 

I ran the RPi without monitor, keyboard or mouse just an ethernet connection to my local network then I SSH'd from my linux desktop computer for windows you could use PuTTY: a free SSH and Telnet client  or something similar the IP address on my system was 192.168.0.26

 

ssh pi@192.168.0.26

 

Then I ran the tests as root privilage

 

sudo -s

 

Each test was run piping the output to a testx.csv where x is the test number. time between tests allowed the RPi co cool back to idle operating temperature and the ambient temperature in the room was 22'C

 

./temptest > test1.csv

 

On completion I had eight csv files, I then used Gnumeric  (a spreadsheet program) on my linux desktop to import just the temperature data and produce the following graph. The numbers along the bottom are approximate seconds and the numbers on the left are CPU temperature. The colours are as listed above for each test. If you click on the image you should get a larger view.

image

As I said in the other blog I will leave it for you to draw your own conclusions and I will give mine when I have done further tests image

 

One thing observed was that the fan on full speed is quite powerful and a little noisy so reducing it's speed with a suitable PWM control would reduce the noise and could still provide sufficient airflow. This is for further testing.

 

Edit: 10-March-2016

A word of caution for the inexperienced

The heatsinks we have been discussing are held in place by a thermally conductive adhesive pad. In essence they are glued to the processor chip.

I would recommend that you DO NOT attempt to remove them as any twisting,pulling or prising is likely to damage the chip or its many extremely tiny soldered connection to the PCB

 

The Raspberry Pi may be an inexpensive single board computer but it could easily become a very expensive piece of scrap.

Attachments:
openscad_files.zip
  • Sign in to reply

Top Comments

  • cstanton
    cstanton over 10 years ago in reply to shabaz +4
    Well, the diamond heatsink and diamond thermal compound arrived, now I just need a way to 3D print the case (I already had the fan).
  • cstanton
    cstanton over 10 years ago +3
    I've picked up some diamond heatsinks and thermal compound, as soon as I find a 3D Printer I want to try it out in this setup with the fan
  • cstanton
    cstanton over 10 years ago +3
    Finally got the 3D printer working at the hackspace, however it had some build quality issues, gaps are temporarily plugged with blu-tac
  • clem57
    clem57 over 10 years ago in reply to cstanton

    Or quote the difference between the ambient temp and the core temp in the graph/figures.

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cstanton
    cstanton over 10 years ago in reply to bwelsby

    I think it would also be important to measure the ambient temperature and humidity when doing these tests as that could affect results. Perhaps inside and outside of the case?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bwelsby
    bwelsby over 10 years ago in reply to cstanton

    Great, I would be interested to see what performance is like in the open too and also in the official RPi enclosure Official Raspberry Pi Case (for use with Raspberry Pi 3 Model B only)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cstanton
    cstanton over 10 years ago in reply to shabaz

    Well, the diamond heatsink and diamond thermal compound arrived, now I just need a way to 3D print the case (I already had the fan).

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bwelsby
    bwelsby over 10 years ago in reply to shabaz

    AMEC produce the flat heatpipes and I have just seen Farnell have then in stock MHP-1220A-100A - AMEC THERMASOL - Heat Sink, Heat Pipe, Ultra Flat, LED, 0.4 °C/W, 1.2 mm, 20 mm, 100 mm    I would like to see if I can fit that in somewhere using the tape you mention and maybe a 3D printed support bracket holding an external heatsink.

     

    What started out as a quick experiment is turning into a full time project image  no complaints I just wish I had more time to do more image

     

    Brian

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>