Raspberry Pi Projects
  • Products & Partners
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog Using the IO on a Raspberry Pi 3 B+
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jc2048
  • Date Created: 16 Mar 2019 11:43 PM Date Created
  • Views 5487 views
  • Likes 7 likes
  • Comments 8 comments
  • raspberry pi 3 b+
  • raspberry_pi_projects
Related
Recommended

Using the IO on a Raspberry Pi 3 B+

jc2048
jc2048
16 Mar 2019

In my quest to use a Raspberry Pi 3B+ for creating art, I need to be able to control the GPIO pins. So next step

was to look for some information on doing just that.

 

A quick search of element14 uncovered this blog by shabaz where he illustrates controlling the GPIO lines with

Python. That should get me off to a quick start and Python should be ok to work with, at least for the simpler

art pieces [I haven't done very much with Python and, to be honest, I didn't entirely like it when I did, but it

will do for the moment].

 

Raspberry Pi GPIO Explained

 

To enter the script I'm going to need a text editor that I can run without the desktop. It seems that GNU Nano

is part of the distribution, so I'll start with that. For it to work with PuTTY, I found that local editing

needed to be turned off.

 

Here's the Python code I'm using, as seen in the Nano editor's text-terminal-style 'window', framed in PuTTY's

Windows GUI-style window. The code is one of Shabaz's examples.

 

image

 

If I give it to the Python interpreter to run and look at the IO pin, it does this on the 'scope

 

image

 

Success!

 

So, I now have the means to control I/O lines under the control of a Python script and that probably gives me

enough to get me going and produce the first simple piece of art (which I've got to come up with by the end of next

week to stay on schedule). Next blog will be the first proper challenge one and will be in the Picasso Challenge

area.

  • Sign in to reply

Top Comments

  • fmilburn
    fmilburn over 7 years ago +4
    Hi Jon, I have been using Geany as the IDE for Python on the Raspberry Pi. It has the advantage of highlighting key words, start the code running with a button click, etc. I have been using it long enough…
  • shabaz
    shabaz over 7 years ago +4
    Hi Jon, That's awesome, glad the blog was helpful! In recent times, another Python API has become available, called "gpiozero". The one in that blog still works, but just in case you want to examine that…
  • beacon_dave
    beacon_dave over 7 years ago in reply to jc2048 +4
    "GPIO Zero is installed by default in the Raspbian image, and the Raspberry Pi Desktop image for PC/Mac, both available from raspberrypi.org . Follow these guides to installing on Raspbian Lite and other…
  • jc2048
    jc2048 over 7 years ago in reply to fmilburn

    That's a useful recommendation for anyone wanting to use Python, but it's a graphical IDE that runs on a desktop.

     

    I'm running the Pi headless where everything is going through an ethernet cable (I don't have a keyboard or display connected to the Pi) and I'm logging-in to a SSH (secure shell) text terminal. So it's like being back in the days of DOS and a command line, except remotely at a distance. The Nano editor (running on the Pi) uses some kind of terminal emulation to construct a kind of pseudo window to do the editing in, but it's still all text based. The GUI window you can see in the picture around that is the PuTTY window that's running on the laptop and communicating via the ethernet with the Pi and does no more than presenting what was on the Pi's terminal screen on the laptop's screen. [Perhaps I should have drawn a picture rather than try and explain in words.]

     

    I could have set up things to use a remote desktop over the ethernet (via a VPN), but that would have been a lot more complicated to get going.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago

    Hi Jon,

     

    That's awesome, glad the blog was helpful!

    In recent times, another Python API has become available, called "gpiozero".

    The one in that blog still works, but just in case you want to examine that other API too, there is some info here:

    https://gpiozero.readthedocs.io/en/stable/migrating_from_rpigpio.html

    The original RPi.GPIO API is similar to how it would be done with any generic microcontroller, i.e. set a port pin to input or output mode, and then read or write it, and let the user code directly call this API and leave the user to optionally write any class to control a pin if desired, whereas gpiozero has ready-made classes for input/output devices, and creating an instance will set the port pin to input or output as part of that ready-made class code, without the user code needing to do that.

    The gpiozero API was not available when that blog was written. I reckon some may still find the original API easier to understand but for others more familiar with classes and objects the gpiozero is probably cleaner. I've been in two minds to update that blog post, since it currently works and isn't broken.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 7 years ago

    Hi Jon,

     

    I have been using Geany as the IDE for Python on the Raspberry Pi.  It has the advantage of highlighting key words, start the code running with a button click, etc.  I have been using it long enough now that I have forgotten what getting started tutorial I used but I don’t remember it being difficult.  It is lightweight and quick.

     

    Frank

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
<