Raspberry Pi Projects
  • Products & Partners
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Documents Building a Low Power Compact LCD Display
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 22 Apr 2016 4:41 PM Date Created
  • Last Updated Last Updated: 10 May 2021 6:52 PM
  • Views 15232 views
  • Likes 20 likes
  • Comments 55 comments
Related
Recommended

Building a Low Power Compact LCD Display

(Note: For a follow-up project which uses a larger screen, click here:Building a 3.5 Digit Low Power LCD Module  )

image

Introduction

Sometimes a really simple, low power display is needed. A lot of information can be shown on even a 7-segment display!

 

This LCD board project could be useful for such purposes. The three 7-segment digits (and two decimal places total, between the digits) can show percentages, hexadecimal values, voltages and current readings. Plenty of characters can be represented too.

 

Up to four of these displays can be connected to a single I2C bus so (for example) a power supply project could use one display for voltage and another for current, for two channels. To save costs for smaller projects a single display could be used to show more than one item of information using  a button press or periodic cycling of data on the display.

image

 

The reflective LCD that is used has no backlight but has very good contrast and in tests had excellent visibility even in dim light. The power consumption is extremely low and this makes it ideal for portable projects which might need to run for years on batteries without charging. The entire bill-of-materials is less than £5GBP (or lower if multiple displays are purchased).

The schematic and plot (gerber) files and source code is attached to this post. I had 20 PCBs made for less than the cost of a pizza.

image

As a quick test I tried it using a Raspberry Pi just counting up from 0.0 to 99.9. With very little effort it would be possible to use it to display Pi stats – for example temperature, or the IP address (one byte at a time) upon start-up. It is easy to get any script to write to the display from the command line.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Features Summary

  • 3.3V or 5V capable
  • Ultra-low current consumption (24uA at 3.3V)
  • Extremely compact; 32x21mm
  • Just a 4 wire connection; I2C Interface, 0V and VDD (3.3V or 5V)
  • Individually addressable segments for alphanumeric and other symbol use
  • Quick to assemble; less than a dozen parts
  • Low cost; about £5GBP in quantities of 1

 

Parts List

RefCodeMnfr Part #DescriptionQtyGBP Each
LCD118389301838930LCD-S301C31TRLCD-S301C31TRLCD 3-digit11.85
U124004602400460PCF85176TLCD Driver11.18
C317591221759122MC0603B104K500CT100N 0603 x7r10.01
R1, R320733492073349MCMR06X1002FTLMCMR06X1002FTL10K Res 060320.01
R2, R4, R5D.N.F.00.00
R6, R793319729331972MC0063W060352K7MC0063W060352K72.7k Res 060320.01
J1159341515934152211S-06G2211S-06GSIL header 6-way10.26
Optional177848177848D01-99012 01PCB pin sockets 12-way21.18
Optional229985622998560552-2-15-01-21-27-10-00552-2-15-01-21-27-10-0PCB pin sockets (alternative)240.07

 

Additional components for 5V operation

RefCodeMnfr Part #DescriptionQtyGBP Each
U223143722314372TPS70925DBVTTPS70925DBVTLDO 2.5V Voltage Regulator10.82
C119073431907343C1608X7R1C105K080AC1u 0603 X7R10.04
C217355421735542GRM21BR71E225KA73LGRM21BR71E225KA73L2.2u 0805 X7R10.24

 

How it Works

There are different types of LCDs, but in general they require an alternating current (AC) signal to turn on segments. Some use a square wave, others require multiple voltage levels in order to achieve high segment density with low pin count through multiplexing.

The particular LCD chosen requires a square wave, and has the benefit of providing high contrast digits. Reflective displays offer high contrast but have the disadvantage that they are opaque from the underside and cannot be lit from behind so require either ambient light to be visible or a side light.

 

Some microcontrollers feature LCD driving capability but there is a classic integrated circuit from NXP that is useful to offload the task from microcontrollers and allow the use of an I2C bus for interfacing. That IC is the PCF8576 which has been around for more than two decades. NXP have a more recent IC called PCF85176 (it appears to be backwards-compatible) and that is the one used for this project because it has very low power consumption requirements and a higher speed I2C bus capability than its predecessor.

Nothing else is needed apart from a few resistors and capacitors.

 

The LCD needs a few volts peak voltage in order to function. For 5V operation a linear regulator provides the lower voltage to run the LCD.

 

Building It

image

Order the boards from a PCB firm (the files are attached to this post). Once the PCBs arrive, the first step is to solder the PCF85176 chip. It is quite small (0.5mm spaced pins) but hand-soldering is still possible. A hot plate and solder paste would be another option. I just used a normal soldering iron (2mm tip) and no-clean flux (cleaned up afterwards) and thin solder.

 

The hardest part is perfect alignment. The way I do it is to tape the IC onto the PCB first. Then, inspect the pins using a magnifying lens. If it looks incorrect, peel the tape from one end but keep the IC attached to the tape. Move the tape and re-stick it onto the PCB. It becomes quite easy to align the IC and secure it in this manner, just moving the tape from one side at a time.

 

Next, apply a small amount of no-clean flux and start soldering. Any bridges will fall away if you re-heat with the iron, but if the bridge is persistent then use de-soldering braid. The soldering iron needs a bit of solder applied to the tip in order to get the solder-wicking effect when using the braid.

 

Optionally use pin sockets (or SIL sockets) so that the LCD does not need to be soldered. It is highly recommended that sockets are used to protect the LCD and also because it would be difficult to unsolder the LCD if there was a problem with the PCF85176 that needed examining.

After all the parts have been soldered clean the board using an IPA solution and then examine each pin on the PCF85176 under a lens (push each pin gently with the side of a scalpel blade) to verify all is well.

image

 

If the display only needs to operate from 3.3V then you don’t need to solder the linear regulator IC and its associated capacitors. If multiple displays on the same I2C bus are needed then the addresses are programmed using two 10k resistors that can be soldered in different positions (see the source code for a table which indicates this).

image

 

The attached files are slightly improved to the boards that I used, in that there is a white space for labelling them if multiple displays are needed for a single project.

 

After checks for any short circuits, the LCD can now be connected up to the Pi.

image

 

Software

As a quick test some C code was written for the ‘Pi. It was tested using a Pi 2 but should work on others, there is nothing special to the code.

To enable I2C on the ‘Pi, add the following line to /boot/config.txt (you need to be root user to do this):

dtparam i2c_arm=on

 

Reboot the Pi and then type (as root user):

modprobe i2c_dev

 

To make it persistent across reboots you can add the following (as root user) to the /etc/modules file:

i2c-dev

 

Grab the code from github. To compile the code type the following:

gcc -c i2cfunc.c -o i2cfunc.o
ar rcs libi2cfunc.a i2cfunc.o
gcc lcd3-test.c -L. -li2cfunc -o lcd3-test

 

To run it, type:

./lcd-test

 

Currently the code can display decimal points, digits 0-9 and space.

To use it, call the print_line() function. Here are some examples:

print_line(" 0.0");
print_line("1.23");
print_line("   "); // clear the screen

 

image

 

The I2C interface is a standard, and it would be very easy to port the code across to any microcontroller/Arduino/etc.

 

Summary

NXP’s I2C LCD chip continues to be useful after two decades. The cost, size and low power consumption are attractive for some use-cases. Although this project uses surface mount components they are cheap enough that it could be a useful board to practice with. The very low power consumption means that a couple of AA batteries should last for five years or more with the display always on.

 

image

 

Advanced Use: Extending the Character Set

Many characters are possible with 7-segment displays.

image

Three bytes represent which segments are to be activated. Refer to the diagram to see the bit mappings.

image

 

To extend the character set to display hyphens or alphabet characters, the following array needs to be extended:

 

const char bit_table[]=
{
  0x38, 0x00, 0x86,    0x00, 0xbe, 0x00,    0x86, 0x00, 0x38,    /* 0 */
  0x08, 0x00, 0x02,    0x00, 0x0a, 0x00,    0x02, 0x00, 0x08,    /* 1 */
  0x30, 0x00, 0x46,    0x00, 0x76, 0x00,    0x46, 0x00, 0x30,    /* 2 */
  0x18, 0x00, 0x46,    0x00, 0x5e, 0x00,    0x46, 0x00, 0x18,    /* 3 */
  0x08, 0x00, 0xc2,    0x00, 0xca, 0x00,    0xc2, 0x00, 0x08,    /* 4 */
  0x18, 0x00, 0xc4,    0x00, 0xdc, 0x00,    0xc4, 0x00, 0x18,    /* 5 */
  0x38, 0x00, 0xc4,    0x00, 0xfc, 0x00,    0xc4, 0x00, 0x38,    /* 6 */
  0x08, 0x00, 0x06,    0x00, 0x0e, 0x00,    0x06, 0x00, 0x08,    /* 7 */
  0x38, 0x00, 0xc6,    0x00, 0xfe, 0x00,    0xc6, 0x00, 0x38,    /* 8 */
  0x18, 0x00, 0xc6,    0x00, 0xde, 0x00,    0xc6, 0x00, 0x18     /* 9 */
};

 

The first group of three bytes indicates the segments that need to be turned on for the digit in the leftmost position, the second group of three refer to the center digit and the last three refer to the rightmost digit. If ASCII sequence is not followed then modify the char_prog function accordingly.

 

To enable the extra characters, the print_line function case statement checks can be extended.

Attachments:
export-lcd3.zip
export-lcd3-rev2.zip
export-lcd3-rev2-with-board-outline.zip
  • low_power
  • eagle
  • eagle-cad
  • lcd
  • rpiintermediate
  • lcd display
  • eagle_cad
  • raspberry_pi
  • display
  • nxp
  • raspberry_pi_projects
  • feature_tutorial
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 9 years ago in reply to shabaz +5
    Works fully now I'll create a follow up blog with the ported code.... edit: done - Building a Low Power Compact LCD Display - Port to Hercules Safety Microcontroller
  • DAB
    DAB over 10 years ago +4
    Great post Shabaz. You provide good information on how to use different LCD screens and interface them to a MCU. DAB
  • Jan Cumps
    Jan Cumps over 9 years ago +4
    I'm going to play along. I'll first try to talk to it with a Bus Pirate v4. Then as a low power reception indicator for a Sub-1GHz range test...
  • clem57
    clem57 over 10 years ago in reply to shabaz

    After I saw this, it hit me that you can choose the I2C address using current/no current.R5 I would not have guessed. Thanks

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to clem57

    Hi Clem!

    R2 and R4 become relevant if more than one display is connected to an I2C bus.

    To send information to the display, the I2C address of the PCF85176 is 0x38, but within the data portion of the I2C stream of data is a separate module address beginning 0x60.

    R2 and R4 (together with R1 and R3) are used to select that address, so that it is possible to fit up to four of these modules onto a single I2C bus, and have different content sent to each.

    By default only R1 and R3 need to be fitted to select the first address (0x60).

    There is a table in the source code that indicates which resistors to fit, depending on the desired address.

    R1    R2    R3    R4    DEVICE_ADDRESS
    Fit         Fit         0x60
          Fit   Fit         0x61
    Fit               Fit   0x62
          Fit         Fit   0x63

     

    As for R5, that can be fitted with a zero-ohm link to enable higher current drive to the LCD, but it turns out that the display has very high contrast even without it, so it is not needed. LCD datasheets are often very sparsely written with much information lacking, so I had to wait to test before I could determine if high current drive would be needed or not. Since I was rapid prototyping (the schematic and board layout were complete within hours, in one evening) I decided to leave space for R5 and then not populate it if it was not needed.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to DAB

    Hi DAB,

     

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 10 years ago

    shabaz

         Curious about the part list:

     

    R2, R4, R5D.N.F.0

    0.00

       

          I get it is not used, but when and why are they here in the first place/

    Clem

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 10 years ago

    Great post Shabaz.

     

    You provide good information on how to use different LCD screens and interface them to a MCU.

     

    DAB

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
<