Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Documents Raspberry Pi 8GB SD card pre-installed with NOOBS
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: joeman
  • Date Created: 5 Aug 2013 6:59 PM Date Created
  • Last Updated Last Updated: 17 Apr 2014 12:41 AM
  • Views 8565 views
  • Likes 3 likes
  • Comments 25 comments
Related
Recommended

Raspberry Pi 8GB SD card pre-installed with NOOBS

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The Raspberry Pi Model B is now available with an 8GB SD card pre-installed with NOOBS offering a choice of over 6 operating systems ready to use with your Pi.

 

Features & Benefits:

·     Get’s you up and running quicker. No need to download operating software, the 6 most popular operating systems are pre-loaded on the card for you and ready to install at the click of a button.

·      Change or re-install operating systems at a click of a button with NOOBS.

·     If the worst should happen and you were to corrupt your files they can be safely and easily restored with NOOBS

·      All the space you will need to create and store your Raspberry Pi projects on the officially recommended SD Card by the Raspberry Pi Foundation


Contents:

A Raspberry Pi Model B 512MB board and an 8GB SD card incorporating the NOOBS (New Out Of Box Software) released from the Raspberry Pi Foundation

 

What is NOOBS?:

NOOBS contains a Recovery System that loads every time you boot up your Raspberry Pi. This recovery system contains pre-loaded images for 6 operating systems that you can install on your device. These include:

Arch Linux

OpenELEC (Xbox Media Centre)

Pidora

RISC OS

RaspBMC (Xbox Media Centre)

Raspbian (Raspberry Pi Foundation’s preferred operating system)

If you want to change operating systems, you can simply choose one from the list above and click ‘Install OS’ and your chosen software will be installed. Please be warned that this will erase all existing software that was previously installed on the card.

 

Why use NOOBS?

It is very easy to use. You do not have to seek out and find an operating system for the Raspberry Pi and then re-flash your card using 3rd party software each time you want to change operating systems. The 6 most popular operating systems are pre-loaded on the card for you and ready to install and use at the click of a button.

Should the worst happen and you manage to corrupt your operating system you do not have to go through the process of downloading the operating system again and re-flashing your SD card, you can simply load up the recovery system and install a fresh operating system directly from the Raspberry Pi. To load the recovery system simply hold the SHIFT key down while you boot your Raspberry Pi.

 

Why use an 8GB card?

With the New Out Of Box Software (NOOBS) all of the operating system images are preloaded on the SD card and held within the recovery partition. These system images use just over 1GB of space on the SD card. Therefore to ensure that you can get the maximum benefit from your Raspberry Pi we recommend using an 8GB card so you have plenty of spare space on the card to create your own files.


Product Recommendation:

Raspberry Pi Model BRaspberry Pi Model B

Raspberry Pi Model B with 8GB SD CardRaspberry Pi Model B with 8GB SD Card

Raspberry Starter KitRaspberry Starter Kit

  • raspberry
  • noobs
  • pi
  • pre-installed
  • with
  • 8gb
  • card
  • sd
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • antihiro
    antihiro over 12 years ago in reply to saurocksall +2
    Nice!
  • rew
    rew over 12 years ago +2
    The SD card provided to you is 8Gb. That is not because the NOOBS installation is 8Gb, but because it gives you 7.something GB of storage space FOR YOU. The files that recovery tools normally can find…
  • e14 Contributor
    e14 Contributor over 13 years ago +1
    i bought a 32GB SD card,, is there a problem with doing that ?
  • e14 Contributor
    e14 Contributor over 12 years ago

    admin

    Is it version 2.0 of model B that element14 selling ?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    Is everything you need, to get started, included in this package?
    It might be me not looking well enough but I don't see the power supply.
    Is it included?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    Ordering this little bad boy now, can't wait to do BIG things with it! image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    what class is the provided sd card

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dwinhold
    dwinhold over 12 years ago

    When you formated 30+% of the card it won't run, most likely at 1% it wouldn't have run anymore. Formatting clears sectors of the card, not programs. It would be like starting to format your main drive on the computer and expect the OS to still work. You will need to finish the format and reload, which isn't to hard. Good luck with this, you'll have no problems.

     

    D Winhold

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rew
    rew over 12 years ago

    The SD card provided to you is 8Gb. That is not because the NOOBS installation is 8Gb, but because it gives you 7.something GB of storage space FOR YOU.

     

    The files that recovery tools normally can find (I know a thing or two about data recovery, as I work at a data-recovery company) are the files that are NOT in the root directory. A (quick) format overwrites the root directory, but not subdirectories. Thus the files in the root are lost, but files in subdirectories might be recovered. ALL files required by the raspberry pi to boot are contained in the root directory.

     

    You stopped the format at 32%. Why? Because you realized it was not the best thing to do.

     

    You can complain all you want about nothing having been there, but all we can now say is that it was most probably caused by your action of formatting the card. Finished or not.

     

    You still have two options. Buy a new NOOBS card or install NOOBS (or something else) on the card yourself. How to do this is easily found by using google or following one of the links in this thread.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • saurocksall
    saurocksall over 12 years ago

    you should watch this video  it will explain every thing to you...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • saurocksall
    saurocksall over 12 years ago

    you shouldn't have formatted the card ... it already had noobs on it, now you need tho format the card completely, and re install noobs on it...

    HERE i a link for that... And HERE is The link for Documentation ....

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rew
    rew over 12 years ago

    I agree with you that the card should have shown some file in windows. That would normally be the case.

     

    However, now you've formatted it (or just started to..), you have lost the ability to doublecheck that. your (partial) formatting has already overwritten the "preinstalled noobs". So your options are:

    * Buy a new NOOBS SD card.

    * Install NOOBS yourself on your freshly formatted SD card.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • saurocksall
    saurocksall over 12 years ago

    Which type of card are you having ??

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>