Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Documents Raspberry Pi 8GB SD card pre-installed with NOOBS
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: joeman
  • Date Created: 5 Aug 2013 6:59 PM Date Created
  • Last Updated Last Updated: 17 Apr 2014 12:41 AM
  • Views 8566 views
  • Likes 3 likes
  • Comments 25 comments
Related
Recommended

Raspberry Pi 8GB SD card pre-installed with NOOBS

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The Raspberry Pi Model B is now available with an 8GB SD card pre-installed with NOOBS offering a choice of over 6 operating systems ready to use with your Pi.

 

Features & Benefits:

·     Get’s you up and running quicker. No need to download operating software, the 6 most popular operating systems are pre-loaded on the card for you and ready to install at the click of a button.

·      Change or re-install operating systems at a click of a button with NOOBS.

·     If the worst should happen and you were to corrupt your files they can be safely and easily restored with NOOBS

·      All the space you will need to create and store your Raspberry Pi projects on the officially recommended SD Card by the Raspberry Pi Foundation


Contents:

A Raspberry Pi Model B 512MB board and an 8GB SD card incorporating the NOOBS (New Out Of Box Software) released from the Raspberry Pi Foundation

 

What is NOOBS?:

NOOBS contains a Recovery System that loads every time you boot up your Raspberry Pi. This recovery system contains pre-loaded images for 6 operating systems that you can install on your device. These include:

Arch Linux

OpenELEC (Xbox Media Centre)

Pidora

RISC OS

RaspBMC (Xbox Media Centre)

Raspbian (Raspberry Pi Foundation’s preferred operating system)

If you want to change operating systems, you can simply choose one from the list above and click ‘Install OS’ and your chosen software will be installed. Please be warned that this will erase all existing software that was previously installed on the card.

 

Why use NOOBS?

It is very easy to use. You do not have to seek out and find an operating system for the Raspberry Pi and then re-flash your card using 3rd party software each time you want to change operating systems. The 6 most popular operating systems are pre-loaded on the card for you and ready to install and use at the click of a button.

Should the worst happen and you manage to corrupt your operating system you do not have to go through the process of downloading the operating system again and re-flashing your SD card, you can simply load up the recovery system and install a fresh operating system directly from the Raspberry Pi. To load the recovery system simply hold the SHIFT key down while you boot your Raspberry Pi.

 

Why use an 8GB card?

With the New Out Of Box Software (NOOBS) all of the operating system images are preloaded on the SD card and held within the recovery partition. These system images use just over 1GB of space on the SD card. Therefore to ensure that you can get the maximum benefit from your Raspberry Pi we recommend using an 8GB card so you have plenty of spare space on the card to create your own files.


Product Recommendation:

Raspberry Pi Model BRaspberry Pi Model B

Raspberry Pi Model B with 8GB SD CardRaspberry Pi Model B with 8GB SD Card

Raspberry Starter KitRaspberry Starter Kit

  • raspberry
  • noobs
  • pi
  • pre-installed
  • with
  • 8gb
  • card
  • sd
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • antihiro
    antihiro over 12 years ago in reply to saurocksall +2
    Nice!
  • rew
    rew over 12 years ago +2
    The SD card provided to you is 8Gb. That is not because the NOOBS installation is 8Gb, but because it gives you 7.something GB of storage space FOR YOU. The files that recovery tools normally can find…
  • e14 Contributor
    e14 Contributor over 13 years ago +1
    i bought a 32GB SD card,, is there a problem with doing that ?
  • saurocksall
    saurocksall over 12 years ago

    Hi Rohit,

     

    If the card is per installed with NOOBS you don't want to format it..

    but if you have a card to which you want to copy NOOBS you will need to format it, for this use SD Formatter Click HERE if you dont have it...

    i. Install and run the Formatting Tool on your machine...

    ii. Set "FORMAT SIZE ADJUSTMENT" option to "ON" in the "Options" menu...

    iii. Check that the SD card you inserted matches the one selected by the Tool...

    iv. Click the “Format” button...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • antihiro
    antihiro over 12 years ago in reply to saurocksall

    Nice!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • saurocksall
    saurocksall over 12 years ago

    Well explained and very informative.. almost every thing is covered...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • packetgeek
    packetgeek over 13 years ago in reply to e14 Contributor

    From what I gather in reading the docs, it shouldn't be an issue.  The site said "4GB or larger".

     

    R/ Tim

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    i bought a 32GB SD card,, is there a problem with doing that ?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<