Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Documents Getting Started With The Raspberry Pi 3
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: pchan
  • Date Created: 12 Oct 2016 4:45 PM Date Created
  • Last Updated Last Updated: 10 May 2021 7:13 PM
  • Views 4455 views
  • Likes 6 likes
  • Comments 4 comments
Related
Recommended

Getting Started With The Raspberry Pi 3

Learn how to get started with the Raspberry Pi 3 including what peripherals you need, putting the Pi in its case, using a NOOBS SD card to install the Raspbian Debian Linux OS, and getting online.  Kelly Hensen of the element14 community guides you through the steps needed to get started.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Episodes in this Series:

Get Started with the Raspberry Pi 3

 

image

The Raspberry Pi 3 is the latest version of the credit card sized computer from the Raspberry Pi Foundation. The Raspberry Pi was released by Premier Farnell, the company behind element14, in 2012.  The Raspberry Pi 3 is about 50% faster than its predecessor, the Pi 2. It includes built in WiFi and Bluetooth Low Energy connectivity, making it truly an IoT-ready device.

 

The Raspberry Pi 3 features a 1.2 GHz QUAD Core 64-bit Arm Cortex A53 processor, chip antenna, 4 USB ports, an ethernet port, a GPIO, HDMI, 3.5mm audio output, WiFi chip, 1GB LPDDR2 for RAM memory, and a microSD slot. The microSD card contains the Pi 3's operating system and it can also be used for file storage.

 

Raspberry Pi 3 Case
image
The Raspberry Pi 3 case is newly designed and comes in five parts - a top, a bottom, two sides, and a top testing/inspection window. Ensure the Pi 3 is seated on the 4 standoffs on the bottom of the case so it slots in smoothly. Then assemble the top and the sides so that they snap on easily. There are also slots for connecting peripherals such as your monitor, keyboard, and mouse. You can connect these peripherals through any of the USB and HDMI slots. If you do not have HDMI on your monitor you can purchase dongles for connecting through DVI or VGA.
16 GB MicroSD Card
image
The Pi 3 comes with a pre-formatted 16 GB microSD card that's pre-loaded with the "new out of the box" software called NOOBS. NOOBS makes setting up a Raspberry Pi for the first time much easier. It allows you to easily install, remove and then reinstall various flavors of the Linux operating system via its easy-to-use GUI. The regular operating system of the Pi 3 is Raspbian, an open source Debian Linux O/S. That's the one demonstrated in the video. If you have your Raspberry Pi in the case there is a slot for swapping out microSD cards to use different operating systems.
Stontronics 2.5AMP PSU
image
A new power adapter was designed for the Raspberry Pi 3 that can handle 2.5 amps so you can plug in and power peripherals directly from the Pi. The US version is demonstrated but included are various power supplies such as the one used in the UK.

 

Installation Process

Installation takes about 25 minutes. During the install, you'll see various informational messages about programming languages, applications and the Raspbian O/S in the installation window. If you are a beginner, these messages are very useful. The Pi 3 is loaded with all kinds of helpful tools, applications and games! After the install is complete you'll see a message that says the "OS(es) Installed Successfully." After the system reboots there will be a menu bar at the top where you can access all the programming languages, tools, file manager, office applications, accessories, and more.

Next, you'll need to configure the Pi 3. You no longer need to type in the command sudo raspi-config to the Raspberry Pi configuration tool. Just go to Preferences in the drop down menu to change your password and set your localization options. Getting online is incredibly easy using the built-in WiFi. Click on the network icon on the top right of the menu bar and enter in the password of your WiFi network to connect.

 

Parts List

Product NameDescriptionBuy All PartsBuy All Parts Buy All PartsBuy All Parts
Raspberry Pi 3Raspberry Pi 3Raspberry Pi 3Raspberry Pi 3Next Generation QUAD Core Broadcom BCM2837 64bit processorBuy this partBuy this partBuy this partBuy this part
Raspberry Pi 3 CaseRaspberry Pi 3 CaseOfficial enclosure from the Raspberry Pi foundationBuy this partBuy this part
16 GB MicroSD Card16 GB MicroSD CardPre-formatted 16 GB microSD card pre-loaded with NOOBS softwareBuy this partBuy this part
Stontronics 2.5AMP PSUStontronics 2.5AMP PSUPower adapter for the Raspberry Pi 3 that can handle 2.5 ampsBuy this partBuy this part
  • video_1
  • video one
  • part one
  • raspberry_pi
  • raspberry pi
  • getting started
  • part 1
  • raspberry pi 3
  • getting started with the raspberry pi 3
  • video 1
  • raspberry_pi_3
  • raspberry_pi_getting_started
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • DAB
    DAB over 8 years ago +1
    I fired up my RPi 3 over the weekend and it went super smooth. Up and running as soon as the Noobs card got everything installed. Much easier than when I fired up my RPi 2 a couple of years ago. DAB
  • mp2100
    mp2100 over 8 years ago in reply to reeve123igna +1
    Are you using NOOBS for the OS, or did you load Raspian directly onto the SD card? First, I would try a smaller SD card, or re-format your 64 GB card as FAT32. A 64 GB card is probably formatted as exFAT…
  • jakethesnake66
    jakethesnake66 over 7 years ago

    Thanks, my first. Was out shopping and began a conversation about coding and was told to use a raspberry pi 4 because that's what he uses. I'm new to coding so where do I go or contact to learn please.

    normanjeremiah8777@gmail.com

    Jerry

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mp2100
    mp2100 over 8 years ago in reply to reeve123igna

    Are you using NOOBS for the OS, or did you load Raspian directly onto the SD card?

     

    First, I would try a smaller SD card, or re-format your 64 GB card as FAT32.  A 64 GB card is probably formatted as exFAT, which I don't think the Pi3 can read.  A 32 GB or 16 GB card would be FAT32 by default.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 8 years ago

    I fired up my RPi 3 over the weekend and it went super smooth.

    Up and running as soon as the Noobs card got everything installed.

     

    Much easier than when I fired up my RPi 2 a couple of years ago.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • reeve123igna
    reeve123igna over 8 years ago

    i need help starting with the raspberry pi 3 i tried everything didnt work... using a 64gb card and a 55inch tv to dispaly... no matter what os i write on the card... it still doesnt work