Raspberry Pi
  • Products
  • More
Raspberry Pi
Documents Raspberry Pi Official Enclosure from the Raspberry Pi Foundation
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: pchan
  • Date Created: 8 Jun 2015 8:02 PM Date Created
  • Last Updated Last Updated: 10 May 2021 8:50 PM
  • Views 3916 views
  • Likes 4 likes
  • Comments 2 comments
Related
Recommended

Raspberry Pi Official Enclosure from the Raspberry Pi Foundation

image

 

Buy NowBuy Now  See other Pi Accessories

 

(N.B. Raspberry Pi 2 not included with case)

 

Technical Specification:

image  Official enclosure from the Raspberry Pi Foundation

image  5 part enclosure

image  Dimensions: 96mm x 70mm x 25mm

image  Raspberry coloured enclosure with White removable lid and sides

image  Removable lid is provided for easy access to the camera and display ports. This removable lid will also support access to an attached Raspberry Pi HAT device.

image  Removable GPIO side is provided for easy access to the 40-pin GPIO port (and attaching a ribbon cable).

image  Compatible with the Raspberry Pi 2 Model B and Raspberry Pi Model B+

 

N.B. Product is supplied assembled, shrink-wrapped with 4 rubber feet loose inside

 

Compatible With:

image  Raspberry Pi 2 Model B

image  Raspberry Pi Model B+

  • raspberry
  • the
  • from
  • pi
  • official
  • raspberry_pi
  • enclosure
  • foundation
  • case
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 11 years ago +1
    Good case but use with caution. I tried to insert the Pi 2 into the case without first removing the micro SD card. Big mistake. The case sheared off a slice of the micro SD card which then failed to boot…
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +1
    I wonder if the 3D model will be provided so we can print our own if able ? would be nice, it looks like a nice case for sure
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago

    I wonder if the 3D model will be provided so we can print our own if able ?

     

    would be nice, it looks like a nice case for sure

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago

    I wonder if the 3D model will be provided so we can print our own if able ?

     

    would be nice, it looks like a nice case for sure